<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Configuring PWM on iMX6UL - Causes system lock up in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Configuring-PWM-on-iMX6UL-Causes-system-lock-up/m-p/852098#M130363</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Running Ubuntu Linux in iMX6UL design.&lt;/P&gt;&lt;P&gt;I have modified the imx6ul.dtsi and imx6ul-14x14-evk.dts as shown below.&amp;nbsp; I logged on to the system and executed the command in sequence.&amp;nbsp; The result is that iMX6UL part becomes unresponsive or locked up.&amp;nbsp; Watchdog timer is not going off, cannot ping the system or connect in anyway without a power cycle.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Anyone have any ideas on what's going on?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;imx6ul.dtsi:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;pwm8: pwm@020fc000 {&lt;BR /&gt; compatible = "fsl,imx6ul-pwm", "fsl,imx27-pwm";&lt;BR /&gt; reg = &amp;lt;0x020fc000 0x4000&amp;gt;;&lt;BR /&gt; interrupts = &amp;lt;GIC_SPI 117 IRQ_TYPE_LEVEL_HIGH&amp;gt;;&lt;BR /&gt; clocks = &amp;lt;&amp;amp;clks IMX6UL_CLK_PWM8&amp;gt;,&lt;BR /&gt; &amp;lt;&amp;amp;clks IMX6UL_CLK_PWM8&amp;gt;;&lt;BR /&gt; clock-names = "ipg", "per";&lt;BR /&gt; #pwm-cells = &amp;lt;2&amp;gt;;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;imx6ul-14x14-evk.dts:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;amp;pwm8 {&lt;BR /&gt; pinctrl-names = "default";&lt;BR /&gt; pinctrl-0 = &amp;lt;&amp;amp;pinctrl_pwm8&amp;gt;;&lt;BR /&gt; status = "okay";&lt;BR /&gt;};&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;pinctrl_pwm8: pwm8grp {&lt;BR /&gt; fsl,pins = &amp;lt;&lt;BR /&gt; MX6UL_PAD_CSI_HSYNC__PWM8_OUT 0x08030&lt;BR /&gt; &amp;gt;;&lt;BR /&gt; };&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Command sequence:&lt;/P&gt;&lt;P&gt;root@sn1803149:~# echo 1 &amp;gt; /sys/class/pwm/pwmchip7/pwm0/enable&lt;BR /&gt;login as: root&lt;BR /&gt;root@10.31.77.115's password:&lt;BR /&gt;Last login: Thu Jan 3 09:55:41 2019 from 10.31.76.160&lt;BR /&gt;root@sn1803149:~# echo 0 &amp;gt; /sys/class/pwm/pwmchip8/export&lt;BR /&gt;-sh: /sys/class/pwm/pwmchip8/export: No such file or directory&lt;BR /&gt;root@sn1803149:~# echo 0 &amp;gt; /sys/class/pwm/pwmchip7/export&lt;BR /&gt;root@sn1803149:~#&lt;BR /&gt;root@sn1803149:~#&lt;BR /&gt;root@sn1803149:~#&lt;BR /&gt;root@sn1803149:~# echo 1000000 /sys/class/pwm/pwmchip7/pwm0/period&lt;BR /&gt;1000000 /sys/class/pwm/pwmchip7/pwm0/period&lt;BR /&gt;root@sn1803149:~#&lt;BR /&gt;root@sn1803149:~# echo 300000 /sys/class/pwm/pwmchip7/pwm0/duty_cycle&lt;BR /&gt;300000 /sys/class/pwm/pwmchip7/pwm0/duty_cycle&lt;BR /&gt;root@sn1803149:~#&lt;BR /&gt;root@sn1803149:~#&lt;BR /&gt;root@sn1803149:~# echo 1 &amp;gt; /sys/class/pwm/pwmchip7/pwm0/enable&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As soon as i execute the enable command, it goes to lunch and never comes back on it's own.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;&lt;P&gt;Jim D&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 03 Jan 2019 20:51:19 GMT</pubDate>
    <dc:creator>james_dunn</dc:creator>
    <dc:date>2019-01-03T20:51:19Z</dc:date>
    <item>
      <title>Configuring PWM on iMX6UL - Causes system lock up</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Configuring-PWM-on-iMX6UL-Causes-system-lock-up/m-p/852098#M130363</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Running Ubuntu Linux in iMX6UL design.&lt;/P&gt;&lt;P&gt;I have modified the imx6ul.dtsi and imx6ul-14x14-evk.dts as shown below.&amp;nbsp; I logged on to the system and executed the command in sequence.&amp;nbsp; The result is that iMX6UL part becomes unresponsive or locked up.&amp;nbsp; Watchdog timer is not going off, cannot ping the system or connect in anyway without a power cycle.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Anyone have any ideas on what's going on?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;imx6ul.dtsi:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;pwm8: pwm@020fc000 {&lt;BR /&gt; compatible = "fsl,imx6ul-pwm", "fsl,imx27-pwm";&lt;BR /&gt; reg = &amp;lt;0x020fc000 0x4000&amp;gt;;&lt;BR /&gt; interrupts = &amp;lt;GIC_SPI 117 IRQ_TYPE_LEVEL_HIGH&amp;gt;;&lt;BR /&gt; clocks = &amp;lt;&amp;amp;clks IMX6UL_CLK_PWM8&amp;gt;,&lt;BR /&gt; &amp;lt;&amp;amp;clks IMX6UL_CLK_PWM8&amp;gt;;&lt;BR /&gt; clock-names = "ipg", "per";&lt;BR /&gt; #pwm-cells = &amp;lt;2&amp;gt;;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;imx6ul-14x14-evk.dts:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;amp;pwm8 {&lt;BR /&gt; pinctrl-names = "default";&lt;BR /&gt; pinctrl-0 = &amp;lt;&amp;amp;pinctrl_pwm8&amp;gt;;&lt;BR /&gt; status = "okay";&lt;BR /&gt;};&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;pinctrl_pwm8: pwm8grp {&lt;BR /&gt; fsl,pins = &amp;lt;&lt;BR /&gt; MX6UL_PAD_CSI_HSYNC__PWM8_OUT 0x08030&lt;BR /&gt; &amp;gt;;&lt;BR /&gt; };&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Command sequence:&lt;/P&gt;&lt;P&gt;root@sn1803149:~# echo 1 &amp;gt; /sys/class/pwm/pwmchip7/pwm0/enable&lt;BR /&gt;login as: root&lt;BR /&gt;root@10.31.77.115's password:&lt;BR /&gt;Last login: Thu Jan 3 09:55:41 2019 from 10.31.76.160&lt;BR /&gt;root@sn1803149:~# echo 0 &amp;gt; /sys/class/pwm/pwmchip8/export&lt;BR /&gt;-sh: /sys/class/pwm/pwmchip8/export: No such file or directory&lt;BR /&gt;root@sn1803149:~# echo 0 &amp;gt; /sys/class/pwm/pwmchip7/export&lt;BR /&gt;root@sn1803149:~#&lt;BR /&gt;root@sn1803149:~#&lt;BR /&gt;root@sn1803149:~#&lt;BR /&gt;root@sn1803149:~# echo 1000000 /sys/class/pwm/pwmchip7/pwm0/period&lt;BR /&gt;1000000 /sys/class/pwm/pwmchip7/pwm0/period&lt;BR /&gt;root@sn1803149:~#&lt;BR /&gt;root@sn1803149:~# echo 300000 /sys/class/pwm/pwmchip7/pwm0/duty_cycle&lt;BR /&gt;300000 /sys/class/pwm/pwmchip7/pwm0/duty_cycle&lt;BR /&gt;root@sn1803149:~#&lt;BR /&gt;root@sn1803149:~#&lt;BR /&gt;root@sn1803149:~# echo 1 &amp;gt; /sys/class/pwm/pwmchip7/pwm0/enable&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As soon as i execute the enable command, it goes to lunch and never comes back on it's own.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;&lt;P&gt;Jim D&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 03 Jan 2019 20:51:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Configuring-PWM-on-iMX6UL-Causes-system-lock-up/m-p/852098#M130363</guid>
      <dc:creator>james_dunn</dc:creator>
      <dc:date>2019-01-03T20:51:19Z</dc:date>
    </item>
    <item>
      <title>Re: Configuring PWM on iMX6UL - Causes system lock up</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Configuring-PWM-on-iMX6UL-Causes-system-lock-up/m-p/852099#M130364</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi James&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;example of i.mx6ul pwm8 can be found in BD linux-imx6/arch/arm/boot/dts/imx6ul-pico-hobbit.dts&lt;/P&gt;&lt;P&gt;and one can try it&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://github.com/boundarydevices/linux-imx6/blob/boundary-imx_4.9.x_2.0.0_ga/arch/arm/boot/dts/imx6ul-pico-hobbit.dts" title="https://github.com/boundarydevices/linux-imx6/blob/boundary-imx_4.9.x_2.0.0_ga/arch/arm/boot/dts/imx6ul-pico-hobbit.dts"&gt;linux-imx6/imx6ul-pico-hobbit.dts at boundary-imx_4.9.x_2.0.0_ga · boundarydevices/linux-imx6 · GitHub&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 08 Jan 2019 01:03:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Configuring-PWM-on-iMX6UL-Causes-system-lock-up/m-p/852099#M130364</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2019-01-08T01:03:33Z</dc:date>
    </item>
    <item>
      <title>Re: Configuring PWM on iMX6UL - Causes system lock up</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Configuring-PWM-on-iMX6UL-Causes-system-lock-up/m-p/1248354#M171083</link>
      <description>&lt;P&gt;Hello Jim,&lt;/P&gt;&lt;P&gt;I've got the very same problem, were you able to solve it?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 18 Mar 2021 17:57:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Configuring-PWM-on-iMX6UL-Causes-system-lock-up/m-p/1248354#M171083</guid>
      <dc:creator>TheSnake69</dc:creator>
      <dc:date>2021-03-18T17:57:29Z</dc:date>
    </item>
  </channel>
</rss>