<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 USB Detection Issue on iMX6ULL processor</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/USB-Detection-Issue-on-iMX6ULL-processor/m-p/851572#M130310</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am using iMX6ULL processor for custom board design. I am facing an issue where USB is not detected every time over USB cable.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there any other way?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Sahil&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 22 Jan 2019 15:03:42 GMT</pubDate>
    <dc:creator>sahilnayak</dc:creator>
    <dc:date>2019-01-22T15:03:42Z</dc:date>
    <item>
      <title>USB Detection Issue on iMX6ULL processor</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/USB-Detection-Issue-on-iMX6ULL-processor/m-p/851572#M130310</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am using iMX6ULL processor for custom board design. I am facing an issue where USB is not detected every time over USB cable.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there any other way?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Sahil&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 22 Jan 2019 15:03:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/USB-Detection-Issue-on-iMX6ULL-processor/m-p/851572#M130310</guid>
      <dc:creator>sahilnayak</dc:creator>
      <dc:date>2019-01-22T15:03:42Z</dc:date>
    </item>
    <item>
      <title>Re: USB Detection Issue on iMX6ULL processor</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/USB-Detection-Issue-on-iMX6ULL-processor/m-p/851573#M130311</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Please try to set USB controller as host-only mode with setting&lt;BR /&gt;dr_mode = "peripheral"&lt;BR /&gt;in the DTS file. It may help.&lt;BR /&gt;Please refer to chapter 39.2.6 "Changing the Controller Operation Mode" of i.MX Linux Reference Manual for the details.&lt;BR /&gt;You can get the documentation here:&lt;BR /&gt;&lt;A href="https://www.nxp.com/webapp/Download?colCode=L4.1.15_2.0.0-LINUX-DOCS"&gt;https://www.nxp.com/webapp/Download?colCode=L4.1.15_2.0.0-LINUX-DOCS&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Victor&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 23 Jan 2019 09:46:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/USB-Detection-Issue-on-iMX6ULL-processor/m-p/851573#M130311</guid>
      <dc:creator>b36401</dc:creator>
      <dc:date>2019-01-23T09:46:40Z</dc:date>
    </item>
  </channel>
</rss>