<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Cortex-M4 Core1 is not working in IMX8QM CPU</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Cortex-M4-Core1-is-not-working-in-IMX8QM-CPU/m-p/851385#M130270</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Please refer to the attached document, especially, to its Section 4.7.6 "Running the Arm Cortex-M4 image" for the information on how to build images and run the code on the M4 core(s) on various asymmetric multicore i.MX processors, including the i.MX8QM one.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 26 Feb 2019 09:47:15 GMT</pubDate>
    <dc:creator>art</dc:creator>
    <dc:date>2019-02-26T09:47:15Z</dc:date>
    <item>
      <title>Cortex-M4 Core1 is not working in IMX8QM CPU</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Cortex-M4-Core1-is-not-working-in-IMX8QM-CPU/m-p/851384#M130269</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;We are testing M4 cores in IMX8QM with pre-build and compiled binaries, in this M4 Core0 is working without any issues.&lt;/P&gt;&lt;P&gt;The M4 Core1 is not working with both the pre-build and compiled binaries. We are able to access the M4 Core0 and Core1 UARTs pin as GPIO in U-boot. We are using 4.14.78-GA BSP release SCFW.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;BR /&gt;Pranav&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 Feb 2019 08:35:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Cortex-M4-Core1-is-not-working-in-IMX8QM-CPU/m-p/851384#M130269</guid>
      <dc:creator>pranav_vaze</dc:creator>
      <dc:date>2019-02-26T08:35:27Z</dc:date>
    </item>
    <item>
      <title>Re: Cortex-M4 Core1 is not working in IMX8QM CPU</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Cortex-M4-Core1-is-not-working-in-IMX8QM-CPU/m-p/851385#M130270</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Please refer to the attached document, especially, to its Section 4.7.6 "Running the Arm Cortex-M4 image" for the information on how to build images and run the code on the M4 core(s) on various asymmetric multicore i.MX processors, including the i.MX8QM one.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 Feb 2019 09:47:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Cortex-M4-Core1-is-not-working-in-IMX8QM-CPU/m-p/851385#M130270</guid>
      <dc:creator>art</dc:creator>
      <dc:date>2019-02-26T09:47:15Z</dc:date>
    </item>
    <item>
      <title>Re: Cortex-M4 Core1 is not working in IMX8QM CPU</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Cortex-M4-Core1-is-not-working-in-IMX8QM-CPU/m-p/851386#M130271</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Artur,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;We are following same commands for creating M4 binaries for booting from u-boot and booting from ROM options.&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;The M4 Core0 is booting with both the boot options (We are getting output messages in M4-Core0 UART).&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;The M4 Core1 is not booting with both the boot options.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Pranav&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 Feb 2019 13:17:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Cortex-M4-Core1-is-not-working-in-IMX8QM-CPU/m-p/851386#M130271</guid>
      <dc:creator>pranav_vaze</dc:creator>
      <dc:date>2019-02-26T13:17:45Z</dc:date>
    </item>
    <item>
      <title>Re: Cortex-M4 Core1 is not working in IMX8QM CPU</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Cortex-M4-Core1-is-not-working-in-IMX8QM-CPU/m-p/851387#M130272</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;How do you define that the M4 Core1 does not boot? By absence of the UART output from it? Which UART do you assign to M4 Core1?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Artur&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 04 Mar 2019 04:43:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Cortex-M4-Core1-is-not-working-in-IMX8QM-CPU/m-p/851387#M130272</guid>
      <dc:creator>art</dc:creator>
      <dc:date>2019-03-04T04:43:09Z</dc:date>
    </item>
  </channel>
</rss>