<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: wifi module rtl8812 softap start failed on android6.0(kernel4.1.15)</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/wifi-module-rtl8812-softap-start-failed-on-android6-0-kernel4-1/m-p/850485#M130169</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I apologize for the delay.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The hotspot from Android only works in one way. It can only be transceiver&amp;nbsp;or sender, not both. You can try to use a GSM module to have a mobile&amp;nbsp;internet connection and then use the hotspot feature. However this out of our scope, I apologize for the inconveniences this could give you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Diego.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 18 Dec 2018 14:41:04 GMT</pubDate>
    <dc:creator>diegoadrian</dc:creator>
    <dc:date>2018-12-18T14:41:04Z</dc:date>
    <item>
      <title>wifi module rtl8812 softap start failed on android6.0(kernel4.1.15)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/wifi-module-rtl8812-softap-start-failed-on-android6-0-kernel4-1/m-p/850484#M130168</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;first,turn on the Portable Wi-Fi hotspot button to enable hotspot，but hotspot keep the status，as shown below redline mark&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="1.jpg"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/76492i4ACB3723791D6DBC/image-size/large?v=v2&amp;amp;px=999" role="button" title="1.jpg" alt="1.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;log:&lt;/P&gt;&lt;P&gt;RTW: EEPROM ID=0x8129&lt;BR /&gt;RTW: VID = 0x0BDA, PID = 0x0811&lt;BR /&gt;RTW: Customer ID: 0x00, SubCustomer ID: 0xCD&lt;BR /&gt;RTW: EEPROMRegulatory = 0x1&lt;BR /&gt;RTW: Board Type: 0x 0&lt;BR /&gt;RTW: Hal_EfuseParseBTCoexistInfo8812A: BTCoexist=Disable, AntNum=1, AntPath=0&lt;BR /&gt;RTW: hal_com_config_channel_plan chplan:0x7F&lt;BR /&gt;RTW: crystal_cap: 0x11&lt;BR /&gt;RTW: ThermalMeter = 0x1b&lt;BR /&gt;RTW: Hal_ReadRemoteWakeup_8812A...bSupportRemoteWakeup(1)&lt;BR /&gt;RTW: pHalData-&amp;gt;PAType_2G is 0x0, pHalData-&amp;gt;ExternalPA_2G = 0&lt;BR /&gt;RTW: pHalData-&amp;gt;PAType_5G is 0x0, pHalData-&amp;gt;external_pa_5g = 0&lt;BR /&gt;RTW: pHalData-&amp;gt;LNAType_2G is 0x0, pHalData-&amp;gt;ExternalLNA_2G = 0&lt;BR /&gt;RTW: pHalData-&amp;gt;LNAType_5G is 0x0, pHalData-&amp;gt;external_lna_5g = 0&lt;BR /&gt;RTW: Usb Switch: 0&lt;BR /&gt;RTW: PID= 0x811, VID= bda&lt;BR /&gt;RTW: PID= 0x811, VID= bda&lt;BR /&gt;RTW: Customer ID: 0x 0&lt;BR /&gt;RTW: hal_ReadUsbType_8812AU: antenna=7, wmode=3&lt;BR /&gt;RTW: rtw_hal_read_chip_info in 190 ms&lt;BR /&gt;RTW: init_channel_set((null)) ChannelPlan ID:0x7f, ch num:37&lt;BR /&gt;RTW: NR_RECVBUFF: 8&lt;BR /&gt;RTW: MAX_RECVBUF_SZ: 32768&lt;BR /&gt;RTW: NR_PREALLOC_RECV_SKB: 8&lt;BR /&gt;RTW: rtw_alloc_macid((null)) if1, hwaddr:ff:ff:ff:ff:ff:ff macid:1&lt;BR /&gt;RTW: rtw_regsty_chk_target_tx_power_valid return _FALSE for band:0, path:0, rs:0, t:-1&lt;BR /&gt;RTW: pwrctrlpriv.bSupportRemoteWakeup~~~~~~&lt;BR /&gt;RTW: pwrctrlpriv.bSupportRemoteWakeup~~~[1]~~~&lt;BR /&gt;RTW: can't get autopm:&lt;BR /&gt;RTW: rtw_macaddr_cfg mac addr:0c:8c:24:6d:e4:ba&lt;BR /&gt;RTW: bDriverStopped:True, bSurpriseRemoved:False, bup:0, hw_init_completed:0&lt;BR /&gt;RTW: init_channel_set((null)) ChannelPlan ID:0x7f, ch num:37&lt;BR /&gt;RTW: NR_RECVBUFF: 8&lt;BR /&gt;RTW: MAX_RECVBUF_SZ: 32768&lt;BR /&gt;RTW: NR_PREALLOC_RECV_SKB: 8&lt;BR /&gt;RTW: rtw_alloc_macid((null)) if2, hwaddr:ff:ff:ff:ff:ff:ff macid:1&lt;BR /&gt;RTW: rtw_drv_add_vir_if if2 mac_addr : 0e:8c:24:6d:e4:ba&lt;BR /&gt;RTW: rtw_wiphy_alloc(phy0)&lt;BR /&gt;RTW: rtw_wdev_alloc(padapter=e7a5d000)&lt;BR /&gt;RTW: rtw_wiphy_alloc(phy1)&lt;BR /&gt;RTW: rtw_wdev_alloc(padapter=e7c1a000)&lt;BR /&gt;RTW: rtw_wiphy_register(phy0)&lt;BR /&gt;RTW: Register RTW cfg80211 vendor cmd(0x67) interface&lt;BR /&gt;RTW: rtw_ndev_init(wlan0) if1 mac_addr=0c:8c:24:6d:e4:ba&lt;BR /&gt;RTW: rtw_ndev_notifier_call(wlan0) state:16&lt;BR /&gt;RTW: rtw_ndev_notifier_call(wlan0) state:5&lt;BR /&gt;RTW: rtw_wiphy_register(phy1)&lt;BR /&gt;RTW: Register RTW cfg80211 vendor cmd(0x67) interface&lt;BR /&gt;RTW: rtw_ndev_init(p2p0) if2 mac_addr=0e:8c:24:6d:e4:ba&lt;BR /&gt;RTW: rtw_ndev_notifier_call(p2p0) state:16&lt;BR /&gt;RTW: rtw_ndev_notifier_call(p2p0) state:5&lt;BR /&gt;usbcore: registered new interface driver rtl8821au&lt;BR /&gt;RTW: module init ret=0&lt;BR /&gt;init: Starting service 'rtw_fwloader'...&lt;BR /&gt;init: Service 'rtw_fwloader' (pid 1590) exited with status 0&lt;BR /&gt;RTW: rtw_ndev_notifier_call(wlan0) state:13&lt;BR /&gt;RTW: _netdev_open(wlan0) , bup=0&lt;BR /&gt;RTW: power-on :REG_SYS_CLKR 0x09=0x30. REG_CR 0x100=0xea.&lt;BR /&gt;RTW: MAC has not been powered on yet.&lt;BR /&gt;RTW: SetHwReg: bMacPwrCtrlOn=1&lt;BR /&gt;RTW: FirmwareDownload8812 fw source from Header&lt;BR /&gt;RTW: FirmwareDownload8812 fw:NIC, size: 31834&lt;BR /&gt;RTW: FirmwareDownload8812: fw_ver=40 fw_subver=1 sig=0x2101&lt;BR /&gt;RTW: polling_fwdl_chksum: Checksum report OK! (1, 0ms), REG_MCUFWDL:0x00070605&lt;BR /&gt;RTW: =====&amp;gt; _8051Reset8812(): 8051 reset success .&lt;BR /&gt;RTW: _FWFreeToGo8812: Polling FW ready OK! (12, 40ms), REG_MCUFWDL:0x000706c6&lt;BR /&gt;RTW: FWDL success. write_fw:1, 90ms&lt;BR /&gt;RTW: rtl8812au_hal_init: Download Firmware Success!!&lt;BR /&gt;11-20 11:42:42.748 1071 1071 I Choreographer: Skipped 51 frames! The application may be doing too much work on its main thread.&lt;BR /&gt;RTW: HW_VAR_BASIC_RATE: 0x15f-&amp;gt;0x15f-&amp;gt;0x15f&lt;BR /&gt;RTW: rtl8812a_combo_card_WifiOnlyHwInit !&lt;BR /&gt;RTW: rtl8812au_hal_init in 880ms&lt;BR /&gt;RTW: rtw_hal_set_macaddr_port wlan0- hw port(0) mac_addr =0c:8c:24:6d:e4:ba&lt;BR /&gt;RTW: rtw_hal_set_macaddr_port p2p0- hw port(1) mac_addr =0e:8c:24:6d:e4:ba&lt;BR /&gt;RTW: rtw_hal_get_macaddr_port wlan0- hw port(0) mac_addr =0c:8c:24:6d:e4:ba&lt;BR /&gt;RTW: wlan0- hw port(0) mac_addr =0c:8c:24:6d:e4:ba&lt;BR /&gt;RTW: rtw_hal_get_macaddr_port p2p0- hw port(1) mac_addr =0e:8c:24:6d:e4:ba&lt;BR /&gt;RTW: p2p0- hw port(1) mac_addr =0e:8c:24:6d:e4:ba&lt;BR /&gt;RTW: MAC Address = 0c:8c:24:6d:e4:ba&lt;BR /&gt;RTW: rtw_cfg80211_init_wiphy:rf_type=3&lt;BR /&gt;RTW: [HT] HAL Support LDPC = 0x02&lt;BR /&gt;RTW: [HT] HAL Support STBC = 0x01&lt;BR /&gt;RTW: [HT] HAL Support LDPC = 0x02&lt;BR /&gt;RTW: [HT] HAL Support STBC = 0x01&lt;BR /&gt;RTW: _netdev_vir_if_open(p2p0) , bup=0&lt;BR /&gt;RTW: rtw_cfg80211_init_wiphy:rf_type=3&lt;BR /&gt;RTW: [HT] HAL Support LDPC = 0x02&lt;BR /&gt;RTW: [HT] HAL Support STBC = 0x01&lt;BR /&gt;RTW: [HT] HAL Support LDPC = 0x02&lt;BR /&gt;RTW: [HT] HAL Support STBC = 0x01&lt;BR /&gt;RTW: _netdev_vir_if_open(p2p0) (bup=1) exit&lt;BR /&gt;RTW: -871x_drv - drv_open, bup=1&lt;BR /&gt;IPv6: ADDRCONF(NETDEV_UP): wlan0: link is not ready&lt;BR /&gt;RTW: cfg80211_rtw_set_power_mgmt(wlan0) enabled:1, timeout:-1&lt;BR /&gt;RTW: rtw_ndev_notifier_call(wlan0) state:1&lt;BR /&gt;11-20 11:42:43.132 562 605 D wifi : set interface wlan0 flags (UP)&lt;BR /&gt;11-20 11:42:43.132 562 605 D wifi : Did set static halHandle = 0x0&lt;BR /&gt;11-20 11:42:43.132 562 605 D wifi : halHandle = 0x0, mVM = 0xb4dbc000, mCls = 0xeee&lt;BR /&gt;11-20 11:42:43.132 562 605 E WifiNative-HAL: Could not start hal&lt;BR /&gt;11-20 11:42:43.132 562 605 E WifiStateMachine: Failed to start HAL&lt;BR /&gt;11-20 11:42:43.133 562 605 D WifiStateMachine: setWifiApState: enabling&lt;BR /&gt;11-20 11:42:43.135 562 605 D WifiStateMachine: SoftAp config channel is: 0&lt;BR /&gt;11-20 11:42:43.183 1390 1390 E SoftapController: SoftAP is already running&lt;BR /&gt;11-20 11:42:43.184 562 1595 D WifiStateMachine: Soft AP start successful&lt;BR /&gt;11-20 11:42:43.185 562 605 D WifiStateMachine: setWifiApState: enabled&lt;BR /&gt;11-20 11:42:43.196 1233 1233 D CommandListener: Setting iface cfg&lt;BR /&gt;11-20 11:42:43.196 1233 1233 D CommandListener: Trying to bring up wlan0&lt;BR /&gt;11-20 11:42:43.198 562 605 D Tethering: Tethering wlan0&lt;BR /&gt;11-20 11:42:43.198 562 605 E Tethering: Tried to Tether an unknown iface :wlan0, ignoring&lt;BR /&gt;11-20 11:42:43.198 562 605 E WifiStateMachine: Error tethering on wlan0&lt;BR /&gt;11-20 11:42:43.203 562 605 D WifiStateMachine: Link configuration changed for netId: -1 old: {InterfaceName: wlan0 LinkAddresses: [] Routes: [] DnsAddresses: [] Domains: null MTU: 0 TcpBufferSizes: 524288,1048576,2097152,262144,524288,1048576} new: {InterfaceName: wlan0 LinkAddresses: [192.168.43.1/24,] Routes: [] DnsAddresses: [] Domains: null MTU: 0 TcpBufferSizes: 524288,1048576,2097152,262144,524288,1048576}&lt;BR /&gt;11-20 11:42:43.203 562 605 D WifiStateMachine: updateLinkProperties nid: -1 state: DISCONNECTED reason: CMD_UPDATE_LINKPROPERTIES v4&lt;BR /&gt;11-20 11:42:44.620 207 535 W audio_hw_primary: do_out_standby... -1242503424&lt;BR /&gt;11-20 11:42:44.730 218 244 D QTAService: ====change@/devices/platform/regulatory.0===&lt;BR /&gt;RTW: ==&amp;gt;rtw_ps_processor .fw_state(0)&lt;BR /&gt;RTW: ==&amp;gt;ips_enter cnts:1&lt;BR /&gt;RTW: nolinked power save enter&lt;BR /&gt;RTW: ===&amp;gt; rtw_ips_pwr_down...................&lt;BR /&gt;RTW: ====&amp;gt; rtw_ips_dev_unload...&lt;BR /&gt;RTW: usb_read_port_cancel&lt;BR /&gt;RTW: usb_read_port_complete() RX Warning! bDriverStopped(False) OR bSurpriseRemoved(False)&lt;BR /&gt;RTW: usb_read_port_complete() RX Warning! bDriverStopped(False) OR bSurpriseRemoved(False)&lt;BR /&gt;RTW: usb_read_port_complete() RX Warning! bDriverStopped(False) OR bSurpriseRemoved(False)&lt;BR /&gt;RTW: usb_read_port_complete() RX Warning! bDriverStopped(False) OR bSurpriseRemoved(False)&lt;BR /&gt;RTW: usb_read_port_complete() RX Warning! bDriverStopped(False) OR bSurpriseRemoved(False)&lt;BR /&gt;RTW: usb_read_port_complete() RX Warning! bDriverStopped(False) OR bSurpriseRemoved(False)&lt;BR /&gt;RTW: usb_read_port_complete() RX Warning! bDriverStopped(False) OR bSurpriseRemoved(False)&lt;BR /&gt;RTW: usb_read_port_complete() RX Warning! bDriverStopped(False) OR bSurpriseRemoved(False)&lt;BR /&gt;RTW: usb_write_port_cancel&lt;BR /&gt;RTW: ==&amp;gt; rtl8812au_hal_deinit&lt;BR /&gt;RTW: hal_poweroff_8812au&lt;BR /&gt;RTW: =====&amp;gt; _8051Reset8812(): 8051 reset success .&lt;BR /&gt;RTW: SetHwReg: bMacPwrCtrlOn=0&lt;BR /&gt;RTW: &amp;lt;=== rtw_ips_pwr_down..................... in 110ms&lt;BR /&gt;11-20 11:42:47.880 218 244 D QTAService: ====change@/devices/platform/regulatory.0===&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;second，if i input command "hostapd -e /data/misc/wifi/entropy.bin /data/misc/wifi/hostapd.conf" to terminal by serial port ,the hotspot is really tuned on，&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="2.jpg"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/76609i4BA45849871D7E88/image-size/large?v=v2&amp;amp;px=999" role="button" title="2.jpg" alt="2.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;log:&lt;/P&gt;&lt;P&gt;hostapd -e /data/misc/wifi/entropy.bin /data/misc/wifi/hostapd.conf &amp;lt;&lt;BR /&gt;RTW: cfg80211_rtw_change_iface(wlan0) type=3, hw_port:0&lt;BR /&gt;RTW: cfg80211_rtw_change_iface(wlan0) call netdev_open&lt;BR /&gt;RTW: _netdev_open(wlan0) , bup=1&lt;BR /&gt;RTW: -871x_drv - drv_open, bup=1&lt;BR /&gt;RTW: _rtw_pwr_wakeup call ips_leave....&lt;BR /&gt;RTW: ==&amp;gt;ips_leave cnts:1&lt;BR /&gt;RTW: ===&amp;gt; rtw_ips_pwr_up..............&lt;BR /&gt;RTW: ===&amp;gt; ips_netdrv_open.........&lt;BR /&gt;RTW: power-on :REG_SYS_CLKR 0x09=0x30. REG_CR 0x100=0xea.&lt;BR /&gt;RTW: MAC has not been powered on yet.&lt;BR /&gt;RTW: SetHwReg: bMacPwrCtrlOn=1&lt;BR /&gt;RTW: FirmwareDownload8812 fw source from Header&lt;BR /&gt;RTW: FirmwareDownload8812 fw:NIC, size: 31834&lt;BR /&gt;RTW: FirmwareDownload8812: fw_ver=40 fw_subver=1 sig=0x2101&lt;BR /&gt;RTW: polling_fwdl_chksum: Checksum report OK! (1, 0ms), REG_MCUFWDL:0x00070605&lt;BR /&gt;RTW: =====&amp;gt; _8051Reset8812(): 8051 reset success .&lt;BR /&gt;RTW: _FWFreeToGo8812: Polling FW ready OK! (202, 30ms), REG_MCUFWDL:0x000706c6&lt;BR /&gt;RTW: FWDL success. write_fw:1, 90ms&lt;BR /&gt;RTW: rtl8812au_hal_init: Download Firmware Success!!&lt;BR /&gt;RTW: HW_VAR_BASIC_RATE: 0x15f-&amp;gt;0x15f-&amp;gt;0x15f&lt;BR /&gt;RTW: rtl8812a_combo_card_WifiOnlyHwInit !&lt;BR /&gt;RTW: rtl8812au_hal_init in 510ms&lt;BR /&gt;RTW: rtw_hal_set_macaddr_port wlan0- hw port(0) mac_addr =0c:8c:24:6d:e4:ba&lt;BR /&gt;RTW: rtw_hal_set_macaddr_port p2p0- hw port(1) mac_addr =0e:8c:24:6d:e4:ba&lt;BR /&gt;RTW: rtw_hal_get_macaddr_port wlan0- hw port(0) mac_addr =0c:8c:24:6d:e4:ba&lt;BR /&gt;RTW: wlan0- hw port(0) mac_addr =0c:8c:24:6d:e4:ba&lt;BR /&gt;RTW: rtw_hal_get_macaddr_port p2p0- hw port(1) mac_addr =0e:8c:24:6d:e4:ba&lt;BR /&gt;RTW: p2p0- hw port(1) mac_addr =0e:8c:24:6d:e4:ba&lt;BR /&gt;RTW: &amp;lt;=== rtw_ips_pwr_up.............. in 550ms&lt;BR /&gt;RTW: nolinked power save leave&lt;BR /&gt;RTW: ==&amp;gt; ips_leave.....LED(0x01408282)...&lt;BR /&gt;RTW: cfg80211_rtw_change_iface(wlan0) old_iftype=2, new_iftype=3&lt;BR /&gt;RTW: ERROR rtw_release_macid(wlan0) if1, hwaddr:ff:ff:ff:ff:ff:ff with macid:1&lt;BR /&gt;RTW: rtw_alloc_macid(wlan0) if1, hwaddr:ff:ff:ff:ff:ff:ff macid:0&lt;BR /&gt;RTW: rtw_hal_set_macaddr_port wlan0- hw port(0) mac_addr =0c:8c:24:6d:e4:ba&lt;BR /&gt;RTW: cfg80211_rtw_change_iface(wlan0) ret:0&lt;BR /&gt;RTW: hw_var_set_opmode()-4711 mode = 3&lt;BR /&gt;RTW: +cfg80211_rtw_del_station(wlan0)&lt;BR /&gt;RTW: flush all sta, and cam_entry&lt;BR /&gt;RTW: rtw_sta_flush(wlan0)&lt;BR /&gt;RTW: issue_deauth to ff:ff:ff:ff:ff:ff&lt;BR /&gt;RTW: +cfg80211_rtw_del_station(wlan0)&lt;BR /&gt;RTW: free sta macaddr =ff:ff:ff:ff:ff:ff&lt;BR /&gt;RTW: cfg80211_rtw_del_key(wlan0) key_index=0&lt;BR /&gt;RTW: cfg80211_rtw_del_key(wlan0) key_index=1&lt;BR /&gt;RTW: cfg80211_rtw_del_key(wlan0) key_index=2&lt;BR /&gt;RTW: cfg80211_rtw_del_key(wlan0) key_index=3&lt;BR /&gt;RTW: cfg80211_rtw_start_ap(wlan0) hidden_ssid:0, auth_type:5&lt;BR /&gt;RTW: rtw_add_beacon beacon_head_len=60, beacon_tail_len=109&lt;BR /&gt;RTW: rtw_check_beacon_data, len=145&lt;BR /&gt;RTW: [HT] HAL Support LDPC = 0x02&lt;BR /&gt;RTW: [HT] HAL Support STBC = 0x01&lt;BR /&gt;RTW: update_hw_ht_param&lt;BR /&gt;RTW: rtw_hal_set_bssid wlan0- hw port -0 BSSID: 0c:8c:24:6d:e4:ba&lt;BR /&gt;RTW: rtw_ap_chbw_decision(wlan0) ld_sta_num:0, lg_sta_num0, ap_num:0&lt;BR /&gt;RTW: rtw_ap_chbw_decision(wlan0) req: 0,-1,-1&lt;BR /&gt;RTW: rtw_ap_chbw_decision(wlan0) dec: 6,0,0&lt;BR /&gt;RTW: HW_VAR_BASIC_RATE: 0x15f-&amp;gt;0x15f-&amp;gt;0x15f&lt;BR /&gt;RTW: add_RATid=&amp;gt; mac_id:0 , raid:8, tx_ra_bitmap:0x000000000000000f, networkType:0x01&lt;BR /&gt;RTW: rtw_update_ramask =&amp;gt; mac_id:0, networkType:0x01, mask:0x000000000000000f&lt;BR /&gt; ==&amp;gt; rssi_level:0, rate_bitmap:0x0000000000000000, shortGIrate=0&lt;BR /&gt; ==&amp;gt; bw:0, ignore_bw:0x0&lt;BR /&gt;RTW: IQK offload finish in 30ms&lt;BR /&gt;RTW: rtw_cfg80211_indicate_connect(wlan0)&lt;BR /&gt;RTW: assoc success&lt;BR /&gt;IPv6: ADDRCONF(NETDEV_CHANGE): wlan0: link becomes ready&lt;BR /&gt;RTW: rtw_ndev_notifier_call(wlan0) state:4&lt;BR /&gt;RTW: cfg80211_rtw_change_bss(wlan0)&lt;BR /&gt;RTW: cfg80211_rtw_add_key(wlan0) adding key for (null)&lt;BR /&gt;RTW: cipher=0xfac04&lt;BR /&gt;RTW: key_len=0x10&lt;BR /&gt;RTW: seq_len=0x0&lt;BR /&gt;RTW: key_index=1&lt;BR /&gt;RTW: pairwise=0&lt;BR /&gt;RTW: rtw_cfg80211_ap_set_encryption&lt;BR /&gt;RTW: rtw_cfg80211_ap_set_encryption, set group_key, CCMP&lt;BR /&gt;RTW: rtw_ap_set_group_key&lt;BR /&gt;RTW: set group key camid:0, addr:0c:8c:24:6d:e4:ba, kid:1, type:AES&lt;BR /&gt;RTW: cfg80211_rtw_set_default_key(wlan0) key_index=1, unicast=0, multicast=1&lt;BR /&gt;RTW: cfg80211_rtw_set_mac_acl(wlan0) acl_policy:0, entry_num:0&lt;BR /&gt;RTW: WARN cfg80211_rtw_set_mac_acl(wlan0) acl_policy:0 with no entry&lt;BR /&gt;RTW: rtw_set_macaddr_acl(wlan0) mode=0&lt;BR /&gt;RTW: SetHwReg8812A, 5544, RCR= f400608e&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;but ， i don't know how to solve it，please help me&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 20 Nov 2018 03:46:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/wifi-module-rtl8812-softap-start-failed-on-android6-0-kernel4-1/m-p/850484#M130168</guid>
      <dc:creator>sunyd</dc:creator>
      <dc:date>2018-11-20T03:46:03Z</dc:date>
    </item>
    <item>
      <title>Re: wifi module rtl8812 softap start failed on android6.0(kernel4.1.15)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/wifi-module-rtl8812-softap-start-failed-on-android6-0-kernel4-1/m-p/850485#M130169</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I apologize for the delay.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The hotspot from Android only works in one way. It can only be transceiver&amp;nbsp;or sender, not both. You can try to use a GSM module to have a mobile&amp;nbsp;internet connection and then use the hotspot feature. However this out of our scope, I apologize for the inconveniences this could give you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Diego.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 18 Dec 2018 14:41:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/wifi-module-rtl8812-softap-start-failed-on-android6-0-kernel4-1/m-p/850485#M130169</guid>
      <dc:creator>diegoadrian</dc:creator>
      <dc:date>2018-12-18T14:41:04Z</dc:date>
    </item>
  </channel>
</rss>