<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックPower consumption (AN4270)</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Power-consumption-AN4270/m-p/212513#M13016</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear all,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm trying to evaluate the power consumption of a system around i.mx53. I've found an application note from Freescale which is based on some use cases:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://cache.freescale.com/files/32bit/doc/app_note/AN4270.pdf"&gt;http://cache.freescale.com/files/32bit/doc/app_note/AN4270.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm particularly interested in the "Stop mode". According to the numbers given in the application note in this mode the DDR3 is operational and consumes 32mW out of a total of 36.5 mW.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Looking at the kernel sources this mode should put DDR3 in self-refresh mode and suspend itself into the internal RAM. In such a case I would expect a much lower power consumption for DDR3.&lt;/P&gt;&lt;P&gt;However those number are given for the Ubuntu image. Are they applicable also to the LTIB build ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank, Marko&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 20 Feb 2012 08:31:26 GMT</pubDate>
    <dc:creator>MarkoPanger</dc:creator>
    <dc:date>2012-02-20T08:31:26Z</dc:date>
    <item>
      <title>Power consumption (AN4270)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Power-consumption-AN4270/m-p/212513#M13016</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear all,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm trying to evaluate the power consumption of a system around i.mx53. I've found an application note from Freescale which is based on some use cases:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://cache.freescale.com/files/32bit/doc/app_note/AN4270.pdf"&gt;http://cache.freescale.com/files/32bit/doc/app_note/AN4270.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm particularly interested in the "Stop mode". According to the numbers given in the application note in this mode the DDR3 is operational and consumes 32mW out of a total of 36.5 mW.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Looking at the kernel sources this mode should put DDR3 in self-refresh mode and suspend itself into the internal RAM. In such a case I would expect a much lower power consumption for DDR3.&lt;/P&gt;&lt;P&gt;However those number are given for the Ubuntu image. Are they applicable also to the LTIB build ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank, Marko&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 20 Feb 2012 08:31:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Power-consumption-AN4270/m-p/212513#M13016</guid>
      <dc:creator>MarkoPanger</dc:creator>
      <dc:date>2012-02-20T08:31:26Z</dc:date>
    </item>
  </channel>
</rss>