<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Programming bootloader i.MX6UL in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Programming-bootloader-i-MX6UL/m-p/849613#M130010</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Olli&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;i.MX6UL has ROM (it can not be reflashed by user) which is used for booting&lt;/P&gt;&lt;P&gt;and described in Chapter 8 System Boot i.MX6UL Reference Manual &lt;/P&gt;&lt;P&gt;&lt;A href="http://www.nxp.com/docs/en/reference-manual/IMX6ULRM.pdf"&gt;http://www.nxp.com/docs/en/reference-manual/IMX6ULRM.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Additional bootloaders, like uboot can be flashed to external boot devices like emmc, nand, e.t.c.&lt;/P&gt;&lt;P&gt;Procedures are described in documentation provided on link&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://www.nxp.com/support/developer-resources/run-time-software/i.mx-developer-resources/i.mx-6series-i.mx-7series-software-and-development-tool-resources:IMX_SW" title="https://www.nxp.com/support/developer-resources/run-time-software/i.mx-developer-resources/i.mx-6series-i.mx-7series-software-and-development-tool-resources:IMX_SW"&gt;i.MX Software|NXP&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 09 Jul 2018 23:29:04 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2018-07-09T23:29:04Z</dc:date>
    <item>
      <title>Programming bootloader i.MX6UL</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Programming-bootloader-i-MX6UL/m-p/849612#M130009</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;This sounds like a very silly question but I just can't find the correct piece of documentation.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;How do you actually flash the bootloader? Do you flash the bootloader? The only hit for a programmer I could find is for some kind of linux-based programmer that appears to use USB and is for the firmware, not bootloader. I presume that'd also require you're running approved software on the i.MX6 design?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;..&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm looking at using the i.Mx6 in our remote monitoring product, my some other options are Sitara and Renesans processors which have roughly similar capabilities. Personally I usually use microcontrollers&amp;nbsp;which don't have an OS, so..&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 04 Jul 2018 16:55:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Programming-bootloader-i-MX6UL/m-p/849612#M130009</guid>
      <dc:creator>olli_mannisto</dc:creator>
      <dc:date>2018-07-04T16:55:59Z</dc:date>
    </item>
    <item>
      <title>Re: Programming bootloader i.MX6UL</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Programming-bootloader-i-MX6UL/m-p/849613#M130010</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Olli&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;i.MX6UL has ROM (it can not be reflashed by user) which is used for booting&lt;/P&gt;&lt;P&gt;and described in Chapter 8 System Boot i.MX6UL Reference Manual &lt;/P&gt;&lt;P&gt;&lt;A href="http://www.nxp.com/docs/en/reference-manual/IMX6ULRM.pdf"&gt;http://www.nxp.com/docs/en/reference-manual/IMX6ULRM.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Additional bootloaders, like uboot can be flashed to external boot devices like emmc, nand, e.t.c.&lt;/P&gt;&lt;P&gt;Procedures are described in documentation provided on link&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://www.nxp.com/support/developer-resources/run-time-software/i.mx-developer-resources/i.mx-6series-i.mx-7series-software-and-development-tool-resources:IMX_SW" title="https://www.nxp.com/support/developer-resources/run-time-software/i.mx-developer-resources/i.mx-6series-i.mx-7series-software-and-development-tool-resources:IMX_SW"&gt;i.MX Software|NXP&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 09 Jul 2018 23:29:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Programming-bootloader-i-MX6UL/m-p/849613#M130010</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2018-07-09T23:29:04Z</dc:date>
    </item>
  </channel>
</rss>