<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックI.MX7 boot failed</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/I-MX7-boot-failed/m-p/849327#M129977</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi All:&lt;/P&gt;&lt;P&gt;My u-boot version is 2016-03&amp;nbsp;and&amp;nbsp;kernel version is 4.9，&lt;/P&gt;&lt;P&gt;and my bootargs was setting as below:&lt;/P&gt;&lt;P&gt;setenv bootargs console=ttymxc0,115200 root=/dev/mmcblk0p2 rootwait ro earlyprintk&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;but the boot process was failed after cpu0&amp;nbsp;&amp;nbsp;Setting up static identity map.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;should I have modified somewhere in my u-boot 2016-03?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;the log as below:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kernel image @ 0x80800000 [ 0x000000 - 0x7d8348 ]&lt;BR /&gt;## Flattened Device Tree blob at 83000000&lt;BR /&gt; Booting using the fdt blob at 0x83000000&lt;BR /&gt; Using Device Tree in place at 83000000, end 8300e618&lt;/P&gt;&lt;P&gt;Starting kernel ...&lt;/P&gt;&lt;P&gt;Uncompressing Linux... done, booting the kernel.&lt;BR /&gt;Booting Linux on physical CPU 0x0&lt;BR /&gt;Linux version 4.9.107-04778-gd590654-dirty (root@harry-workstation) (gcc version 4.9.2 ( 4.9.2-10) ) #38 SMP PREEMPT Wed Jul 4 15:10:53 CST 2018&lt;BR /&gt;CPU: ARMv7 Processor [410fc075] revision 5 (ARMv7), cr=10c53c7d&lt;BR /&gt;CPU: div instructions available: patching division code&lt;BR /&gt;CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache&lt;BR /&gt;OF: fdt:Machine model: Freescale i.MX7 SabreSD Board&lt;BR /&gt;bootconsole [earlycon0] enabled&lt;BR /&gt;Reserved memory: created CMA memory pool at 0xdc000000, size 320 MiB&lt;BR /&gt;OF: reserved mem: initialized node linux,cma, compatible id shared-dma-pool&lt;BR /&gt;Memory policy: Data cache writealloc&lt;BR /&gt;psci: probing for conduit method from DT.&lt;BR /&gt;psci: Using PSCI v0.1 Function IDs from DT&lt;BR /&gt;percpu: Embedded 14 pages/cpu @daf1a000 s26048 r8192 d23104 u57344&lt;BR /&gt;Built 1 zonelists in Zone order, mobility grouping on. Total pages: 520703&lt;BR /&gt;Kernel command line: console=ttymxc0,115200 root=/dev/mmcblk0p2 rootwait ro earlyprintk&lt;BR /&gt;PID hash table entries: 4096 (order: 2, 16384 bytes)&lt;BR /&gt;Dentry cache hash table entries: 262144 (order: 8, 1048576 bytes)&lt;BR /&gt;Inode-cache hash table entries: 131072 (order: 7, 524288 bytes)&lt;BR /&gt;Memory: 1734160K/2097148K available (10240K kernel code, 551K rwdata, 3424K rodata, 1024K init, 476K bss, 35308K reserved, 327680K cma-reserved, 262140K highmem)&lt;BR /&gt;Virtual kernel memory layout:&lt;BR /&gt; vector : 0xffff0000 - 0xffff1000 ( 4 kB)&lt;BR /&gt; fixmap : 0xffc00000 - 0xfff00000 (3072 kB)&lt;BR /&gt; vmalloc : 0xf0800000 - 0xff800000 ( 240 MB)&lt;BR /&gt; lowmem : 0x80000000 - 0xf0000000 (1792 MB)&lt;BR /&gt; pkmap : 0x7fe00000 - 0x80000000 ( 2 MB)&lt;BR /&gt; modules : 0x7f000000 - 0x7fe00000 ( 14 MB)&lt;BR /&gt; .text : 0x80008000 - 0x80b00000 (11232 kB)&lt;BR /&gt; .init : 0x80f00000 - 0x81000000 (1024 kB)&lt;BR /&gt; .data : 0x81000000 - 0x81089ea0 ( 552 kB)&lt;BR /&gt; .bss : 0x8108b000 - 0x811020c8 ( 477 kB)&lt;BR /&gt;SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=2, Nodes=1&lt;BR /&gt;Preemptible hierarchical RCU implementation.&lt;BR /&gt; Build-time adjustment of leaf fanout to 32.&lt;BR /&gt; RCU restricting CPUs from NR_CPUS=4 to nr_cpu_ids=2.&lt;BR /&gt;RCU: Adjusting geometry for rcu_fanout_leaf=32, nr_cpu_ids=2&lt;BR /&gt;NR_IRQS:16 nr_irqs:16 16&lt;BR /&gt;arm_arch_timer: Architected cp15 timer(s) running at 8.00MHz (phys).&lt;BR /&gt;clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x1d854df40, max_idle_ns: 440795202120 ns&lt;/P&gt;&lt;P&gt;sched_clock: 56 bits at 8MHz, resolution 125ns, wraps every 2199023255500ns&lt;BR /&gt;Switching to timer-based delay loop, resolution 125ns&lt;BR /&gt;Ignoring duplicate/late registration of read_current_timer delay&lt;BR /&gt;clocksource: mxc_timer1: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 637086815595 ns&lt;BR /&gt;Console: colour dummy device 80x30&lt;BR /&gt;Calibrating delay loop (skipped), value calculated using timer frequency.. 16.00 BogoMIPS (lpj=80000)&lt;BR /&gt;pid_max: default: 32768 minimum: 301&lt;BR /&gt;Mount-cache hash table entries: 4096 (order: 2, 16384 bytes)&lt;BR /&gt;Mountpoint-cache hash table entries: 4096 (order: 2, 16384 bytes)&lt;BR /&gt;CPU: Testing write buffer coherency: ok&lt;BR /&gt;CPU0: update cpu_capacity 1024&lt;BR /&gt;CPU0: thread -1, cpu 0, socket 0, mpidr 80000000&lt;BR /&gt;Setting up static identity map for 0x80100000 - 0x80100058&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;my u-boot env as below:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;baudrate=115200 [3/1956]&lt;BR /&gt;biosver=1.0.0S01&lt;BR /&gt;boot_fdt=try&lt;BR /&gt;bootcmd=mmc dev ${mmcdev};mmc dev ${mmcdev}; if mmc rescan; then if run loadbootscript; then run bootscript; else if run loadimage; then run mmcboot; else run netboot; fi;$&lt;BR /&gt;bootcmd_mfg=run mfgtool_args;bootz ${loadaddr} ${initrd_addr} ${fdt_addr};&lt;BR /&gt;bootdelay=3&lt;BR /&gt;bootscript=echo Running bootscript from mmc ...; source&lt;BR /&gt;console=ttymxc0&lt;BR /&gt;dfu_alt_info=image raw 0 0x800000;u-boot raw 0 0x4000;bootimg part 0 1;rootfs part 0 2&lt;BR /&gt;eth1addr=00:90:e8:33:55:42&lt;BR /&gt;ethact=FEC0&lt;BR /&gt;ethaddr=00:90:e8:33:55:41&lt;BR /&gt;ethprime=FEC&lt;BR /&gt;fastboot=0&lt;BR /&gt;fdt_addr=0x83000000&lt;BR /&gt;fdt_file=imx7d-sdb.dtb&lt;BR /&gt;fdt_high=0xffffffff&lt;BR /&gt;ifname=0&lt;BR /&gt;image=zImage&lt;BR /&gt;initrd_addr=0x83800000&lt;BR /&gt;initrd_high=0xffffffff&lt;BR /&gt;ip_dyn=yes&lt;BR /&gt;ipaddr=10.144.4.179&lt;BR /&gt;loadaddr=0x80800000&lt;BR /&gt;loadbootscript=fatload mmc ${mmcdev}:${mmcpart} ${loadaddr} ${script};&lt;BR /&gt;loadfdt=fatload mmc ${mmcdev}:${mmcpart} ${fdt_addr} ${fdt_file}&lt;BR /&gt;loadimage=fatload mmc ${mmcdev}:${mmcpart} ${loadaddr} ${image}&lt;BR /&gt;mfgtool_args=setenv bootargs console=${console},${baudrate} rdinit=/linuxrc g_mass_storage.stall=0 g_mass_storage.removable=1 g_mass_storage.idVendor=0x066F g_mass_storage&lt;BR /&gt;mmcargs=setenv bootargs console=${console},${baudrate} root=${mmcroot}&lt;BR /&gt;mmcautodetect=yes&lt;BR /&gt;mmcboot=echo Booting from mmc ...; run mmcargs; if test ${boot_fdt} = yes || test ${boot_fdt} = try; then if run loadfdt; then bootz ${loadaddr} - ${fdt_addr}; else if tes;&lt;BR /&gt;mmcdev=0&lt;BR /&gt;mmcpart=1&lt;BR /&gt;mmcroot=/dev/mmcblk0p2 rootwait rw&lt;BR /&gt;netargs=setenv bootargs console=${console},${baudrate} root=/dev/nfs ip=dhcp nfsroot=${serverip}:${nfsroot},v3,tcp&lt;BR /&gt;netboot=echo Booting from net ...; run netargs; if test ${ip_dyn} = yes; then setenv get_cmd dhcp; else setenv get_cmd tftp; fi; ${get_cmd} ${image}; if test ${boot_fdt} =;&lt;BR /&gt;robust=0&lt;BR /&gt;script=boot.scr&lt;BR /&gt;serverip=10.144.4.180&lt;BR /&gt;stderr=serial&lt;BR /&gt;stdin=serial&lt;BR /&gt;stdout=serial&lt;BR /&gt;videomode=video=ctfb:x:480,y:272,depth:24,pclk:108695,le:8,ri:4,up:2,lo:4,hs:41,vs:10,sync:0,vmode:0&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 04 Jul 2018 13:03:38 GMT</pubDate>
    <dc:creator>kennithhsu</dc:creator>
    <dc:date>2018-07-04T13:03:38Z</dc:date>
    <item>
      <title>I.MX7 boot failed</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/I-MX7-boot-failed/m-p/849327#M129977</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi All:&lt;/P&gt;&lt;P&gt;My u-boot version is 2016-03&amp;nbsp;and&amp;nbsp;kernel version is 4.9，&lt;/P&gt;&lt;P&gt;and my bootargs was setting as below:&lt;/P&gt;&lt;P&gt;setenv bootargs console=ttymxc0,115200 root=/dev/mmcblk0p2 rootwait ro earlyprintk&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;but the boot process was failed after cpu0&amp;nbsp;&amp;nbsp;Setting up static identity map.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;should I have modified somewhere in my u-boot 2016-03?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;the log as below:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kernel image @ 0x80800000 [ 0x000000 - 0x7d8348 ]&lt;BR /&gt;## Flattened Device Tree blob at 83000000&lt;BR /&gt; Booting using the fdt blob at 0x83000000&lt;BR /&gt; Using Device Tree in place at 83000000, end 8300e618&lt;/P&gt;&lt;P&gt;Starting kernel ...&lt;/P&gt;&lt;P&gt;Uncompressing Linux... done, booting the kernel.&lt;BR /&gt;Booting Linux on physical CPU 0x0&lt;BR /&gt;Linux version 4.9.107-04778-gd590654-dirty (root@harry-workstation) (gcc version 4.9.2 ( 4.9.2-10) ) #38 SMP PREEMPT Wed Jul 4 15:10:53 CST 2018&lt;BR /&gt;CPU: ARMv7 Processor [410fc075] revision 5 (ARMv7), cr=10c53c7d&lt;BR /&gt;CPU: div instructions available: patching division code&lt;BR /&gt;CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache&lt;BR /&gt;OF: fdt:Machine model: Freescale i.MX7 SabreSD Board&lt;BR /&gt;bootconsole [earlycon0] enabled&lt;BR /&gt;Reserved memory: created CMA memory pool at 0xdc000000, size 320 MiB&lt;BR /&gt;OF: reserved mem: initialized node linux,cma, compatible id shared-dma-pool&lt;BR /&gt;Memory policy: Data cache writealloc&lt;BR /&gt;psci: probing for conduit method from DT.&lt;BR /&gt;psci: Using PSCI v0.1 Function IDs from DT&lt;BR /&gt;percpu: Embedded 14 pages/cpu @daf1a000 s26048 r8192 d23104 u57344&lt;BR /&gt;Built 1 zonelists in Zone order, mobility grouping on. Total pages: 520703&lt;BR /&gt;Kernel command line: console=ttymxc0,115200 root=/dev/mmcblk0p2 rootwait ro earlyprintk&lt;BR /&gt;PID hash table entries: 4096 (order: 2, 16384 bytes)&lt;BR /&gt;Dentry cache hash table entries: 262144 (order: 8, 1048576 bytes)&lt;BR /&gt;Inode-cache hash table entries: 131072 (order: 7, 524288 bytes)&lt;BR /&gt;Memory: 1734160K/2097148K available (10240K kernel code, 551K rwdata, 3424K rodata, 1024K init, 476K bss, 35308K reserved, 327680K cma-reserved, 262140K highmem)&lt;BR /&gt;Virtual kernel memory layout:&lt;BR /&gt; vector : 0xffff0000 - 0xffff1000 ( 4 kB)&lt;BR /&gt; fixmap : 0xffc00000 - 0xfff00000 (3072 kB)&lt;BR /&gt; vmalloc : 0xf0800000 - 0xff800000 ( 240 MB)&lt;BR /&gt; lowmem : 0x80000000 - 0xf0000000 (1792 MB)&lt;BR /&gt; pkmap : 0x7fe00000 - 0x80000000 ( 2 MB)&lt;BR /&gt; modules : 0x7f000000 - 0x7fe00000 ( 14 MB)&lt;BR /&gt; .text : 0x80008000 - 0x80b00000 (11232 kB)&lt;BR /&gt; .init : 0x80f00000 - 0x81000000 (1024 kB)&lt;BR /&gt; .data : 0x81000000 - 0x81089ea0 ( 552 kB)&lt;BR /&gt; .bss : 0x8108b000 - 0x811020c8 ( 477 kB)&lt;BR /&gt;SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=2, Nodes=1&lt;BR /&gt;Preemptible hierarchical RCU implementation.&lt;BR /&gt; Build-time adjustment of leaf fanout to 32.&lt;BR /&gt; RCU restricting CPUs from NR_CPUS=4 to nr_cpu_ids=2.&lt;BR /&gt;RCU: Adjusting geometry for rcu_fanout_leaf=32, nr_cpu_ids=2&lt;BR /&gt;NR_IRQS:16 nr_irqs:16 16&lt;BR /&gt;arm_arch_timer: Architected cp15 timer(s) running at 8.00MHz (phys).&lt;BR /&gt;clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x1d854df40, max_idle_ns: 440795202120 ns&lt;/P&gt;&lt;P&gt;sched_clock: 56 bits at 8MHz, resolution 125ns, wraps every 2199023255500ns&lt;BR /&gt;Switching to timer-based delay loop, resolution 125ns&lt;BR /&gt;Ignoring duplicate/late registration of read_current_timer delay&lt;BR /&gt;clocksource: mxc_timer1: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 637086815595 ns&lt;BR /&gt;Console: colour dummy device 80x30&lt;BR /&gt;Calibrating delay loop (skipped), value calculated using timer frequency.. 16.00 BogoMIPS (lpj=80000)&lt;BR /&gt;pid_max: default: 32768 minimum: 301&lt;BR /&gt;Mount-cache hash table entries: 4096 (order: 2, 16384 bytes)&lt;BR /&gt;Mountpoint-cache hash table entries: 4096 (order: 2, 16384 bytes)&lt;BR /&gt;CPU: Testing write buffer coherency: ok&lt;BR /&gt;CPU0: update cpu_capacity 1024&lt;BR /&gt;CPU0: thread -1, cpu 0, socket 0, mpidr 80000000&lt;BR /&gt;Setting up static identity map for 0x80100000 - 0x80100058&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;my u-boot env as below:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;baudrate=115200 [3/1956]&lt;BR /&gt;biosver=1.0.0S01&lt;BR /&gt;boot_fdt=try&lt;BR /&gt;bootcmd=mmc dev ${mmcdev};mmc dev ${mmcdev}; if mmc rescan; then if run loadbootscript; then run bootscript; else if run loadimage; then run mmcboot; else run netboot; fi;$&lt;BR /&gt;bootcmd_mfg=run mfgtool_args;bootz ${loadaddr} ${initrd_addr} ${fdt_addr};&lt;BR /&gt;bootdelay=3&lt;BR /&gt;bootscript=echo Running bootscript from mmc ...; source&lt;BR /&gt;console=ttymxc0&lt;BR /&gt;dfu_alt_info=image raw 0 0x800000;u-boot raw 0 0x4000;bootimg part 0 1;rootfs part 0 2&lt;BR /&gt;eth1addr=00:90:e8:33:55:42&lt;BR /&gt;ethact=FEC0&lt;BR /&gt;ethaddr=00:90:e8:33:55:41&lt;BR /&gt;ethprime=FEC&lt;BR /&gt;fastboot=0&lt;BR /&gt;fdt_addr=0x83000000&lt;BR /&gt;fdt_file=imx7d-sdb.dtb&lt;BR /&gt;fdt_high=0xffffffff&lt;BR /&gt;ifname=0&lt;BR /&gt;image=zImage&lt;BR /&gt;initrd_addr=0x83800000&lt;BR /&gt;initrd_high=0xffffffff&lt;BR /&gt;ip_dyn=yes&lt;BR /&gt;ipaddr=10.144.4.179&lt;BR /&gt;loadaddr=0x80800000&lt;BR /&gt;loadbootscript=fatload mmc ${mmcdev}:${mmcpart} ${loadaddr} ${script};&lt;BR /&gt;loadfdt=fatload mmc ${mmcdev}:${mmcpart} ${fdt_addr} ${fdt_file}&lt;BR /&gt;loadimage=fatload mmc ${mmcdev}:${mmcpart} ${loadaddr} ${image}&lt;BR /&gt;mfgtool_args=setenv bootargs console=${console},${baudrate} rdinit=/linuxrc g_mass_storage.stall=0 g_mass_storage.removable=1 g_mass_storage.idVendor=0x066F g_mass_storage&lt;BR /&gt;mmcargs=setenv bootargs console=${console},${baudrate} root=${mmcroot}&lt;BR /&gt;mmcautodetect=yes&lt;BR /&gt;mmcboot=echo Booting from mmc ...; run mmcargs; if test ${boot_fdt} = yes || test ${boot_fdt} = try; then if run loadfdt; then bootz ${loadaddr} - ${fdt_addr}; else if tes;&lt;BR /&gt;mmcdev=0&lt;BR /&gt;mmcpart=1&lt;BR /&gt;mmcroot=/dev/mmcblk0p2 rootwait rw&lt;BR /&gt;netargs=setenv bootargs console=${console},${baudrate} root=/dev/nfs ip=dhcp nfsroot=${serverip}:${nfsroot},v3,tcp&lt;BR /&gt;netboot=echo Booting from net ...; run netargs; if test ${ip_dyn} = yes; then setenv get_cmd dhcp; else setenv get_cmd tftp; fi; ${get_cmd} ${image}; if test ${boot_fdt} =;&lt;BR /&gt;robust=0&lt;BR /&gt;script=boot.scr&lt;BR /&gt;serverip=10.144.4.180&lt;BR /&gt;stderr=serial&lt;BR /&gt;stdin=serial&lt;BR /&gt;stdout=serial&lt;BR /&gt;videomode=video=ctfb:x:480,y:272,depth:24,pclk:108695,le:8,ri:4,up:2,lo:4,hs:41,vs:10,sync:0,vmode:0&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 04 Jul 2018 13:03:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/I-MX7-boot-failed/m-p/849327#M129977</guid>
      <dc:creator>kennithhsu</dc:creator>
      <dc:date>2018-07-04T13:03:38Z</dc:date>
    </item>
    <item>
      <title>Re: I.MX7 boot failed</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/I-MX7-boot-failed/m-p/849328#M129978</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Kennith&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;what bsp used in the case, please try nxp releases described on&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=https%3A%2F%2Fwww.nxp.com%2Fsupport%2Fdeveloper-resources%2Frun-time-software%2Fi.mx-developer-resources%2Fi.mx-6series-i.mx-7series-software-and-development-tool-resources%3AIMX_SW" rel="nofollow" target="_blank"&gt;https://www.nxp.com/support/developer-resources/run-time-software/i.mx-developer-resources/i.mx-6series-i.mx-7series-software-and-development-tool-resources:IMX_SW&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://source.codeaurora.org/external/imx/linux-imx/tree/?h=imx_4.1.15_2.0.0_ga" title="https://source.codeaurora.org/external/imx/linux-imx/tree/?h=imx_4.1.15_2.0.0_ga"&gt;linux-imx - i.MX Linux kernel&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 09 Jul 2018 23:22:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/I-MX7-boot-failed/m-p/849328#M129978</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2018-07-09T23:22:44Z</dc:date>
    </item>
  </channel>
</rss>