<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Time shift after resume</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Time-shift-after-resume/m-p/849078#M129957</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm using iMX6ULL Board. I have two instances of the same device, both are connected as IIO devices.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;These two devices produce ADC ready interrupts. Normally, it follows a difference of 5ms between the devices.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But, each time when the devices wake up from suspend mode 5ms is increased by 100usec.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What's the reason for this timeshift?&lt;/P&gt;&lt;P&gt;How to avoid it or maintain 5ms difference?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 11 Oct 2018 04:42:25 GMT</pubDate>
    <dc:creator>mathew_k_t</dc:creator>
    <dc:date>2018-10-11T04:42:25Z</dc:date>
    <item>
      <title>Time shift after resume</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Time-shift-after-resume/m-p/849078#M129957</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm using iMX6ULL Board. I have two instances of the same device, both are connected as IIO devices.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;These two devices produce ADC ready interrupts. Normally, it follows a difference of 5ms between the devices.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But, each time when the devices wake up from suspend mode 5ms is increased by 100usec.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What's the reason for this timeshift?&lt;/P&gt;&lt;P&gt;How to avoid it or maintain 5ms difference?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 11 Oct 2018 04:42:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Time-shift-after-resume/m-p/849078#M129957</guid>
      <dc:creator>mathew_k_t</dc:creator>
      <dc:date>2018-10-11T04:42:25Z</dc:date>
    </item>
  </channel>
</rss>