<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Android Oreo compilation Problem</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Android-Oreo-compilation-Problem/m-p/848906#M129932</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Just to let register the solution:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In my environment, I had an older version of make_ext4fs at /usr/bin which was confusing the build - as it was not using the properly binary on out/host/linux-x86/bin - so, make sure you're using the properly version of the tools in order to get the build done.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I figure it out&amp;nbsp;looking at build log and right&amp;nbsp;after reducing the build to only one job (make -j1) - when I could see that the&amp;nbsp;make_ext4fs was failing.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 09 Apr 2019 20:06:28 GMT</pubDate>
    <dc:creator>nilson_oliveira</dc:creator>
    <dc:date>2019-04-09T20:06:28Z</dc:date>
    <item>
      <title>Android Oreo compilation Problem</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Android-Oreo-compilation-Problem/m-p/848899#M129925</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;PLATFORM_VERSION_CODENAME=REL&lt;BR /&gt;PLATFORM_VERSION=8.0.0&lt;BR /&gt;TARGET_PRODUCT=aosp_arm&lt;BR /&gt;TARGET_BUILD_VARIANT=eng&lt;BR /&gt;TARGET_BUILD_TYPE=release&lt;BR /&gt;TARGET_ARCH=arm&lt;BR /&gt;TARGET_ARCH_VARIANT=armv7-a&lt;BR /&gt;TARGET_CPU_VARIANT=generic&lt;BR /&gt;HOST_ARCH=x86_64&lt;BR /&gt;HOST_2ND_ARCH=x86&lt;BR /&gt;HOST_OS=linux&lt;BR /&gt;HOST_OS_EXTRA=Linux-4.4.0-131-generic-x86_64-with-Ubuntu-16.04-xenial&lt;BR /&gt;HOST_CROSS_OS=windows&lt;BR /&gt;HOST_CROSS_ARCH=x86&lt;BR /&gt;HOST_CROSS_2ND_ARCH=x86_64&lt;BR /&gt;HOST_BUILD_TYPE=release&lt;BR /&gt;BUILD_ID=OPD1.170816.018&lt;BR /&gt;OUT_DIR=out&lt;BR /&gt;============================================&lt;BR /&gt;[1/2] out/soong/.bootstrap/bin/minibp out/soong/.minibootstrap/build.ninja.in&lt;BR /&gt;[2/2] bootstrap out/soong/.minibootstrap/build.ninja.in&lt;BR /&gt;[1/2] out/soong/.bootstrap/bin/minibp out/soong/.minibootstrap/build.ninja.in&lt;BR /&gt;ninja: no work to do.&lt;BR /&gt;ninja: no work to do.&lt;BR /&gt;build/core/main.mk:21: recipe for target 'run_soong_ui' failed&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 25 Jul 2018 06:20:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Android-Oreo-compilation-Problem/m-p/848899#M129925</guid>
      <dc:creator>pavandornadula7</dc:creator>
      <dc:date>2018-07-25T06:20:40Z</dc:date>
    </item>
    <item>
      <title>Re: Android Oreo compilation Problem</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Android-Oreo-compilation-Problem/m-p/848900#M129926</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Pavan Kumar,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I see that this thread was duplicated so I will delete the duplicated thread and you can follow up in this thread, if that’s okay with you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;From the log you shared it looks like you are not building for an i.MX board. Would you please let us know which i.MX board you want to build for? You would need to set the board to use using the lunch command and it should apprar in “TARGET_PRODUCT”.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As of right now your settings are for the aosp_arm, which, if I’m correct is a simple android build for development meant to be used with emulators. We do not support builds different than those listed on the i.MX Android BSP documentation.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I will be looking forward to hearing back from you!&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 25 Jul 2018 22:05:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Android-Oreo-compilation-Problem/m-p/848900#M129926</guid>
      <dc:creator>gusarambula</dc:creator>
      <dc:date>2018-07-25T22:05:09Z</dc:date>
    </item>
    <item>
      <title>Re: Android Oreo compilation Problem</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Android-Oreo-compilation-Problem/m-p/848901#M129927</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;dornadula.pavankumar@sysadmin-Vostro-470:~$ make&lt;BR /&gt;============================================&lt;BR /&gt;PLATFORM_VERSION_CODENAME=REL&lt;BR /&gt;PLATFORM_VERSION=8.0.0&lt;BR /&gt;TARGET_PRODUCT=aosp_arm&lt;BR /&gt;TARGET_BUILD_VARIANT=eng&lt;BR /&gt;TARGET_BUILD_TYPE=release&lt;BR /&gt;TARGET_ARCH=arm&lt;BR /&gt;TARGET_ARCH_VARIANT=armv7-a&lt;BR /&gt;TARGET_CPU_VARIANT=generic&lt;BR /&gt;HOST_ARCH=x86_64&lt;BR /&gt;HOST_2ND_ARCH=x86&lt;BR /&gt;HOST_OS=linux&lt;BR /&gt;HOST_OS_EXTRA=Linux-4.4.0-131-generic-x86_64-with-Ubuntu-16.04-xenial&lt;BR /&gt;HOST_CROSS_OS=windows&lt;BR /&gt;HOST_CROSS_ARCH=x86&lt;BR /&gt;HOST_CROSS_2ND_ARCH=x86_64&lt;BR /&gt;HOST_BUILD_TYPE=release&lt;BR /&gt;BUILD_ID=OPD1.170816.018&lt;BR /&gt;OUT_DIR=out&lt;BR /&gt;============================================&lt;BR /&gt;[2/2] bootstrap out/soong/.minibootstrap/build.ninja.in&lt;BR /&gt;[2/2] bootstrap out/soong/.minibootstrap/build.ninja.in&lt;BR /&gt;ninja: no work to do.&lt;BR /&gt;[1/1] out/soong/.bootstrap/bin/soong_build out/soong/build.ninja&lt;BR /&gt;FAILED: out/soong/build.ninja&lt;BR /&gt;out/soong/.bootstrap/bin/soong_build -t -b out/soong -d out/soong/build.ninja.d -o out/soong/build.ninja Android.bp&lt;BR /&gt;error: frameworks/av/media/libstagefright/Android.bp:7:1: module "libstagefright" variant "android_arm_armv7-a_shared_core": source path vendor/nxp/fsl-codec/ghdr/common does not exist&lt;BR /&gt;ninja: build stopped: subcommand failed.&lt;BR /&gt;09:28:16 soong failed with: exit status 1&lt;BR /&gt;build/core/main.mk:21: recipe for target 'run_soong_ui' failed&lt;BR /&gt;make: *** [run_soong_ui] Error 1&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Steps :&amp;nbsp;$ source build/envsetup.sh&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;&amp;nbsp;$ lunch sabresd_6dq-userdebug&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;$ make&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Pavan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 26 Jul 2018 03:59:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Android-Oreo-compilation-Problem/m-p/848901#M129927</guid>
      <dc:creator>pavandornadula7</dc:creator>
      <dc:date>2018-07-26T03:59:52Z</dc:date>
    </item>
    <item>
      <title>Re: Android Oreo compilation Problem</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Android-Oreo-compilation-Problem/m-p/848902#M129928</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Where is thread and where i need to start to build oreo for my sabresd board . i am following android oreo user guide .&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Pavan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 26 Jul 2018 04:02:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Android-Oreo-compilation-Problem/m-p/848902#M129928</guid>
      <dc:creator>pavandornadula7</dc:creator>
      <dc:date>2018-07-26T04:02:39Z</dc:date>
    </item>
    <item>
      <title>Re: Android Oreo compilation Problem</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Android-Oreo-compilation-Problem/m-p/848903#M129929</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello &lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/gusarambula"&gt;gusarambula&lt;/A&gt;,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Even I'm getting the similar issue for &lt;STRONG&gt;sabresd_6dq&lt;/STRONG&gt; target board while compiling the fresh code.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;============================================&lt;BR /&gt;PLATFORM_VERSION_CODENAME=REL&lt;BR /&gt;PLATFORM_VERSION=8.0.0&lt;BR /&gt;TARGET_PRODUCT=sabresd_6dq&lt;BR /&gt;TARGET_BUILD_VARIANT=userdebug&lt;BR /&gt;TARGET_BUILD_TYPE=release&lt;BR /&gt;TARGET_ARCH=arm&lt;BR /&gt;TARGET_ARCH_VARIANT=armv7-a-neon&lt;BR /&gt;TARGET_CPU_VARIANT=cortex-a9&lt;BR /&gt;HOST_ARCH=x86_64&lt;BR /&gt;HOST_2ND_ARCH=x86&lt;BR /&gt;HOST_OS=linux&lt;BR /&gt;HOST_OS_EXTRA=Linux-4.4.0-31-generic-x86_64-with-Ubuntu-16.04-xenial&lt;BR /&gt;HOST_CROSS_OS=windows&lt;BR /&gt;HOST_CROSS_ARCH=x86&lt;BR /&gt;HOST_CROSS_2ND_ARCH=x86_64&lt;BR /&gt;HOST_BUILD_TYPE=release&lt;BR /&gt;BUILD_ID=1.0.0-rfp-rc4&lt;BR /&gt;OUT_DIR=out&lt;BR /&gt;============================================&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;------&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;------&lt;/P&gt;&lt;P&gt;LD drivers/video/built-in.o&lt;BR /&gt; LD drivers/built-in.o&lt;BR /&gt; CC lib/efi_loader/helloworld.o&lt;BR /&gt; LD drivers/usb/gadget/built-in.o&lt;BR /&gt; LD lib/efi_loader/helloworld.so&lt;BR /&gt; OBJCOPY lib/efi_loader/helloworld.efi&lt;BR /&gt; CC lib/smbios.o&lt;BR /&gt; CC lib/display_options.o&lt;BR /&gt; LD lib/built-in.o&lt;BR /&gt; LD u-boot&lt;BR /&gt; OBJCOPY u-boot-nodtb.bin&lt;BR /&gt; OBJCOPY u-boot.srec&lt;BR /&gt; SYM u-boot.sym&lt;BR /&gt; CAT u-boot-dtb.bin&lt;BR /&gt; COPY u-boot.bin&lt;BR /&gt; MKIMAGE u-boot-dtb.imx&lt;BR /&gt; CFGCHK u-boot.cfg&lt;BR /&gt;make[1]: Leaving directory '/home/shreejith/android_build/out/target/product/sabresd_6dq/obj/BOOTLOADER_OBJ'&lt;BR /&gt;make: Leaving directory '/home/shreejith/android_build/vendor/nxp-opensource/uboot-imx'&lt;BR /&gt;/bin/bash: line 0: [: =: unary operator expected&lt;BR /&gt;ninja: build stopped: subcommand failed.&lt;BR /&gt;11:18:25 ninja failed with: exit status 1&lt;BR /&gt;build/core/main.mk:21: recipe for target 'run_soong_ui' failed&lt;BR /&gt;make: *** [run_soong_ui] Error 1&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please help me out to solve the problem.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Shreejith&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 20 Sep 2018 05:52:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Android-Oreo-compilation-Problem/m-p/848903#M129929</guid>
      <dc:creator>shreejith_nekka</dc:creator>
      <dc:date>2018-09-20T05:52:44Z</dc:date>
    </item>
    <item>
      <title>Re: Android Oreo compilation Problem</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Android-Oreo-compilation-Problem/m-p/848904#M129930</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Pavan,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;A quick and dirty working solution:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;PRE class="language-none line-numbers"&gt;&lt;CODE&gt;$ cp -r vendor/nxp/* android_build/vendor/nxp‍‍‍‍‍&lt;SPAN class="line-numbers-rows"&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/CODE&gt;&lt;/PRE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Then run make again&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Maro&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 08 Oct 2018 08:45:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Android-Oreo-compilation-Problem/m-p/848904#M129930</guid>
      <dc:creator>marouene_boubakri</dc:creator>
      <dc:date>2018-10-08T08:45:59Z</dc:date>
    </item>
    <item>
      <title>Re: Android Oreo compilation Problem</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Android-Oreo-compilation-Problem/m-p/848905#M129931</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, I've tried to do quick&amp;amp;dirty solution but it still gives me 'run_soong_ui' error on my var_mx6&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;============================================&lt;BR /&gt;PLATFORM_VERSION_CODENAME=REL&lt;BR /&gt;PLATFORM_VERSION=8.0.0&lt;BR /&gt;TARGET_PRODUCT=var_mx6&lt;BR /&gt;TARGET_BUILD_VARIANT=userdebug&lt;BR /&gt;TARGET_BUILD_TYPE=release&lt;BR /&gt;TARGET_PLATFORM_VERSION=OPD1&lt;BR /&gt;TARGET_BUILD_APPS=&lt;BR /&gt;TARGET_ARCH=arm&lt;BR /&gt;TARGET_ARCH_VARIANT=armv7-a-neon&lt;BR /&gt;TARGET_CPU_VARIANT=cortex-a9&lt;BR /&gt;TARGET_2ND_ARCH=&lt;BR /&gt;TARGET_2ND_ARCH_VARIANT=&lt;BR /&gt;TARGET_2ND_CPU_VARIANT=&lt;BR /&gt;HOST_ARCH=x86_64&lt;BR /&gt;HOST_2ND_ARCH=x86&lt;BR /&gt;HOST_OS=linux&lt;BR /&gt;HOST_OS_EXTRA=Linux-4.15.0-47-generic-x86_64-with-Ubuntu-16.04-xenial&lt;BR /&gt;HOST_CROSS_OS=windows&lt;BR /&gt;HOST_CROSS_ARCH=x86&lt;BR /&gt;HOST_CROSS_2ND_ARCH=x86_64&lt;BR /&gt;HOST_BUILD_TYPE=release&lt;BR /&gt;BUILD_ID=1.0.0-ga&lt;BR /&gt;OUT_DIR=out&lt;BR /&gt;AUX_OS_VARIANT_LIST=&lt;BR /&gt;============================================&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;---&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;COPY u-boot.bin&lt;BR /&gt; MKIMAGE u-boot.img&lt;BR /&gt; LD spl/fs/ext4/built-in.o&lt;BR /&gt; LD spl/fs/built-in.o&lt;BR /&gt; LD spl/u-boot-spl&lt;BR /&gt; OBJCOPY spl/u-boot-spl-nodtb.bin&lt;BR /&gt; COPY spl/u-boot-spl.bin&lt;BR /&gt; CFGS arch/arm/imx-common/spl_sd.cfg.cfgtmp&lt;BR /&gt; MKIMAGE SPL&lt;BR /&gt; CFGCHK u-boot.cfg&lt;BR /&gt;make[1]: Leaving directory '/media/nilson/69716c8f-0359-4303-a1aa-481e72f885ae1/imx6-variscite/imx-o8.0.0_1.0.0_ga/android_build/out/target/product/var_mx6/obj/BOOTLOADER_OBJ'&lt;BR /&gt;make: Leaving directory '/media/nilson/69716c8f-0359-4303-a1aa-481e72f885ae1/imx6-variscite/imx-o8.0.0_1.0.0_ga/android_build/vendor/variscite/uboot-imx'&lt;BR /&gt;/bin/bash: line 0: [: =: unary operator expected&lt;BR /&gt;ninja: build stopped: subcommand failed.&lt;BR /&gt;19:08:48 ninja failed with: exit status 1&lt;BR /&gt;build/core/main.mk:21: recipe for target 'run_soong_ui' failed&lt;BR /&gt;make: *** [run_soong_ui] Error 1&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there any alternative solution to get run_soong_ui target working?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 05 Apr 2019 23:12:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Android-Oreo-compilation-Problem/m-p/848905#M129931</guid>
      <dc:creator>nilson_oliveira</dc:creator>
      <dc:date>2019-04-05T23:12:35Z</dc:date>
    </item>
    <item>
      <title>Re: Android Oreo compilation Problem</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Android-Oreo-compilation-Problem/m-p/848906#M129932</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Just to let register the solution:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In my environment, I had an older version of make_ext4fs at /usr/bin which was confusing the build - as it was not using the properly binary on out/host/linux-x86/bin - so, make sure you're using the properly version of the tools in order to get the build done.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I figure it out&amp;nbsp;looking at build log and right&amp;nbsp;after reducing the build to only one job (make -j1) - when I could see that the&amp;nbsp;make_ext4fs was failing.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 09 Apr 2019 20:06:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Android-Oreo-compilation-Problem/m-p/848906#M129932</guid>
      <dc:creator>nilson_oliveira</dc:creator>
      <dc:date>2019-04-09T20:06:28Z</dc:date>
    </item>
    <item>
      <title>Re: Android Oreo compilation Problem</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Android-Oreo-compilation-Problem/m-p/848907#M129933</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am having the exact same issue, can you specify exactly how did you resolve the issue?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have completely deleted /usr/bin/make_ext4fs&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 01 Jun 2019 17:11:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Android-Oreo-compilation-Problem/m-p/848907#M129933</guid>
      <dc:creator>ilanganor</dc:creator>
      <dc:date>2019-06-01T17:11:22Z</dc:date>
    </item>
  </channel>
</rss>