<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Uboot Custom Version Number in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Uboot-Custom-Version-Number/m-p/848764#M129906</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Naveed&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You can check:&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/325300"&gt;Update u-boot via serial communication&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://boundarydevices.com/i-mx-6dq-u-boot-updates/" title="https://boundarydevices.com/i-mx-6dq-u-boot-updates/"&gt;i.MX 6 U-Boot updates - Boundary Devices&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 21 Sep 2018 14:57:03 GMT</pubDate>
    <dc:creator>Bio_TICFSL</dc:creator>
    <dc:date>2018-09-21T14:57:03Z</dc:date>
    <item>
      <title>Uboot Custom Version Number</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Uboot-Custom-Version-Number/m-p/848763#M129905</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;What is the best way to expose a custom uboot version (we have an internal version number for our release build of uboot). WOuld be even better to also expose a build timestamp.&lt;/P&gt;&lt;P&gt;I have tried using the compiler command line however this worked fine when programming with Mfgtool but I found when upgrading uboot this sometimes would not be updated (Weird I know).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As I am a bit of a newbie I may be missing something. I used the u-boot.imx file to create a full 2MB file and write that to the u-boot partition to ensure any other data is erased. Not sure if other stuff is saved elsewhere.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Note: we are using uboot 2014.04 and Linux 3.14&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 20 Sep 2018 00:55:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Uboot-Custom-Version-Number/m-p/848763#M129905</guid>
      <dc:creator>naveedghori</dc:creator>
      <dc:date>2018-09-20T00:55:32Z</dc:date>
    </item>
    <item>
      <title>Re: Uboot Custom Version Number</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Uboot-Custom-Version-Number/m-p/848764#M129906</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Naveed&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You can check:&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/325300"&gt;Update u-boot via serial communication&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://boundarydevices.com/i-mx-6dq-u-boot-updates/" title="https://boundarydevices.com/i-mx-6dq-u-boot-updates/"&gt;i.MX 6 U-Boot updates - Boundary Devices&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 21 Sep 2018 14:57:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Uboot-Custom-Version-Number/m-p/848764#M129906</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2018-09-21T14:57:03Z</dc:date>
    </item>
    <item>
      <title>Re: Uboot Custom Version Number</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Uboot-Custom-Version-Number/m-p/848765#M129907</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I want a way for Linux to be able to read the custom uboot version. Eg for every minot change to uboot we will give it our own number eg 1.01, 1.02. and we want linux to be able to detect the current running uboot.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Currently I am looking at punting some info at the end of the uboot partition. Not sure if this is advisable or done by anyone else. Maybe there is a better way?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 27 Sep 2018 01:59:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Uboot-Custom-Version-Number/m-p/848765#M129907</guid>
      <dc:creator>naveedghori</dc:creator>
      <dc:date>2018-09-27T01:59:00Z</dc:date>
    </item>
    <item>
      <title>Re: Uboot Custom Version Number</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Uboot-Custom-Version-Number/m-p/848766#M129908</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;For now I have gone with creating an info block a the end of the uboot partition. This is done by creating a file for the full 2MB partition and adding meta data into an info block at the very end. This can then be read by and interpreted as required (will probably write a driver to expose this information).&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 02 Oct 2018 02:16:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Uboot-Custom-Version-Number/m-p/848766#M129908</guid>
      <dc:creator>naveedghori</dc:creator>
      <dc:date>2018-10-02T02:16:18Z</dc:date>
    </item>
  </channel>
</rss>