<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Android Oreo 8.0: Use two displays with different resolution</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Android-Oreo-8-0-Use-two-displays-with-different-resolution/m-p/846245#M129617</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;you can boot up dual display successfully, but couldn't show the different resolution, right? pls refer to the topic as below:&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/384600"&gt;https://community.nxp.com/thread/384600&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 10 Jan 2019 07:04:01 GMT</pubDate>
    <dc:creator>joanxie</dc:creator>
    <dc:date>2019-01-10T07:04:01Z</dc:date>
    <item>
      <title>Android Oreo 8.0: Use two displays with different resolution</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Android-Oreo-8-0-Use-two-displays-with-different-resolution/m-p/846244#M129616</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am using the default images on the i.MX6 reference board and I see that when using HDMI + LVDS display, Android works in mirror mode showing the same content in both displays, rescaling it if needed.&lt;/P&gt;&lt;P&gt;How can I configure Android so that different resolutions are used? (The HDMI negociated&amp;nbsp;resolution for HDMI, and the LVDS native resolution for the LVDS display)&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 02 Jan 2019 17:23:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Android-Oreo-8-0-Use-two-displays-with-different-resolution/m-p/846244#M129616</guid>
      <dc:creator>jdepedro</dc:creator>
      <dc:date>2019-01-02T17:23:13Z</dc:date>
    </item>
    <item>
      <title>Re: Android Oreo 8.0: Use two displays with different resolution</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Android-Oreo-8-0-Use-two-displays-with-different-resolution/m-p/846245#M129617</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;you can boot up dual display successfully, but couldn't show the different resolution, right? pls refer to the topic as below:&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/384600"&gt;https://community.nxp.com/thread/384600&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 10 Jan 2019 07:04:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Android-Oreo-8-0-Use-two-displays-with-different-resolution/m-p/846245#M129617</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2019-01-10T07:04:01Z</dc:date>
    </item>
  </channel>
</rss>