<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックIMXRT1050-EVKB - Setting up a HTTP Client</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMXRT1050-EVKB-Setting-up-a-HTTP-Client/m-p/844911#M129478</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi there,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have recently acquired this board and would like to set it up as a &lt;STRONG&gt;HTTP client&lt;/STRONG&gt; and make a HTTP request through the ethernet port using the 'lwip' package (either bm or FreeRTOS is fine)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Having looked through the demo apps, there is one which sets up the board as the &lt;STRONG&gt;HTTP server&lt;/STRONG&gt; whereby the PC it is connected to, can make a HTTP request through a browser. This app is located at &lt;EM&gt;"\boards\evkbimxrt1050\lwip_examples\lwip_httpsrv\"&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Essentially, I am attempting to do the inverse of what the demo app implements. I was wondering if anyone could suggest how I could modify the code to achieve this, or advise me on some code which does this.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 03 Jul 2018 14:52:41 GMT</pubDate>
    <dc:creator>marcus_masca</dc:creator>
    <dc:date>2018-07-03T14:52:41Z</dc:date>
    <item>
      <title>IMXRT1050-EVKB - Setting up a HTTP Client</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMXRT1050-EVKB-Setting-up-a-HTTP-Client/m-p/844911#M129478</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi there,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have recently acquired this board and would like to set it up as a &lt;STRONG&gt;HTTP client&lt;/STRONG&gt; and make a HTTP request through the ethernet port using the 'lwip' package (either bm or FreeRTOS is fine)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Having looked through the demo apps, there is one which sets up the board as the &lt;STRONG&gt;HTTP server&lt;/STRONG&gt; whereby the PC it is connected to, can make a HTTP request through a browser. This app is located at &lt;EM&gt;"\boards\evkbimxrt1050\lwip_examples\lwip_httpsrv\"&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Essentially, I am attempting to do the inverse of what the demo app implements. I was wondering if anyone could suggest how I could modify the code to achieve this, or advise me on some code which does this.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Jul 2018 14:52:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMXRT1050-EVKB-Setting-up-a-HTTP-Client/m-p/844911#M129478</guid>
      <dc:creator>marcus_masca</dc:creator>
      <dc:date>2018-07-03T14:52:41Z</dc:date>
    </item>
    <item>
      <title>Re: IMXRT1050-EVKB - Setting up a HTTP Client</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMXRT1050-EVKB-Setting-up-a-HTTP-Client/m-p/844912#M129479</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Marcus,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In newest SDK (2.4) you can find the following example:&lt;/P&gt;&lt;P&gt;C:\nxp\EVKB-IMXRT1050\boards\evkbimxrt1050\lwip_examples\lwip_httpscli_mbedTLS&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You can also use a library like this:&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://os.mbed.com/users/WiredHome/code/HTTPClient/" title="https://os.mbed.com/users/WiredHome/code/HTTPClient/"&gt;HTTPClient - Fixed custom headers and Basic authorization, a... | Mbed&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Regards,&lt;BR /&gt;Carlos&lt;BR /&gt;NXP Technical Support&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 09 Jul 2018 21:54:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMXRT1050-EVKB-Setting-up-a-HTTP-Client/m-p/844912#M129479</guid>
      <dc:creator>Carlos_Musich</dc:creator>
      <dc:date>2018-07-09T21:54:34Z</dc:date>
    </item>
  </channel>
</rss>