<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic imx6d+ IPU virtual channels? in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/imx6d-IPU-virtual-channels/m-p/843896#M129382</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Customer is Aptiv.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;They have a design with imx6d+, with connections as follows:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Parallel0 &amp;lt;- HDMI1&lt;/P&gt;&lt;P&gt;Parallel1 &amp;lt;- HDMI2&lt;/P&gt;&lt;P&gt;mipi-csi0 &amp;lt;- three inputs muxed through a lattice fpga - each using a different virtual channel.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Will the imx6d+ have the throughput to input and seperate all three inputs from the lattice at the same time? Assuming 720p resolution?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Randy Krakora&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 10 Aug 2018 14:26:42 GMT</pubDate>
    <dc:creator>RandyKrakora</dc:creator>
    <dc:date>2018-08-10T14:26:42Z</dc:date>
    <item>
      <title>imx6d+ IPU virtual channels?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6d-IPU-virtual-channels/m-p/843896#M129382</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Customer is Aptiv.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;They have a design with imx6d+, with connections as follows:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Parallel0 &amp;lt;- HDMI1&lt;/P&gt;&lt;P&gt;Parallel1 &amp;lt;- HDMI2&lt;/P&gt;&lt;P&gt;mipi-csi0 &amp;lt;- three inputs muxed through a lattice fpga - each using a different virtual channel.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Will the imx6d+ have the throughput to input and seperate all three inputs from the lattice at the same time? Assuming 720p resolution?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Randy Krakora&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 10 Aug 2018 14:26:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6d-IPU-virtual-channels/m-p/843896#M129382</guid>
      <dc:creator>RandyKrakora</dc:creator>
      <dc:date>2018-08-10T14:26:42Z</dc:date>
    </item>
    <item>
      <title>Re: imx6d+ IPU virtual channels?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6d-IPU-virtual-channels/m-p/843897#M129383</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;do you need 2CSI+3MIPI? current bsp can support up to 4-CAMERA&lt;/P&gt;&lt;P&gt;The 4 cameras can be:&lt;/P&gt;&lt;P&gt;- 1xCSI, 3xMIPI&lt;/P&gt;&lt;P&gt;- 2xCSI, 2xMIPI&lt;/P&gt;&lt;P&gt;- 4xMIPI&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;more detailed settings, pls refer to the document as below:&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" class="link-titled" href="https://community.nxp.com/docs/DOC-328548?commentID=55362#comment-55362" title="https://community.nxp.com/docs/DOC-328548?commentID=55362#comment-55362"&gt;https://community.nxp.com/docs/DOC-328548?commentID=55362#comment-55362&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 17 Aug 2018 04:28:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6d-IPU-virtual-channels/m-p/843897#M129383</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2018-08-17T04:28:47Z</dc:date>
    </item>
  </channel>
</rss>