<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic MIMXRT1052DVL6B lcd interface in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/MIMXRT1052DVL6B-lcd-interface/m-p/843684#M129365</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I attached a excel sheet with this. In that I mentioned 2 models for 24 bit data for RGB display and 1 for 16 bit data. In one 24 bit data model I gave first 16 bit data in 5,6,5 format( D0 to D4 for B3 to B7,D5 to D10 for G2 to G7 ,D11 to D15 to R3 to R7).&lt;/P&gt;&lt;P&gt;The remaining 8bit data is given as in excel sheet (D16 to D18 as R0 to R3, D19 &amp;amp; D20 as G0 &amp;amp; G1 , D21 to D23 as B0 to B3).&lt;/P&gt;&lt;P&gt;In second model I gave D0 to D7 for B0 to B7, D8 to D15 as G0 to G7 and D16 to D23 as R0 to R7.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;From these two which can I use for 24 bit display. Can you please tell which is correct and which is wrong. (If both are wrong please suggest correct one).&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 23 Jul 2018 13:00:54 GMT</pubDate>
    <dc:creator>muhammed_shafee</dc:creator>
    <dc:date>2018-07-23T13:00:54Z</dc:date>
    <item>
      <title>MIMXRT1052DVL6B lcd interface</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MIMXRT1052DVL6B-lcd-interface/m-p/843684#M129365</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I attached a excel sheet with this. In that I mentioned 2 models for 24 bit data for RGB display and 1 for 16 bit data. In one 24 bit data model I gave first 16 bit data in 5,6,5 format( D0 to D4 for B3 to B7,D5 to D10 for G2 to G7 ,D11 to D15 to R3 to R7).&lt;/P&gt;&lt;P&gt;The remaining 8bit data is given as in excel sheet (D16 to D18 as R0 to R3, D19 &amp;amp; D20 as G0 &amp;amp; G1 , D21 to D23 as B0 to B3).&lt;/P&gt;&lt;P&gt;In second model I gave D0 to D7 for B0 to B7, D8 to D15 as G0 to G7 and D16 to D23 as R0 to R7.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;From these two which can I use for 24 bit display. Can you please tell which is correct and which is wrong. (If both are wrong please suggest correct one).&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 23 Jul 2018 13:00:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MIMXRT1052DVL6B-lcd-interface/m-p/843684#M129365</guid>
      <dc:creator>muhammed_shafee</dc:creator>
      <dc:date>2018-07-23T13:00:54Z</dc:date>
    </item>
  </channel>
</rss>