<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Minimum external DDR3 amount in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Minimum-external-DDR3-amount/m-p/843442#M129325</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The i.MX7Solo datasheet says the DDR interface density is 256MB to 2GB (9.1.2 table 9-1). Does that actually mean that using 512Mbit or 1Gbit DDR3 chips is out of the question?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 23 Jul 2018 16:18:02 GMT</pubDate>
    <dc:creator>olli_mannisto</dc:creator>
    <dc:date>2018-07-23T16:18:02Z</dc:date>
    <item>
      <title>Minimum external DDR3 amount</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Minimum-external-DDR3-amount/m-p/843442#M129325</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The i.MX7Solo datasheet says the DDR interface density is 256MB to 2GB (9.1.2 table 9-1). Does that actually mean that using 512Mbit or 1Gbit DDR3 chips is out of the question?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 23 Jul 2018 16:18:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Minimum-external-DDR3-amount/m-p/843442#M129325</guid>
      <dc:creator>olli_mannisto</dc:creator>
      <dc:date>2018-07-23T16:18:02Z</dc:date>
    </item>
    <item>
      <title>Re: Minimum external DDR3 amount</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Minimum-external-DDR3-amount/m-p/843443#M129326</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; i.MX7 DDRC supports devices with column size of 8-12 bits and row size of 11-16 bits;&lt;/P&gt;&lt;P&gt;data port size 16/32-bit; up to two CSs. Total memory size is restricted by 2048 MBytes (look at system&lt;/P&gt;&lt;P&gt;memory map).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 24 Jul 2018 05:14:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Minimum-external-DDR3-amount/m-p/843443#M129326</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2018-07-24T05:14:08Z</dc:date>
    </item>
    <item>
      <title>Re: Minimum external DDR3 amount</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Minimum-external-DDR3-amount/m-p/843444#M129327</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hei,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I was asking about&amp;nbsp;&lt;EM&gt;minimum&lt;/EM&gt; memory size. Are we fine with 512Mbit (32MBx16) part that's organized 12bit Row, 10bit Column? Apparently yes, but the datasheet claims 256MB is the minimum RAM size?&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 25 Jul 2018 11:24:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Minimum-external-DDR3-amount/m-p/843444#M129327</guid>
      <dc:creator>olli_mannisto</dc:creator>
      <dc:date>2018-07-25T11:24:37Z</dc:date>
    </item>
  </channel>
</rss>