<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Parallel camera Device tree entries.</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Parallel-camera-Device-tree-entries/m-p/843410#M129324</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Igor,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your reply.&lt;/P&gt;&lt;P&gt;Input available to CSI interface is RGB24, i,e 24 bits / Clk.&amp;nbsp;&lt;/P&gt;&lt;P&gt;In iMX7 Reference manual, section "13.3 CMOS Sensor Interaface" it is mentioned that it supports RGB24. But when I captured a frame from the CSI interface it is not as expected.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What is the CSI register configuration required to enable RGB24 capture.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;BR /&gt;Subbarao.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 04 Jul 2018 11:24:28 GMT</pubDate>
    <dc:creator>subbaraopnv</dc:creator>
    <dc:date>2018-07-04T11:24:28Z</dc:date>
    <item>
      <title>Parallel camera Device tree entries.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Parallel-camera-Device-tree-entries/m-p/843408#M129322</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In iMX7, We are going to interface a parallel camera. What are the device tree entries are required for a parallel camera?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;BR /&gt;Subbarao.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Jul 2018 12:35:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Parallel-camera-Device-tree-entries/m-p/843408#M129322</guid>
      <dc:creator>subbaraopnv</dc:creator>
      <dc:date>2018-07-03T12:35:04Z</dc:date>
    </item>
    <item>
      <title>Re: Parallel camera Device tree entries.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Parallel-camera-Device-tree-entries/m-p/843409#M129323</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Subbaro&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am not aware of parallel camera dts for i.MX7, but as it has the same CSI module&lt;/P&gt;&lt;P&gt;as i.MX6UL, SL one can look at its dts:&lt;/P&gt;&lt;P&gt;linux/arch/arm/boot/dts/imx6ul-14x14-evk-csi.dts&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://source.codeaurora.org/external/imx/linux-imx/tree/arch/arm/boot/dts/imx6ul-14x14-evk-csi.dts?h=imx_4.1.15_2.0.0_ga" title="https://source.codeaurora.org/external/imx/linux-imx/tree/arch/arm/boot/dts/imx6ul-14x14-evk-csi.dts?h=imx_4.1.15_2.0.0_ga"&gt;imx6ul-14x14-evk-csi.dts\dts\boot\arm\arch - linux-imx - i.MX Linux kernel&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://source.codeaurora.org/external/imx/linux-imx/tree/arch/arm/boot/dts/imx6sl-evk-csi.dts?h=imx_4.1.15_2.0.0_ga" title="https://source.codeaurora.org/external/imx/linux-imx/tree/arch/arm/boot/dts/imx6sl-evk-csi.dts?h=imx_4.1.15_2.0.0_ga"&gt;imx6sl-evk-csi.dts\dts\boot\arm\arch - linux-imx - i.MX Linux kernel&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/375865"&gt;About preview function in i.MX6SL.&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 04 Jul 2018 01:31:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Parallel-camera-Device-tree-entries/m-p/843409#M129323</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2018-07-04T01:31:54Z</dc:date>
    </item>
    <item>
      <title>Re: Parallel camera Device tree entries.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Parallel-camera-Device-tree-entries/m-p/843410#M129324</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Igor,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your reply.&lt;/P&gt;&lt;P&gt;Input available to CSI interface is RGB24, i,e 24 bits / Clk.&amp;nbsp;&lt;/P&gt;&lt;P&gt;In iMX7 Reference manual, section "13.3 CMOS Sensor Interaface" it is mentioned that it supports RGB24. But when I captured a frame from the CSI interface it is not as expected.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What is the CSI register configuration required to enable RGB24 capture.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;BR /&gt;Subbarao.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 04 Jul 2018 11:24:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Parallel-camera-Device-tree-entries/m-p/843410#M129324</guid>
      <dc:creator>subbaraopnv</dc:creator>
      <dc:date>2018-07-04T11:24:28Z</dc:date>
    </item>
  </channel>
</rss>