<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: How can add a zigbee/thread module to IMX8Mq board.</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/How-can-add-a-zigbee-thread-module-to-IMX8Mq-board/m-p/843026#M129238</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;To implement&amp;nbsp;this in the DTB, the only changes that you could do is with the frequency of your SPI module&amp;nbsp;and sometimes the SPI driver is disabled in the DTB, you may need to activate it also.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regarding how to implement the zigbee communication, depends a lot on your end application. However, how you are implementing&amp;nbsp;your communication through SPI, you will create the zigbee communication through&amp;nbsp;SPI commands. Please see the below web-page, there is an example of how to use the&amp;nbsp;Linux SPI driver.&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="http://linux-sunxi.org/SPIdev" title="http://linux-sunxi.org/SPIdev"&gt;http://linux-sunxi.org/SPIdev&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Diego.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Aug 2018 17:08:49 GMT</pubDate>
    <dc:creator>diegoadrian</dc:creator>
    <dc:date>2018-08-15T17:08:49Z</dc:date>
    <item>
      <title>How can add a zigbee/thread module to IMX8Mq board.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-can-add-a-zigbee-thread-module-to-IMX8Mq-board/m-p/843025#M129237</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, &lt;/P&gt;&lt;P&gt;I have having a&amp;nbsp;mgm111a256v2 module, which is tobe integrated to our imx8m based custom board. According schematic spi will be used to interface with mgm111a256v2 module.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1. To implement this in DT, kernel, and application side what should be done. Can I have some reference which can help me to integrate it?&lt;/P&gt;&lt;P&gt;2. How can I test this implementation?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I appreciated your help.&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 10 Aug 2018 13:00:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-can-add-a-zigbee-thread-module-to-IMX8Mq-board/m-p/843025#M129237</guid>
      <dc:creator>ysandeepkumar07</dc:creator>
      <dc:date>2018-08-10T13:00:33Z</dc:date>
    </item>
    <item>
      <title>Re: How can add a zigbee/thread module to IMX8Mq board.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-can-add-a-zigbee-thread-module-to-IMX8Mq-board/m-p/843026#M129238</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;To implement&amp;nbsp;this in the DTB, the only changes that you could do is with the frequency of your SPI module&amp;nbsp;and sometimes the SPI driver is disabled in the DTB, you may need to activate it also.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regarding how to implement the zigbee communication, depends a lot on your end application. However, how you are implementing&amp;nbsp;your communication through SPI, you will create the zigbee communication through&amp;nbsp;SPI commands. Please see the below web-page, there is an example of how to use the&amp;nbsp;Linux SPI driver.&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="http://linux-sunxi.org/SPIdev" title="http://linux-sunxi.org/SPIdev"&gt;http://linux-sunxi.org/SPIdev&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Diego.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Aug 2018 17:08:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-can-add-a-zigbee-thread-module-to-IMX8Mq-board/m-p/843026#M129238</guid>
      <dc:creator>diegoadrian</dc:creator>
      <dc:date>2018-08-15T17:08:49Z</dc:date>
    </item>
  </channel>
</rss>