<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Transfer IMX6 audio data to fpga over EIM bus</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Transfer-IMX6-audio-data-to-fpga-over-EIM-bus/m-p/842246#M129158</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am working on a imx6q custom board and using freescale linux kernel 3.14.52 .&lt;/P&gt;&lt;P&gt;I want to send and receive audio data from sgtl5000 codec connected to SSI interface of imx6 to an FPGA via EIM. What would be the best way to do that ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks and regards,&lt;/P&gt;&lt;P&gt;Sumish&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 06 Dec 2018 07:13:17 GMT</pubDate>
    <dc:creator>sumish_ks</dc:creator>
    <dc:date>2018-12-06T07:13:17Z</dc:date>
    <item>
      <title>Transfer IMX6 audio data to fpga over EIM bus</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Transfer-IMX6-audio-data-to-fpga-over-EIM-bus/m-p/842246#M129158</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am working on a imx6q custom board and using freescale linux kernel 3.14.52 .&lt;/P&gt;&lt;P&gt;I want to send and receive audio data from sgtl5000 codec connected to SSI interface of imx6 to an FPGA via EIM. What would be the best way to do that ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks and regards,&lt;/P&gt;&lt;P&gt;Sumish&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 06 Dec 2018 07:13:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Transfer-IMX6-audio-data-to-fpga-over-EIM-bus/m-p/842246#M129158</guid>
      <dc:creator>sumish_ks</dc:creator>
      <dc:date>2018-12-06T07:13:17Z</dc:date>
    </item>
    <item>
      <title>Re: Transfer IMX6 audio data to fpga over EIM bus</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Transfer-IMX6-audio-data-to-fpga-over-EIM-bus/m-p/842247#M129159</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Sumish&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can check Chapter 28 Advanced Linux Sound Architecture (ALSA) System&lt;BR /&gt;on a Chip (ASoC) Sound Driver attached Linux Manual for linux sound subsystem description.&lt;/P&gt;&lt;P&gt;Data from fpga can be written to file, then played using examples in&lt;/P&gt;&lt;P&gt;imx-test (./mxc_sound_test) package&lt;BR /&gt;&lt;A href="https://community.nxp.com/www.nxp.com/lgfiles/NMG/MAD/YOCTO/imx-test-5.7.tar.gz" target="test_blank"&gt;www.nxp.com/lgfiles/NMG/MAD/YOCTO/imx-test-5.7.tar.gz&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 07 Dec 2018 00:25:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Transfer-IMX6-audio-data-to-fpga-over-EIM-bus/m-p/842247#M129159</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2018-12-07T00:25:51Z</dc:date>
    </item>
    <item>
      <title>Re: Transfer IMX6 audio data to fpga over EIM bus</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Transfer-IMX6-audio-data-to-fpga-over-EIM-bus/m-p/842248#M129160</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi igor,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks a lot. To send continuous audio data from audio codec to fpga through EIM, can I use the same approach as you mentioned for the data received from fpga (for e.g. writing to a file first then send it to fpga)? Please note that we are sending/receiving &lt;STRONG&gt;continuous audio data&lt;/STRONG&gt;.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Sumish&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 07 Dec 2018 04:57:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Transfer-IMX6-audio-data-to-fpga-over-EIM-bus/m-p/842248#M129160</guid>
      <dc:creator>sumish_ks</dc:creator>
      <dc:date>2018-12-07T04:57:06Z</dc:date>
    </item>
    <item>
      <title>Re: Transfer IMX6 audio data to fpga over EIM bus</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Transfer-IMX6-audio-data-to-fpga-over-EIM-bus/m-p/842249#M129161</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Sumish&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I think this is posiible, consider changing writing audio data to memory&lt;/P&gt;&lt;P&gt;circular buffer instead file.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 08 Dec 2018 03:39:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Transfer-IMX6-audio-data-to-fpga-over-EIM-bus/m-p/842249#M129161</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2018-12-08T03:39:52Z</dc:date>
    </item>
    <item>
      <title>Re: Transfer IMX6 audio data to fpga over EIM bus</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Transfer-IMX6-audio-data-to-fpga-over-EIM-bus/m-p/842250#M129162</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks igor.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 10 Dec 2018 10:44:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Transfer-IMX6-audio-data-to-fpga-over-EIM-bus/m-p/842250#M129162</guid>
      <dc:creator>sumish_ks</dc:creator>
      <dc:date>2018-12-10T10:44:59Z</dc:date>
    </item>
  </channel>
</rss>