<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Build yocto image for i.MX6 without GPU support and with LinuxFB</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Build-yocto-image-for-i-MX6-without-GPU-support-and-with-LinuxFB/m-p/842177#M129151</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You can start from a core-image-minimal and add any extra packages that you need either on the conf/local.conf or creating a new image recipe.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;-Marco&lt;/P&gt;&lt;P&gt;&lt;A class="link-bare" href="http://www.ridgerun.com"&gt;http://www.ridgerun.com&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 19 Sep 2018 13:48:41 GMT</pubDate>
    <dc:creator>marcomadrigal</dc:creator>
    <dc:date>2018-09-19T13:48:41Z</dc:date>
    <item>
      <title>Build yocto image for i.MX6 without GPU support and with LinuxFB</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Build-yocto-image-for-i-MX6-without-GPU-support-and-with-LinuxFB/m-p/842176#M129150</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;How can I build yocto image with only LinuxFB support for i.MX6 with GPU disabled. I want to do this to create same environment and scenario for testing qt gui which was being run earlier on i.MX35.&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 18 Sep 2018 15:47:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Build-yocto-image-for-i-MX6-without-GPU-support-and-with-LinuxFB/m-p/842176#M129150</guid>
      <dc:creator>chintan_raval</dc:creator>
      <dc:date>2018-09-18T15:47:07Z</dc:date>
    </item>
    <item>
      <title>Re: Build yocto image for i.MX6 without GPU support and with LinuxFB</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Build-yocto-image-for-i-MX6-without-GPU-support-and-with-LinuxFB/m-p/842177#M129151</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You can start from a core-image-minimal and add any extra packages that you need either on the conf/local.conf or creating a new image recipe.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;-Marco&lt;/P&gt;&lt;P&gt;&lt;A class="link-bare" href="http://www.ridgerun.com"&gt;http://www.ridgerun.com&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 19 Sep 2018 13:48:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Build-yocto-image-for-i-MX6-without-GPU-support-and-with-LinuxFB/m-p/842177#M129151</guid>
      <dc:creator>marcomadrigal</dc:creator>
      <dc:date>2018-09-19T13:48:41Z</dc:date>
    </item>
    <item>
      <title>Re: Build yocto image for i.MX6 without GPU support and with LinuxFB</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Build-yocto-image-for-i-MX6-without-GPU-support-and-with-LinuxFB/m-p/842178#M129152</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Chintan Raval,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As Marco Madrigal mentioned the easiest way to achieve this is creating your image with only the required packages. Core-image-minimal is a great place to start! As this inherits from the core-image.bbclass and allows to add some standard IMAGE_FEATURES.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;You can find more information on the Yocto Reference Manual:&lt;BR /&gt;&lt;A href="https://www.yoctoproject.org/docs/2.2/ref-manual/ref-manual.html#ref-classes-core-image"&gt;https://www.yoctoproject.org/docs/2.2/ref-manual/ref-manual.html#ref-classes-core-image&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Alternatively, you can disable the GPU support on the kernel defconfig.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;I hope this helps!&lt;BR /&gt;Regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 19 Sep 2018 17:06:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Build-yocto-image-for-i-MX6-without-GPU-support-and-with-LinuxFB/m-p/842178#M129152</guid>
      <dc:creator>gusarambula</dc:creator>
      <dc:date>2018-09-19T17:06:49Z</dc:date>
    </item>
  </channel>
</rss>