<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: How to settle the error in Yocto build system? in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/How-to-settle-the-error-in-Yocto-build-system/m-p/842141#M129145</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Better to ask MYIR to provide you the BSP document for Yocto BSP build. &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 28 Sep 2018 07:10:18 GMT</pubDate>
    <dc:creator>jimmychan</dc:creator>
    <dc:date>2018-09-28T07:10:18Z</dc:date>
    <item>
      <title>How to settle the error in Yocto build system?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-to-settle-the-error-in-Yocto-build-system/m-p/842140#M129144</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;H3 style="color: #000000; border-top: none; border-bottom: 1px solid #cccccc; border-left: none; border-right: none; font-size: 14px; margin: 1em 0px; padding: 0px 0px 0.5em;"&gt;How to settle the error in Yocto build system?&lt;/H3&gt;&lt;P&gt;When making a distro for MYIR's &lt;A href="http://www.myirtech.com/list.asp?id=573"&gt;MYD-Y6ULX&lt;/A&gt; board. The error has occurred in Yocto build system. How to settle it then?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.5pt;"&gt;|&amp;nbsp;dd:&amp;nbsp;failed&amp;nbsp;to&amp;nbsp;open&amp;nbsp;'/home/v/MYD-Y6ULX-devel/fsl-release-yocto/build/tmp/deploy/images/myd-y6ull14x14/u-boot-myd-y6ull14x14.imx-sd':&amp;nbsp;No&amp;nbsp;such&amp;nbsp;file&amp;nbsp;or&amp;nbsp;directory&lt;BR /&gt; |&amp;nbsp;WARNING:&amp;nbsp;exit&amp;nbsp;code&amp;nbsp;1&amp;nbsp;from&amp;nbsp;a&amp;nbsp;shell&amp;nbsp;command.&lt;BR /&gt; |&amp;nbsp;ERROR:&amp;nbsp;Function&amp;nbsp;failed:&amp;nbsp;do_image_sdcard&amp;nbsp;(log&amp;nbsp;file&amp;nbsp;is&amp;nbsp;located&amp;nbsp;at&amp;nbsp;/home/v/MYD-Y6ULX-devel/fsl-release-yocto/build/tmp/work/myd_y6ull14x14-poky-linux-gnueabi/core-image-base/1.0-r0/temp/log.do_image_sdcard.9743) &lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Jul 2018 07:55:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-to-settle-the-error-in-Yocto-build-system/m-p/842140#M129144</guid>
      <dc:creator>linda_zhang</dc:creator>
      <dc:date>2018-07-03T07:55:09Z</dc:date>
    </item>
    <item>
      <title>Re: How to settle the error in Yocto build system?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-to-settle-the-error-in-Yocto-build-system/m-p/842141#M129145</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Better to ask MYIR to provide you the BSP document for Yocto BSP build. &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 28 Sep 2018 07:10:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-to-settle-the-error-in-Yocto-build-system/m-p/842141#M129145</guid>
      <dc:creator>jimmychan</dc:creator>
      <dc:date>2018-09-28T07:10:18Z</dc:date>
    </item>
    <item>
      <title>Re: How to settle the error in Yocto build system?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-to-settle-the-error-in-Yocto-build-system/m-p/842142#M129146</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm facing problem on yocto build for MYS6ULX-IOT board.&lt;/P&gt;&lt;P&gt;After putting .sdcard image into sdcard&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;at the time of kernel up:&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;E/TC:0 plat_rng_init:354 Warning: seeding RNG with zeroes&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;-------&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;U-Boot 2018.03-imx_v2018.03_4.14.78_1.0.0_ga+g654088cc21 (Feb 02 2019 - 06:32:32 +0000)&lt;/P&gt;&lt;P&gt;CPU: Freescale i.MX6ULL rev1.1 528 MHz (running at 396 MHz)&lt;BR /&gt;CPU: Commercial temperature grade (0C to 95C) at 42C&lt;BR /&gt;Reset cause: POR&lt;BR /&gt;Model: Freescale i.MX6 ULL 14x14 EVK Board&lt;BR /&gt;Board: MX6ULL 14x14 EVK&lt;BR /&gt;DRAM: 512 MiB&lt;BR /&gt;MMC: FSL_SDHC: 0, FSL_SDHC: 1&lt;BR /&gt;Loading Environment from MMC... *** Warning - bad CRC, using default environment&lt;/P&gt;&lt;P&gt;Failed (-5)&lt;BR /&gt;Display: TFT43AB (480x272)&lt;BR /&gt;Video: 480x272x24&lt;BR /&gt;In: serial&lt;BR /&gt;Out: serial&lt;BR /&gt;Err: serial&lt;BR /&gt;switch to partitions #0, OK&lt;BR /&gt;mmc0 is current device&lt;BR /&gt;flash target is MMC:0&lt;BR /&gt;Net: No ethernet found.&lt;BR /&gt;Fastboot: Normal&lt;BR /&gt;Normal Boot&lt;BR /&gt;Hit any key to stop autoboot: 0&lt;BR /&gt;switch to partitions #0, OK&lt;BR /&gt;mmc0 is current device&lt;BR /&gt;switch to partitions #0, OK&lt;BR /&gt;mmc0 is current device&lt;BR /&gt;** Unable to read file boot.scr **&lt;BR /&gt;7389640 bytes read in 327 ms (21.6 MiB/s)&lt;BR /&gt;Booting from mmc ...&lt;BR /&gt;36385 bytes read in 16 ms (2.2 MiB/s)&lt;BR /&gt;267112 bytes read in 26 ms (9.8 MiB/s)&lt;BR /&gt;## Booting kernel from Legacy Image at 84000000 ...&lt;BR /&gt; Image Name:&lt;BR /&gt; Image Type: ARM Linux Kernel Image (uncompressed)&lt;BR /&gt; Data Size: 267048 Bytes = 260.8 KiB&lt;BR /&gt; Load Address: 84000000&lt;BR /&gt; Entry Point: 84000000&lt;BR /&gt; Verifying Checksum ... OK&lt;BR /&gt;## Flattened Device Tree blob at 83000000&lt;BR /&gt; Booting using the fdt blob at 0x83000000&lt;BR /&gt; Loading Kernel Image ... OK&lt;BR /&gt; Using Device Tree in place at 83000000, end 8300be20&lt;BR /&gt;Modify /soc/aips-bus@02200000/epdc@0228c000:status disabled&lt;BR /&gt;ft_system_setup for mx6&lt;/P&gt;&lt;P&gt;Starting kernel ...&lt;/P&gt;&lt;P&gt;E/TC:0 plat_rng_init:354 Warning: seeding RNG with zeroes&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 02 Feb 2019 12:02:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-to-settle-the-error-in-Yocto-build-system/m-p/842142#M129146</guid>
      <dc:creator>chum</dc:creator>
      <dc:date>2019-02-02T12:02:59Z</dc:date>
    </item>
  </channel>
</rss>