<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: Problems setting up an MIMX1060 EVK</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Problems-setting-up-an-MIMX1060-EVK/m-p/841905#M129113</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Martin,&lt;/P&gt;&lt;P&gt;I don't have a RT1060, but I do have the RT1064-EVK (see &lt;A class="link-titled" href="https://mcuoneclipse.com/2018/12/28/first-steps-with-the-nxp-i-mx-rt1064-evk-board/" title="https://mcuoneclipse.com/2018/12/28/first-steps-with-the-nxp-i-mx-rt1064-evk-board/"&gt;First Steps with the NXP i.MX RT1064-EVK Board | MCU on Eclipse&lt;/A&gt;&amp;nbsp;). From what I see is that the RT1060-EVK is using the same OpenSDA processor, and on these boards it is a LPC device and not the Kinetis K20 as on other OpenSDA designs. So that k20dx_mimxrt1050_evk_hyper_if_crc.bin won't work for that LPC device, as the code is for K20 and not for the LPC4370.&lt;/P&gt;&lt;P&gt;To my understanding, there is no Segger OpenSDA binary for the LPC4370 (yet).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;I hope this helps,&lt;/P&gt;&lt;P&gt;Erich&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sun, 30 Dec 2018 15:36:00 GMT</pubDate>
    <dc:creator>BlackNight</dc:creator>
    <dc:date>2018-12-30T15:36:00Z</dc:date>
    <item>
      <title>Problems setting up an MIMX1060 EVK</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Problems-setting-up-an-MIMX1060-EVK/m-p/841902#M129110</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am trying to run this evaluation board with JLINK debugger, but never seem able to get USB operating.&amp;nbsp; I downloaded&amp;nbsp;k20dx_mimxrt1050_evk_hyper_if_crc.bin and copied into maintenance folder, but the J-LINK usb port never appears and the J-LINK app never sees a USB emulator.&amp;nbsp; When I copy the file to the maintenance folder, do I wait before re-powering the unit, or re-power immediately.&amp;nbsp; If I wait, I get a fail.txt with a transfer timeout.&amp;nbsp; Instructions are not too clear, perhaps there is a site with more comprehensive steps of what to do and what to expect somewhere.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 26 Oct 2018 21:33:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Problems-setting-up-an-MIMX1060-EVK/m-p/841902#M129110</guid>
      <dc:creator>jautry</dc:creator>
      <dc:date>2018-10-26T21:33:12Z</dc:date>
    </item>
    <item>
      <title>Re: Problems setting up an MIMX1060 EVK</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Problems-setting-up-an-MIMX1060-EVK/m-p/841903#M129111</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;To make me able to accurately answer your question, please specify your task clearly. Do you want to use the Segger J-LINK JTAG probe with corresponding host software to directly debug the i.MX RT1060 processor? Or, do you want to use the OpenSDA debug interface, implemented with the on-board LPC4322 microcontroller on J41 USB connector? Please specify.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Artur&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 31 Oct 2018 12:21:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Problems-setting-up-an-MIMX1060-EVK/m-p/841903#M129111</guid>
      <dc:creator>art</dc:creator>
      <dc:date>2018-10-31T12:21:14Z</dc:date>
    </item>
    <item>
      <title>Re: Problems setting up an MIMX1060 EVK</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Problems-setting-up-an-MIMX1060-EVK/m-p/841904#M129112</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I wanted to use the OpenSDA via the USB connector&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 31 Oct 2018 23:03:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Problems-setting-up-an-MIMX1060-EVK/m-p/841904#M129112</guid>
      <dc:creator>jautry</dc:creator>
      <dc:date>2018-10-31T23:03:50Z</dc:date>
    </item>
    <item>
      <title>Re: Problems setting up an MIMX1060 EVK</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Problems-setting-up-an-MIMX1060-EVK/m-p/841905#M129113</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Martin,&lt;/P&gt;&lt;P&gt;I don't have a RT1060, but I do have the RT1064-EVK (see &lt;A class="link-titled" href="https://mcuoneclipse.com/2018/12/28/first-steps-with-the-nxp-i-mx-rt1064-evk-board/" title="https://mcuoneclipse.com/2018/12/28/first-steps-with-the-nxp-i-mx-rt1064-evk-board/"&gt;First Steps with the NXP i.MX RT1064-EVK Board | MCU on Eclipse&lt;/A&gt;&amp;nbsp;). From what I see is that the RT1060-EVK is using the same OpenSDA processor, and on these boards it is a LPC device and not the Kinetis K20 as on other OpenSDA designs. So that k20dx_mimxrt1050_evk_hyper_if_crc.bin won't work for that LPC device, as the code is for K20 and not for the LPC4370.&lt;/P&gt;&lt;P&gt;To my understanding, there is no Segger OpenSDA binary for the LPC4370 (yet).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;I hope this helps,&lt;/P&gt;&lt;P&gt;Erich&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 30 Dec 2018 15:36:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Problems-setting-up-an-MIMX1060-EVK/m-p/841905#M129113</guid>
      <dc:creator>BlackNight</dc:creator>
      <dc:date>2018-12-30T15:36:00Z</dc:date>
    </item>
  </channel>
</rss>