<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックSupport for edt-ft5x06</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Support-for-edt-ft5x06/m-p/840844#M128984</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear all,&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt; we have got a capacitive touchscreen display (ETMV570G0BDHU) which we would like to test with our Sabreboard MCIMX7SABRE. Because the default configuration in device tree file only support resistive touch, I disabled it and add our configuration for capacitive touch. The touch driver edt-ft5x06 was installed in linux kernel through CONFIG TOUCHSCREEN_EDT_FT5X06. The linux kernel was built with a yocto system. The kernel version is 4.12. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;After booting, we saw that the driver is connected with the device. However, touch doesn't work. We didn't see any interrupt coming from display if we press on the screen.&amp;nbsp; &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Do you have any working example of device tree file for capacitive touch on this board? &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;best regards &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Pan&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 06 Dec 2018 13:25:45 GMT</pubDate>
    <dc:creator>panli</dc:creator>
    <dc:date>2018-12-06T13:25:45Z</dc:date>
    <item>
      <title>Support for edt-ft5x06</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Support-for-edt-ft5x06/m-p/840844#M128984</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear all,&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt; we have got a capacitive touchscreen display (ETMV570G0BDHU) which we would like to test with our Sabreboard MCIMX7SABRE. Because the default configuration in device tree file only support resistive touch, I disabled it and add our configuration for capacitive touch. The touch driver edt-ft5x06 was installed in linux kernel through CONFIG TOUCHSCREEN_EDT_FT5X06. The linux kernel was built with a yocto system. The kernel version is 4.12. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;After booting, we saw that the driver is connected with the device. However, touch doesn't work. We didn't see any interrupt coming from display if we press on the screen.&amp;nbsp; &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Do you have any working example of device tree file for capacitive touch on this board? &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;best regards &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Pan&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 06 Dec 2018 13:25:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Support-for-edt-ft5x06/m-p/840844#M128984</guid>
      <dc:creator>panli</dc:creator>
      <dc:date>2018-12-06T13:25:45Z</dc:date>
    </item>
    <item>
      <title>Re: Support for edt-ft5x06</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Support-for-edt-ft5x06/m-p/840845#M128985</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Pan&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;FT5X&lt;/SPAN&gt; is supported on some third party boards, for example imx6qdl-sabrelite.dtsi&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://github.com/boundarydevices/linux-imx6/blob/boundary-imx_4.9.x_2.0.0_ga/arch/arm/boot/dts/imx6qdl-sabrelite.dtsi" title="https://github.com/boundarydevices/linux-imx6/blob/boundary-imx_4.9.x_2.0.0_ga/arch/arm/boot/dts/imx6qdl-sabrelite.dtsi"&gt;linux-imx6/imx6qdl-sabrelite.dtsi at boundary-imx_4.9.x_2.0.0_ga · boundarydevices/linux-imx6 · GitHub&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://github.com/boundarydevices/linux-imx6/blob/boundary-imx_4.9.x_2.0.0_ga/arch/arm/boot/dts/imx6ul-tx6ul.dtsi" title="https://github.com/boundarydevices/linux-imx6/blob/boundary-imx_4.9.x_2.0.0_ga/arch/arm/boot/dts/imx6ul-tx6ul.dtsi"&gt;linux-imx6/imx6ul-tx6ul.dtsi at boundary-imx_4.9.x_2.0.0_ga · boundarydevices/linux-imx6 · GitHub&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/311450"&gt;Sabrelite: New FT5x06 touch screen and swapped Y (input_set_abs_params)&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://patchwork.kernel.org/patch/9787423/" title="https://patchwork.kernel.org/patch/9787423/"&gt;[RFC,1/3] ARM: dts: imx7d: add imx7d-phyboard-zeta - Patchwork&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 07 Dec 2018 00:34:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Support-for-edt-ft5x06/m-p/840845#M128985</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2018-12-07T00:34:24Z</dc:date>
    </item>
  </channel>
</rss>