<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Android(oreo) compilation issue</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Android-oreo-compilation-issue/m-p/840833#M128981</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; refer to&amp;nbsp; the following thread&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/message/1038423"&gt;https://community.nxp.com/message/1038423&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 26 Jul 2018 03:21:00 GMT</pubDate>
    <dc:creator>Yuri</dc:creator>
    <dc:date>2018-07-26T03:21:00Z</dc:date>
    <item>
      <title>Android(oreo) compilation issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Android-oreo-compilation-issue/m-p/840832#M128980</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hii,&lt;/P&gt;&lt;P&gt;I was compiling the android source code for&amp;nbsp;sabresd_6dq with the freshly downloaded code, but it fails everytime. Here are the logs,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;:~/android_build$ sudo make -j4&lt;BR /&gt;============================================&lt;BR /&gt;PLATFORM_VERSION_CODENAME=REL&lt;BR /&gt;PLATFORM_VERSION=8.0.0&lt;BR /&gt;TARGET_PRODUCT=aosp_arm&lt;BR /&gt;TARGET_BUILD_VARIANT=eng&lt;BR /&gt;TARGET_BUILD_TYPE=release&lt;BR /&gt;TARGET_ARCH=arm&lt;BR /&gt;TARGET_ARCH_VARIANT=armv7-a&lt;BR /&gt;TARGET_CPU_VARIANT=generic&lt;BR /&gt;HOST_ARCH=x86_64&lt;BR /&gt;HOST_2ND_ARCH=x86&lt;BR /&gt;HOST_OS=linux&lt;BR /&gt;HOST_OS_EXTRA=Linux-4.4.0-31-generic-x86_64-with-Ubuntu-16.04-xenial&lt;BR /&gt;HOST_CROSS_OS=windows&lt;BR /&gt;HOST_CROSS_ARCH=x86&lt;BR /&gt;HOST_CROSS_2ND_ARCH=x86_64&lt;BR /&gt;HOST_BUILD_TYPE=release&lt;BR /&gt;BUILD_ID=OPD1.170816.018&lt;BR /&gt;OUT_DIR=out&lt;BR /&gt;============================================&lt;BR /&gt;[38/38] bootstrap out/soong/.minibootstrap/build.ninja.in&lt;BR /&gt;[1/2] out/soong/.bootstrap/bin/minibp out/soong/.minibootstrap/build.ninja.in&lt;BR /&gt;[4/4] out/soong/.bootstrap/bin/minibp out/soong/.bootstrap/build.ninja&lt;BR /&gt;[791/792] glob vendor/*/*/Android.bp&lt;BR /&gt;[47/47] out/soong/.bootstrap/bin/soong_build out/soong/build.ninja&lt;BR /&gt;FAILED: out/soong/build.ninja&lt;BR /&gt;out/soong/.bootstrap/bin/soong_build -t -b out/soong -d out/soong/build.ninja.d -o out/soong/build.ninja Android.bp&lt;BR /&gt;error: frameworks/av/media/libstagefright/Android.bp:7:1: module "libstagefright" variant "android_arm_armv7-a_shared_core": source path vendor/nxp/fsl-codec/ghdr/common does not exist&lt;BR /&gt;ninja: build stopped: subcommand failed.&lt;BR /&gt;12:30:47 soong failed with: exit status 1&lt;BR /&gt;build/core/main.mk:21: recipe for target 'run_soong_ui' failed&lt;BR /&gt;make: *** [run_soong_ui] Error 1&lt;BR /&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 23 Jul 2018 07:04:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Android-oreo-compilation-issue/m-p/840832#M128980</guid>
      <dc:creator>pavandornadula7</dc:creator>
      <dc:date>2018-07-23T07:04:47Z</dc:date>
    </item>
    <item>
      <title>Re: Android(oreo) compilation issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Android-oreo-compilation-issue/m-p/840833#M128981</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; refer to&amp;nbsp; the following thread&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/message/1038423"&gt;https://community.nxp.com/message/1038423&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 26 Jul 2018 03:21:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Android-oreo-compilation-issue/m-p/840833#M128981</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2018-07-26T03:21:00Z</dc:date>
    </item>
  </channel>
</rss>