<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processorsのトピックi.MX6UL Initial Load</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6UL-Initial-Load/m-p/839990#M128857</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have a board with a i.MX6UL processor. UART1 is the only serial boot interface connected on the board. I was wondering what the standard procedure for initially loading u-boot or a first stage bootloader (FSBL) onto the system is.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I can communicate with the chip through the serial download protocol but I am having trouble transferring a file of more than 2kB (the protocol just seems to stop responding).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have tried using the program at&amp;nbsp;&lt;A class="jivelink1" href="https://github.com/boundarydevices/imx_usb_loader" title="https://github.com/boundarydevices/imx_usb_loader"&gt;https://github.com/boundarydevices/imx_usb_loader&lt;/A&gt;&amp;nbsp;with little success.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The JTAG port is available on the board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any advice that could be offered on how to go about initial load would be greatly appreciated.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 09 Aug 2018 17:01:22 GMT</pubDate>
    <dc:creator>vandoornum</dc:creator>
    <dc:date>2018-08-09T17:01:22Z</dc:date>
    <item>
      <title>i.MX6UL Initial Load</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6UL-Initial-Load/m-p/839990#M128857</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have a board with a i.MX6UL processor. UART1 is the only serial boot interface connected on the board. I was wondering what the standard procedure for initially loading u-boot or a first stage bootloader (FSBL) onto the system is.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I can communicate with the chip through the serial download protocol but I am having trouble transferring a file of more than 2kB (the protocol just seems to stop responding).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have tried using the program at&amp;nbsp;&lt;A class="jivelink1" href="https://github.com/boundarydevices/imx_usb_loader" title="https://github.com/boundarydevices/imx_usb_loader"&gt;https://github.com/boundarydevices/imx_usb_loader&lt;/A&gt;&amp;nbsp;with little success.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The JTAG port is available on the board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any advice that could be offered on how to go about initial load would be greatly appreciated.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 09 Aug 2018 17:01:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6UL-Initial-Load/m-p/839990#M128857</guid>
      <dc:creator>vandoornum</dc:creator>
      <dc:date>2018-08-09T17:01:22Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX6UL Initial Load</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6UL-Initial-Load/m-p/839991#M128858</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jay&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;for jtag usage one can look on&lt;/P&gt;&lt;P&gt;AN5229 ARM DS-5 Development Studio Debug i.MX6UL-EVK&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://www.nxp.com/docs/en/application-note/AN5229.pdf" title="https://www.nxp.com/docs/en/application-note/AN5229.pdf"&gt;https://www.nxp.com/docs/en/application-note/AN5229.pdf&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;or write own application loading code through uart using sect.8.9.3 Serial Download protocol&lt;/P&gt;&lt;P&gt;i.MX6UL Reference Manual &lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fwww.nxp.com%2Fdocs%2Fen%2Freference-manual%2FIMX6ULRM.pdf" rel="nofollow" target="_blank"&gt;http://www.nxp.com/docs/en/reference-manual/IMX6ULRM.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 10 Aug 2018 01:37:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6UL-Initial-Load/m-p/839991#M128858</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2018-08-10T01:37:49Z</dc:date>
    </item>
  </channel>
</rss>