<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Boot problems with yocto sumo on imx8 in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Boot-problems-with-yocto-sumo-on-imx8/m-p/838219#M128660</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Erica Magari,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The 4.14 BSP is in beta status right now so it’s not currently supported, but I would double check the MACHINE you are setting up as I couldn’t find imx8qmlpddr4arm2 on the available machine configurations.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My apologies for the inconvenience.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 05 Dec 2018 20:51:08 GMT</pubDate>
    <dc:creator>gusarambula</dc:creator>
    <dc:date>2018-12-05T20:51:08Z</dc:date>
    <item>
      <title>Boot problems with yocto sumo on imx8</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Boot-problems-with-yocto-sumo-on-imx8/m-p/838218#M128659</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, I am using Yocto sumo on nxp imx8qmlpddr4arm2, with kernel 4.14. I have normally compiled a wayland image and flashed it on my sdcard but when I boot the board nothing happens. It seems that the bootloader is not loaded. I am using minicom to see the board output. Am I missing some steps? Thank you&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 05 Dec 2018 13:31:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Boot-problems-with-yocto-sumo-on-imx8/m-p/838218#M128659</guid>
      <dc:creator>s233199</dc:creator>
      <dc:date>2018-12-05T13:31:38Z</dc:date>
    </item>
    <item>
      <title>Re: Boot problems with yocto sumo on imx8</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Boot-problems-with-yocto-sumo-on-imx8/m-p/838219#M128660</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Erica Magari,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The 4.14 BSP is in beta status right now so it’s not currently supported, but I would double check the MACHINE you are setting up as I couldn’t find imx8qmlpddr4arm2 on the available machine configurations.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My apologies for the inconvenience.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 05 Dec 2018 20:51:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Boot-problems-with-yocto-sumo-on-imx8/m-p/838219#M128660</guid>
      <dc:creator>gusarambula</dc:creator>
      <dc:date>2018-12-05T20:51:08Z</dc:date>
    </item>
    <item>
      <title>Re: Boot problems with yocto sumo on imx8</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Boot-problems-with-yocto-sumo-on-imx8/m-p/838220#M128661</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Gusarambula, thank you for the answer. Previously I was using Yocto Morty, but I needed support for spi slave mode and morty's kernel does not offer it. I also found this patch (&lt;A class="link-titled" href="https://patchwork.kernel.org/patch/10678195/" title="https://patchwork.kernel.org/patch/10678195/"&gt;spi: lpspi: Add Slave Mode support for LPSPI - Patchwork&lt;/A&gt; ) wich provides spi slave support for mx8qm too., but it supposes to use the new kernel. How can I load this new kernel in my board then? I thought I could solve my problems with sumo, but if this is not the case, I wonder how I can achieve it.&amp;nbsp; Thank you for your help,&lt;/P&gt;&lt;P&gt;Erica&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 06 Dec 2018 15:10:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Boot-problems-with-yocto-sumo-on-imx8/m-p/838220#M128661</guid>
      <dc:creator>s233199</dc:creator>
      <dc:date>2018-12-06T15:10:11Z</dc:date>
    </item>
  </channel>
</rss>