<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 8-bit lcd parallel bus interface</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/8-bit-lcd-parallel-bus-interface/m-p/837941#M128618</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We have a 8-bit parallel bus LCD connected to EIM_A21 (DATA16) to EIM_D27(DATA23). The data to to be sent should be RGB565 but in a 8-bit in two clock clock cycles fashion. I know we should change the microcodes found in ipu_disp.c but I have no clue as of how to do this. We are using Linux&amp;nbsp;3.14.52.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I tried adding RGB565 to the same if statements for YUYV and added some changes to the&amp;nbsp;_ipu_init_dc_mappings function. but it still does not give me two clock cycles per pixel.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can someone please help.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 29 Aug 2018 06:39:06 GMT</pubDate>
    <dc:creator>reuelhaavrahami</dc:creator>
    <dc:date>2018-08-29T06:39:06Z</dc:date>
    <item>
      <title>8-bit lcd parallel bus interface</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/8-bit-lcd-parallel-bus-interface/m-p/837941#M128618</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We have a 8-bit parallel bus LCD connected to EIM_A21 (DATA16) to EIM_D27(DATA23). The data to to be sent should be RGB565 but in a 8-bit in two clock clock cycles fashion. I know we should change the microcodes found in ipu_disp.c but I have no clue as of how to do this. We are using Linux&amp;nbsp;3.14.52.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I tried adding RGB565 to the same if statements for YUYV and added some changes to the&amp;nbsp;_ipu_init_dc_mappings function. but it still does not give me two clock cycles per pixel.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can someone please help.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 29 Aug 2018 06:39:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/8-bit-lcd-parallel-bus-interface/m-p/837941#M128618</guid>
      <dc:creator>reuelhaavrahami</dc:creator>
      <dc:date>2018-08-29T06:39:06Z</dc:date>
    </item>
    <item>
      <title>Re: 8-bit lcd parallel bus interface</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/8-bit-lcd-parallel-bus-interface/m-p/837942#M128619</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Reul&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;number of IPU clock cycles was available for programming in early IPU&lt;/P&gt;&lt;P&gt;versions, for example in i.MX31 IPU DI Display Access Cycles Count Register (DI_DISP_ACC_CC).&lt;/P&gt;&lt;P&gt;Below example of such microcodes programming&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/message/294603#294603"&gt;https://community.nxp.com/message/294603#294603&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Usually such kind of support can be provided with&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://www.nxp.com/support/support/nxp-professional-services:PROFESSIONAL-SERVICE" title="https://www.nxp.com/support/support/nxp-professional-services:PROFESSIONAL-SERVICE"&gt;NXP Professional Services|NXP&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 29 Aug 2018 10:49:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/8-bit-lcd-parallel-bus-interface/m-p/837942#M128619</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2018-08-29T10:49:14Z</dc:date>
    </item>
  </channel>
</rss>