<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processorsのトピックabout  I.MX6 linux kernel4.1 - rt18  used GPU question?</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/about-I-MX6-linux-kernel4-1-rt18-used-GPU-question/m-p/837916#M128612</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The SDK I used was imx-4.1-krogoth, compiled with DISTRO = fsl-imx-wayland MACHINE = imx6qsabresd source fsl-setup-release.sh-b build, compiled with bitbake fsl-image-gui.&lt;/P&gt;&lt;P&gt;But Linux kernel I want to add patch-4.1.15-rt18.patch on&amp;nbsp; the bsp linux4.1 kernel.&amp;nbsp; Will the GPU still work&amp;nbsp;ok? Is GPU SDK specified only in version 4.1?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 29 Aug 2018 06:38:52 GMT</pubDate>
    <dc:creator>lvxiong</dc:creator>
    <dc:date>2018-08-29T06:38:52Z</dc:date>
    <item>
      <title>about  I.MX6 linux kernel4.1 - rt18  used GPU question?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/about-I-MX6-linux-kernel4-1-rt18-used-GPU-question/m-p/837916#M128612</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The SDK I used was imx-4.1-krogoth, compiled with DISTRO = fsl-imx-wayland MACHINE = imx6qsabresd source fsl-setup-release.sh-b build, compiled with bitbake fsl-image-gui.&lt;/P&gt;&lt;P&gt;But Linux kernel I want to add patch-4.1.15-rt18.patch on&amp;nbsp; the bsp linux4.1 kernel.&amp;nbsp; Will the GPU still work&amp;nbsp;ok? Is GPU SDK specified only in version 4.1?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 29 Aug 2018 06:38:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/about-I-MX6-linux-kernel4-1-rt18-used-GPU-question/m-p/837916#M128612</guid>
      <dc:creator>lvxiong</dc:creator>
      <dc:date>2018-08-29T06:38:52Z</dc:date>
    </item>
    <item>
      <title>Re: about  I.MX6 linux kernel4.1 - rt18  used GPU question?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/about-I-MX6-linux-kernel4-1-rt18-used-GPU-question/m-p/837917#M128613</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi James&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I believe GPU will still work&amp;nbsp;ok in your case.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 29 Aug 2018 23:52:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/about-I-MX6-linux-kernel4-1-rt18-used-GPU-question/m-p/837917#M128613</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2018-08-29T23:52:12Z</dc:date>
    </item>
  </channel>
</rss>