<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: boot kernel use tftp in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/boot-kernel-use-tftp/m-p/837911#M128611</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jianwen&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;for tftp configuration and usage one can check sect.&amp;nbsp;sect.4.4.1.1 Downloading an image to MMC/SD,&lt;/P&gt;&lt;P&gt;sect.4.7.5 Running the Linux image from NFS attached Linux Guide&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 29 Dec 2018 02:38:22 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2018-12-29T02:38:22Z</dc:date>
    <item>
      <title>boot kernel use tftp</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/boot-kernel-use-tftp/m-p/837910#M128610</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I want to run Linux on my board,imx6q-sabresd.My step is:&lt;/P&gt;&lt;P&gt;=&amp;gt;tftp 0x10000000 zImage&lt;/P&gt;&lt;P&gt;=&amp;gt;tftp 0x20000000 imx6q-sabresd.dtb&lt;/P&gt;&lt;P&gt;=&amp;gt;bootz 0x10000000 - 0x20000000&lt;/P&gt;&lt;P&gt;now,the Linux is booting,I want to know ,why the address is 0x10000000 and 0x20000000? if I use other address,like bootz 0x12000000 - 0x18000000,the kernel boot failed.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 28 Dec 2018 07:04:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/boot-kernel-use-tftp/m-p/837910#M128610</guid>
      <dc:creator>jianwenzhang</dc:creator>
      <dc:date>2018-12-28T07:04:52Z</dc:date>
    </item>
    <item>
      <title>Re: boot kernel use tftp</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/boot-kernel-use-tftp/m-p/837911#M128611</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jianwen&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;for tftp configuration and usage one can check sect.&amp;nbsp;sect.4.4.1.1 Downloading an image to MMC/SD,&lt;/P&gt;&lt;P&gt;sect.4.7.5 Running the Linux image from NFS attached Linux Guide&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 29 Dec 2018 02:38:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/boot-kernel-use-tftp/m-p/837911#M128611</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2018-12-29T02:38:22Z</dc:date>
    </item>
  </channel>
</rss>