<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックSecond camera interface</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Second-camera-interface/m-p/837835#M128597</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We have two cameras connected to IMX6D. The first CSI0 work fine. The second CSI1 has an shift on the data. I suppose that due to the fact that CSI0 is taken from DATA04 to DATA19, it does a bit-shift of 4 to correct it towards the memory buffer. Seemingly the CSI1 does the same thing, however our camera interface is connected to DATA00 to DATA15. This causes the data to shift 4 bits thus we don't get the correct data.Where can I fix this issue?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We are using Linux kernel&amp;nbsp;3.14.52 on a custom board.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 29 Aug 2018 06:21:46 GMT</pubDate>
    <dc:creator>reuelhaavrahami</dc:creator>
    <dc:date>2018-08-29T06:21:46Z</dc:date>
    <item>
      <title>Second camera interface</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Second-camera-interface/m-p/837835#M128597</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We have two cameras connected to IMX6D. The first CSI0 work fine. The second CSI1 has an shift on the data. I suppose that due to the fact that CSI0 is taken from DATA04 to DATA19, it does a bit-shift of 4 to correct it towards the memory buffer. Seemingly the CSI1 does the same thing, however our camera interface is connected to DATA00 to DATA15. This causes the data to shift 4 bits thus we don't get the correct data.Where can I fix this issue?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We are using Linux kernel&amp;nbsp;3.14.52 on a custom board.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 29 Aug 2018 06:21:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Second-camera-interface/m-p/837835#M128597</guid>
      <dc:creator>reuelhaavrahami</dc:creator>
      <dc:date>2018-08-29T06:21:46Z</dc:date>
    </item>
    <item>
      <title>Re: Second camera interface</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Second-camera-interface/m-p/837836#M128598</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Reuel&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;sensor connection to IPU CSI is fixed and depends on used format, described on&lt;/P&gt;&lt;P&gt;sect.4.12.10.1 IPU Sensor Interface Signal Mapping&amp;nbsp;i.MX6DQ Datasheet&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.nxp.com/docs/en/data-sheet/IMX6DQCEC.pdf"&gt;http://www.nxp.com/docs/en/data-sheet/IMX6DQCEC.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/67754i91E8C329769A88F2/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_2.jpg" alt="pastedImage_2.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;so shifting may be due to other reasons.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 29 Aug 2018 09:20:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Second-camera-interface/m-p/837836#M128598</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2018-08-29T09:20:47Z</dc:date>
    </item>
    <item>
      <title>Re: Second camera interface</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Second-camera-interface/m-p/837837#M128599</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;When you say "the sensor connections to the IPU CSI is fixed", is that a hardware limitation or can that be changed through changing the driver?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 29 Aug 2018 12:16:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Second-camera-interface/m-p/837837#M128599</guid>
      <dc:creator>reuelhaavrahami</dc:creator>
      <dc:date>2018-08-29T12:16:17Z</dc:date>
    </item>
    <item>
      <title>Re: Second camera interface</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Second-camera-interface/m-p/837838#M128600</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;right, this is a hardware limitation and described in sect.4.12.10.1&lt;/P&gt;&lt;P&gt;IPU Sensor Interface Signal Mapping&amp;nbsp;i.MX6DQ Datasheet&lt;/P&gt;&lt;P&gt;&lt;A class="" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fwww.nxp.com%2Fdocs%2Fen%2Fdata-sheet%2FIMX6DQCEC.pdf" rel="nofollow" target="_blank"&gt;http://www.nxp.com/docs/en/data-sheet/IMX6DQCEC.pdf&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 29 Aug 2018 14:29:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Second-camera-interface/m-p/837838#M128600</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2018-08-29T14:29:37Z</dc:date>
    </item>
  </channel>
</rss>