<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic GPT Input Capture Linux Driver in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/GPT-Input-Capture-Linux-Driver/m-p/837311#M128505</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am running on an iMX6QDL and I would like to configure the GPT input capture channels. I have not located any Linux drivers that allow me to configure the GPT registers and read the count register. I have seen the imx6-gpt driver and it doesn't seem to do much other than set the clocks and enable the interrupt. I would like to configure the input channels as well. Anyone have any thoughts on how to achieve this?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 08 Oct 2018 20:21:32 GMT</pubDate>
    <dc:creator>aliismail</dc:creator>
    <dc:date>2018-10-08T20:21:32Z</dc:date>
    <item>
      <title>GPT Input Capture Linux Driver</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/GPT-Input-Capture-Linux-Driver/m-p/837311#M128505</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am running on an iMX6QDL and I would like to configure the GPT input capture channels. I have not located any Linux drivers that allow me to configure the GPT registers and read the count register. I have seen the imx6-gpt driver and it doesn't seem to do much other than set the clocks and enable the interrupt. I would like to configure the input channels as well. Anyone have any thoughts on how to achieve this?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 08 Oct 2018 20:21:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/GPT-Input-Capture-Linux-Driver/m-p/837311#M128505</guid>
      <dc:creator>aliismail</dc:creator>
      <dc:date>2018-10-08T20:21:32Z</dc:date>
    </item>
    <item>
      <title>Re: GPT Input Capture Linux Driver</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/GPT-Input-Capture-Linux-Driver/m-p/837312#M128506</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Ali&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can look on timer-imx-gpt.c&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://patchwork.kernel.org/patch/9177095/" title="https://patchwork.kernel.org/patch/9177095/"&gt;[27/38] clocksource/drivers/imx: add input capture support - Patchwork&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 09 Oct 2018 00:59:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/GPT-Input-Capture-Linux-Driver/m-p/837312#M128506</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2018-10-09T00:59:56Z</dc:date>
    </item>
    <item>
      <title>Re: GPT Input Capture Linux Driver</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/GPT-Input-Capture-Linux-Driver/m-p/837313#M128507</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks a lot Igor! Do you happen to know if there is a more updated patch?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 09 Oct 2018 18:22:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/GPT-Input-Capture-Linux-Driver/m-p/837313#M128507</guid>
      <dc:creator>aliismail</dc:creator>
      <dc:date>2018-10-09T18:22:51Z</dc:date>
    </item>
  </channel>
</rss>