<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: mx6 camera preview black border about 10dp</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/mx6-camera-preview-black-border-about-10dp/m-p/836983#M128466</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Running,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You have a bad configuration of your Camera Settings refer to the DTS (device Tree) where the camera it is connected and change the resolution or your camera, or you are using a wrong driver for the camera and the settings from the firmware are incorrect which you need to add a different driver.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards&lt;/P&gt;&lt;P&gt;TIC Support Team&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 19 Jul 2018 13:26:38 GMT</pubDate>
    <dc:creator>jamesbone</dc:creator>
    <dc:date>2018-07-19T13:26:38Z</dc:date>
    <item>
      <title>mx6 camera preview black border about 10dp</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/mx6-camera-preview-black-border-about-10dp/m-p/836982#M128465</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;call camera startPreview ，the preview frame has about 10dp black border, Could anybody tell haw to do...&amp;nbsp;thx&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="QQ图片20180630180843.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/64632i060AFA9CBE660B83/image-size/large?v=v2&amp;amp;px=999" role="button" title="QQ图片20180630180843.png" alt="QQ图片20180630180843.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 30 Jun 2018 10:09:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/mx6-camera-preview-black-border-about-10dp/m-p/836982#M128465</guid>
      <dc:creator>121762540</dc:creator>
      <dc:date>2018-06-30T10:09:57Z</dc:date>
    </item>
    <item>
      <title>Re: mx6 camera preview black border about 10dp</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/mx6-camera-preview-black-border-about-10dp/m-p/836983#M128466</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Running,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You have a bad configuration of your Camera Settings refer to the DTS (device Tree) where the camera it is connected and change the resolution or your camera, or you are using a wrong driver for the camera and the settings from the firmware are incorrect which you need to add a different driver.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards&lt;/P&gt;&lt;P&gt;TIC Support Team&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 19 Jul 2018 13:26:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/mx6-camera-preview-black-border-about-10dp/m-p/836983#M128466</guid>
      <dc:creator>jamesbone</dc:creator>
      <dc:date>2018-07-19T13:26:38Z</dc:date>
    </item>
  </channel>
</rss>