<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Compiler problem with KSZ8895</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Compiler-problem-with-KSZ8895/m-p/836238#M128377</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Emin&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can look at Yocto project documentation&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-334088"&gt;Adding the WF111 Driver to the i.MX6 Yocto BSP&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/444387"&gt;https://community.nxp.com/thread/444387&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-95003"&gt;i.MX Yocto Project: How can I (quickly) modify the kernel and test it?&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 08 Oct 2018 23:15:14 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2018-10-08T23:15:14Z</dc:date>
    <item>
      <title>Compiler problem with KSZ8895</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Compiler-problem-with-KSZ8895/m-p/836237#M128376</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am using IMX7dea Ucom Som board and Ksz8895 ethernet switch chip.I used SPI interface between mpu and ethernet chip.I add linux driver to mey kernel but i didnt see xx.o file.I guss ccross compile didnt worked.Ant it didnt creat xx.o files.I used &lt;A data-doctype="Software Library" data-type="SoftwareLibrary" href="http://www.microchip.com/SWLibraryWeb/product.aspx?product=KSZ8895 Software Linux 3.3" target="_blank"&gt;KSZ8895 Linux driver for revision 3.3 tared&lt;/A&gt;.&lt;/P&gt;&lt;P&gt;How can I fix this?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also I saw writing blove these in KSZ8895MQ/RQ Evaluation Board User’s Guide &lt;BR /&gt; &lt;BR /&gt;The KSZ8895 will power up initial default configuration with the start switch in register 1 bit 0 &lt;BR /&gt;= ‘0’ which means the switch is “off”. You can set the bit 0 =’1’ to start switch.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;How Can I change this register with spi interface?&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 08 Oct 2018 09:02:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Compiler-problem-with-KSZ8895/m-p/836237#M128376</guid>
      <dc:creator>emintolgasivri</dc:creator>
      <dc:date>2018-10-08T09:02:55Z</dc:date>
    </item>
    <item>
      <title>Re: Compiler problem with KSZ8895</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Compiler-problem-with-KSZ8895/m-p/836238#M128377</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Emin&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can look at Yocto project documentation&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-334088"&gt;Adding the WF111 Driver to the i.MX6 Yocto BSP&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/444387"&gt;https://community.nxp.com/thread/444387&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-95003"&gt;i.MX Yocto Project: How can I (quickly) modify the kernel and test it?&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 08 Oct 2018 23:15:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Compiler-problem-with-KSZ8895/m-p/836238#M128377</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2018-10-08T23:15:14Z</dc:date>
    </item>
  </channel>
</rss>