<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic u-boot-fw-utils issue with mx6ul_14x14_evk in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/u-boot-fw-utils-issue-with-mx6ul-14x14-evk/m-p/835987#M128341</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;we are using&amp;nbsp;imx6ul evaluation kit "mx6ul_14x14_evk".&lt;/P&gt;&lt;P&gt;We have built the u-boot-fw-utils by adding&amp;nbsp;"CORE_IMAGE_EXTRA_INSTALL += "u-boot-fw-utils" in local.conf file.&lt;/P&gt;&lt;P&gt;We are facing two issues:&lt;/P&gt;&lt;P&gt;1. Not able to update the existing boot variable. We tried updating the boot delay but it is not reflected while rebooting.&lt;/P&gt;&lt;P&gt;2. We are not able to add the new variables. When we execute "fw_setenv board_name evalkit" then we can see it using fw_printenv. But if we reboot and check the boot variables using the command "printenv" then the variable is not shown there.&lt;/P&gt;&lt;P&gt;3. We also tried adding the variable through&amp;nbsp;CONFIG_EXTRA_ENV_SETTINGS in mx6ul_14x14_evk.h&amp;nbsp; at&amp;nbsp;./tmp/work/../../include/configs/ but it is also not shown when we use fw_printenv.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 27 Dec 2018 12:04:13 GMT</pubDate>
    <dc:creator>hardikpadhariya</dc:creator>
    <dc:date>2018-12-27T12:04:13Z</dc:date>
    <item>
      <title>u-boot-fw-utils issue with mx6ul_14x14_evk</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/u-boot-fw-utils-issue-with-mx6ul-14x14-evk/m-p/835987#M128341</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;we are using&amp;nbsp;imx6ul evaluation kit "mx6ul_14x14_evk".&lt;/P&gt;&lt;P&gt;We have built the u-boot-fw-utils by adding&amp;nbsp;"CORE_IMAGE_EXTRA_INSTALL += "u-boot-fw-utils" in local.conf file.&lt;/P&gt;&lt;P&gt;We are facing two issues:&lt;/P&gt;&lt;P&gt;1. Not able to update the existing boot variable. We tried updating the boot delay but it is not reflected while rebooting.&lt;/P&gt;&lt;P&gt;2. We are not able to add the new variables. When we execute "fw_setenv board_name evalkit" then we can see it using fw_printenv. But if we reboot and check the boot variables using the command "printenv" then the variable is not shown there.&lt;/P&gt;&lt;P&gt;3. We also tried adding the variable through&amp;nbsp;CONFIG_EXTRA_ENV_SETTINGS in mx6ul_14x14_evk.h&amp;nbsp; at&amp;nbsp;./tmp/work/../../include/configs/ but it is also not shown when we use fw_printenv.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 27 Dec 2018 12:04:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/u-boot-fw-utils-issue-with-mx6ul-14x14-evk/m-p/835987#M128341</guid>
      <dc:creator>hardikpadhariya</dc:creator>
      <dc:date>2018-12-27T12:04:13Z</dc:date>
    </item>
    <item>
      <title>Re: u-boot-fw-utils issue with mx6ul_14x14_evk</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/u-boot-fw-utils-issue-with-mx6ul-14x14-evk/m-p/835988#M128342</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Hardik&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;reason may be in wrong addresses as in similar question on&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="http://forum.variscite.com/viewtopic.php?t=416" title="http://forum.variscite.com/viewtopic.php?t=416"&gt;fw_printenv and fw_setenv [ANSWERED] - Variscite Forums&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;also as this is specific uboot issue it may be posted on uboot mail list&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://lists.denx.de/listinfo/u-boot" title="https://lists.denx.de/listinfo/u-boot"&gt;U-Boot Info Page&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 04 Jan 2019 07:56:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/u-boot-fw-utils-issue-with-mx6ul-14x14-evk/m-p/835988#M128342</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2019-01-04T07:56:52Z</dc:date>
    </item>
  </channel>
</rss>