<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic permanently adjust framebuffer image position in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/permanently-adjust-framebuffer-image-position/m-p/835703#M128324</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;for some reason, anything displayed on my lcd is shifted up by about 13 pixels. i tried setting vsync front porch in the device tree and that didn't help. the only thing that works is using the fbset command "fbset -upper 13" which shifts the screen down to the correct position.&amp;nbsp; How do I make this change permanent?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 25 Oct 2018 13:37:50 GMT</pubDate>
    <dc:creator>dluberger</dc:creator>
    <dc:date>2018-10-25T13:37:50Z</dc:date>
    <item>
      <title>permanently adjust framebuffer image position</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/permanently-adjust-framebuffer-image-position/m-p/835703#M128324</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;for some reason, anything displayed on my lcd is shifted up by about 13 pixels. i tried setting vsync front porch in the device tree and that didn't help. the only thing that works is using the fbset command "fbset -upper 13" which shifts the screen down to the correct position.&amp;nbsp; How do I make this change permanent?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 25 Oct 2018 13:37:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/permanently-adjust-framebuffer-image-position/m-p/835703#M128324</guid>
      <dc:creator>dluberger</dc:creator>
      <dc:date>2018-10-25T13:37:50Z</dc:date>
    </item>
    <item>
      <title>Re: permanently adjust framebuffer image position</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/permanently-adjust-framebuffer-image-position/m-p/835704#M128325</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Please try to play with upper margin option of the framebuffer.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day, &lt;BR /&gt;Victor &lt;BR /&gt; &lt;BR /&gt;----------------------------------------------------------------------------------------------------------------------- &lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you! &lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 26 Oct 2018 09:02:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/permanently-adjust-framebuffer-image-position/m-p/835704#M128325</guid>
      <dc:creator>b36401</dc:creator>
      <dc:date>2018-10-26T09:02:06Z</dc:date>
    </item>
    <item>
      <title>Re: permanently adjust framebuffer image position</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/permanently-adjust-framebuffer-image-position/m-p/835705#M128326</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;That's what I'm asking how to do.&amp;nbsp; As I said I can set temporarily the margin with fbset but how do i make the change permanent?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 26 Oct 2018 12:30:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/permanently-adjust-framebuffer-image-position/m-p/835705#M128326</guid>
      <dc:creator>dluberger</dc:creator>
      <dc:date>2018-10-26T12:30:24Z</dc:date>
    </item>
  </channel>
</rss>