<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Maximum Frequency of ACLK_EIM_SLOW_CLK_ROOT for i.MX6QP in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Maximum-Frequency-of-ACLK-EIM-SLOW-CLK-ROOT-for-i-MX6QP/m-p/835148#M128234</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The maximum ACLK_EIM_SLOW_CLK_ROOT frequency for the i.MX6QP processor is 132MHz.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Artur&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 26 Nov 2018 09:59:01 GMT</pubDate>
    <dc:creator>art</dc:creator>
    <dc:date>2018-11-26T09:59:01Z</dc:date>
    <item>
      <title>Maximum Frequency of ACLK_EIM_SLOW_CLK_ROOT for i.MX6QP</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Maximum-Frequency-of-ACLK-EIM-SLOW-CLK-ROOT-for-i-MX6QP/m-p/835147#M128233</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello community,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I received this question form my customer.&lt;/P&gt;&lt;P&gt;So I'm searching past thread of it.&lt;/P&gt;&lt;P&gt;But I can not find an answer for i.MX6QuadPlus.&lt;/P&gt;&lt;P&gt;And different 2 pattern comment for i.MX6DL and i.MX6Quad, I can found.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1) Maximum Frequency of ACLK_EIM_SLOW_CLK_ROOT = 104MHz&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/442559"&gt;Maximum Frequency of ACLK_EIM_SLOW_CLK_ROOT&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2) Maximum Frequency of ACLK_EIM_SLOW_CLK_ROOT= 133MHz for asynchronous mode.&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; 104MHz for synchronous mode.&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/359892"&gt;i.MX6DQ EIM clock for asynchronous access.&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; or in datasheet for i.MX6SDL&lt;/P&gt;&lt;P style="padding-left: 60px;"&gt;4.9.3 External Interface Module (EIM)&lt;BR /&gt;The following subsections provide information on the EIM. Maximum operating frequency for EIM data&lt;BR /&gt;transfer is 104 MHz. Two system clocks are used with the EIM:&lt;BR /&gt;• ACLK_EIM_SLOW_CLK_ROOT is used to clock the EIM module.&lt;BR /&gt;The maximum frequency for CLK_EIM_SLOW_CLK_ROOT is 132 MHz.&lt;BR /&gt;• ACLK_EXSC is also used when the EIM is in synchronous mode.&lt;BR /&gt;The maximum frequency for ACLK_EXSC is 104 MHz.&lt;BR /&gt;Timing parameters in this section that are given as a function of register settings.&lt;/P&gt;&lt;P style="padding-left: 60px;"&gt;&lt;/P&gt;&lt;P&gt;Q1. Which is a correct answer of maximum frequency of ACLK_EIM_SLOW_CLK_ROOT for i.MX6QP?&lt;/P&gt;&lt;P&gt;Q2. In "Table 8-4. Normal frequency clocks configuration" at section "8.4.3 Clocks at boot time" of&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; IMX6DQPRM rev 2 it say that ROM boot loader is set aclk_eim_slow_clk_root = 132MHz.&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; The other hand, u-boot for Linux BSP is setting ACLK_EIM_SLOW_CLK_ROOT=132MHz too.&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; Is it a timing violation setting for i.MX6DQ and i.MX6DQP? and not recommended to use it?&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp;I think it is OK for i.MX6SDL because it say that maximum frequency of ACLK_EIM_SLOW_CLK_ROOT=132MHz&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp;in their datasheet.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Ishii.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 14 Nov 2018 06:14:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Maximum-Frequency-of-ACLK-EIM-SLOW-CLK-ROOT-for-i-MX6QP/m-p/835147#M128233</guid>
      <dc:creator>takayuki_ishii</dc:creator>
      <dc:date>2018-11-14T06:14:01Z</dc:date>
    </item>
    <item>
      <title>Re: Maximum Frequency of ACLK_EIM_SLOW_CLK_ROOT for i.MX6QP</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Maximum-Frequency-of-ACLK-EIM-SLOW-CLK-ROOT-for-i-MX6QP/m-p/835148#M128234</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The maximum ACLK_EIM_SLOW_CLK_ROOT frequency for the i.MX6QP processor is 132MHz.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Artur&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 26 Nov 2018 09:59:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Maximum-Frequency-of-ACLK-EIM-SLOW-CLK-ROOT-for-i-MX6QP/m-p/835148#M128234</guid>
      <dc:creator>art</dc:creator>
      <dc:date>2018-11-26T09:59:01Z</dc:date>
    </item>
    <item>
      <title>Re: Maximum Frequency of ACLK_EIM_SLOW_CLK_ROOT for i.MX6QP</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Maximum-Frequency-of-ACLK-EIM-SLOW-CLK-ROOT-for-i-MX6QP/m-p/835149#M128235</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Artur,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for your response.&lt;/P&gt;&lt;P&gt;I will answer it to my customer.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope that the datasheet will be updated.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Ishii.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 27 Nov 2018 11:26:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Maximum-Frequency-of-ACLK-EIM-SLOW-CLK-ROOT-for-i-MX6QP/m-p/835149#M128235</guid>
      <dc:creator>takayuki_ishii</dc:creator>
      <dc:date>2018-11-27T11:26:46Z</dc:date>
    </item>
  </channel>
</rss>