<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: imx6 serial port rx problem</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/imx6-serial-port-rx-problem/m-p/835057#M128218</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi zhanxiaozhang,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Were you able to get the bottom of this problem? I'm seeing similar issues on my custom board based on IMX6 Solo. I was running a test with heavy CPU load (&amp;gt;85%), after about 1.5 hours, the IMX got too hot and crashed. After this, I can't get any sensible UART TX trace but the RX is fine. Even though I can't read it, I know the RX is working because I sent a boot command (on uboot) and the board was booting Linux.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I looked at the TX line using a scope and it looks like it is struggling to pull low. Any ideas?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 13 Mar 2020 14:01:35 GMT</pubDate>
    <dc:creator>danielberhe</dc:creator>
    <dc:date>2020-03-13T14:01:35Z</dc:date>
    <item>
      <title>imx6 serial port rx problem</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6-serial-port-rx-problem/m-p/835054#M128215</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We use imx6q ,android 4.4.3 kernel 3.10.53.&lt;/P&gt;&lt;P&gt;when high temperature working (under 80°c). After about 3 hours ,uart can not receive any data ,but tx works well.&lt;/P&gt;&lt;P&gt;we test 4 pcs at the same time ,1/4 meet this issue (the same one failed ).&lt;/P&gt;&lt;P&gt;Is there anybody meet the issue?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 08 Oct 2018 07:53:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6-serial-port-rx-problem/m-p/835054#M128215</guid>
      <dc:creator>zhanxiaozhang</dc:creator>
      <dc:date>2018-10-08T07:53:14Z</dc:date>
    </item>
    <item>
      <title>Re: imx6 serial port rx problem</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6-serial-port-rx-problem/m-p/835055#M128216</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi zhanxiaozhang&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;at high temperatures linux decrease processor clocks as described in&lt;/P&gt;&lt;P&gt;Chapter 26 Thermal Driver attached Linux Manual. Just for test one can try to&lt;/P&gt;&lt;P&gt;disable bus frequency driver using Chapter 25 Dynamic Bus Frequency Driver.&lt;/P&gt;&lt;P&gt;AN4579 i.MX 6 Series Thermal Management Guidelines describes thermal&lt;/P&gt;&lt;P&gt;management solutions:&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://www.nxp.com/docs/en/application-note/AN4579.pdf" title="https://www.nxp.com/docs/en/application-note/AN4579.pdf"&gt;https://www.nxp.com/docs/en/application-note/AN4579.pdf&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 09 Oct 2018 00:47:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6-serial-port-rx-problem/m-p/835055#M128216</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2018-10-09T00:47:52Z</dc:date>
    </item>
    <item>
      <title>Re: imx6 serial port rx problem</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6-serial-port-rx-problem/m-p/835056#M128217</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;you mean maybe the high temperature cause the hardware problem,not firmware releated?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 09 Oct 2018 00:57:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6-serial-port-rx-problem/m-p/835056#M128217</guid>
      <dc:creator>zhanxiaozhang</dc:creator>
      <dc:date>2018-10-09T00:57:21Z</dc:date>
    </item>
    <item>
      <title>Re: imx6 serial port rx problem</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6-serial-port-rx-problem/m-p/835057#M128218</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi zhanxiaozhang,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Were you able to get the bottom of this problem? I'm seeing similar issues on my custom board based on IMX6 Solo. I was running a test with heavy CPU load (&amp;gt;85%), after about 1.5 hours, the IMX got too hot and crashed. After this, I can't get any sensible UART TX trace but the RX is fine. Even though I can't read it, I know the RX is working because I sent a boot command (on uboot) and the board was booting Linux.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I looked at the TX line using a scope and it looks like it is struggling to pull low. Any ideas?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 13 Mar 2020 14:01:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6-serial-port-rx-problem/m-p/835057#M128218</guid>
      <dc:creator>danielberhe</dc:creator>
      <dc:date>2020-03-13T14:01:35Z</dc:date>
    </item>
  </channel>
</rss>