<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: adb reboot cannot reboot system. in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/adb-reboot-cannot-reboot-system/m-p/835002#M128212</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;please close the question.&lt;/P&gt;&lt;P&gt;we find that the WDT pin hardware is missed.&amp;nbsp; now the reset feature is ok.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 24 Jul 2018 10:05:32 GMT</pubDate>
    <dc:creator>kangjianwei</dc:creator>
    <dc:date>2018-07-24T10:05:32Z</dc:date>
    <item>
      <title>adb reboot cannot reboot system.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/adb-reboot-cannot-reboot-system/m-p/835000#M128210</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We change the PF3000 Power On mode from auto mode to pressing power key to power on mode.&amp;nbsp; we find that the command 'adb reboot' cannot to restart system. Before no change mode, the reboot is ok.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;the log as:&lt;/P&gt;&lt;P&gt;:/ # reboot&lt;BR /&gt;snvs_rtc_set_alarm set&lt;BR /&gt;sysrq: rtc_set_alarm done&lt;BR /&gt;sysrq: SysRq : Emergency Remount R/O&lt;BR /&gt;EXT4-fs (mmcblk2p4): re-mounted. Opts: (null)&lt;BR /&gt;EXT4-fs (mmcblk2p10): re-mounted. Opts: (null)&lt;BR /&gt;Emergency Remount complete&lt;BR /&gt;ci_hdrc ci_hdrc.1: remove, state 4&lt;BR /&gt;usb usb1: USB disconnect, device number 1&lt;BR /&gt;ci_hdrc ci_hdrc.1: USB bus 1 deregistered&lt;BR /&gt;android_work: sent uevent USB_STATE=DISCONNECTED&lt;BR /&gt;reboot: Restarting system with command ''&lt;BR /&gt;Unable to restart system&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Now the power on mode is ok, we can press button to power on, and set "PWRONRSTEN = 1", press Button key &amp;gt; 4S, the system can power off.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;why we change the power mode cause the reboot issue?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 20 Jul 2018 06:16:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/adb-reboot-cannot-reboot-system/m-p/835000#M128210</guid>
      <dc:creator>kangjianwei</dc:creator>
      <dc:date>2018-07-20T06:16:31Z</dc:date>
    </item>
    <item>
      <title>Re: adb reboot cannot reboot system.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/adb-reboot-cannot-reboot-system/m-p/835001#M128211</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;which board are you using?&lt;/P&gt;&lt;P&gt;which bsp are you using?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 24 Jul 2018 09:45:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/adb-reboot-cannot-reboot-system/m-p/835001#M128211</guid>
      <dc:creator>jimmychan</dc:creator>
      <dc:date>2018-07-24T09:45:59Z</dc:date>
    </item>
    <item>
      <title>Re: adb reboot cannot reboot system.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/adb-reboot-cannot-reboot-system/m-p/835002#M128212</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;please close the question.&lt;/P&gt;&lt;P&gt;we find that the WDT pin hardware is missed.&amp;nbsp; now the reset feature is ok.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 24 Jul 2018 10:05:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/adb-reboot-cannot-reboot-system/m-p/835002#M128212</guid>
      <dc:creator>kangjianwei</dc:creator>
      <dc:date>2018-07-24T10:05:32Z</dc:date>
    </item>
  </channel>
</rss>