<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックCommunicating over Statically assignend IP.</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Communicating-over-Statically-assignend-IP/m-p/151731#M1282</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I would like to know, how one can communicate using statical ip settings between host PC and iMX25 boad.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Following is the requirement:&lt;/P&gt;&lt;P&gt;To pick the ipaddress&amp;nbsp;from a particular&amp;nbsp;file and start comminucating ovet the assigned ipAddress.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;To meat the above feature, when I restarted the network it had poped the following message:&lt;/P&gt;&lt;P&gt;&lt;A href="mailto:root@fressScale~$"&gt;root@fressScale~$&lt;/A&gt; /etc/rc.d/init.d/network restart&lt;/P&gt;&lt;P&gt;follwoing message is given:&lt;/P&gt;&lt;P&gt;Runing sysctl&lt;/P&gt;&lt;P&gt;setting up network on loopback device:&lt;/P&gt;&lt;P&gt;route: SIOCADDRT file exists.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Warning: no IPAddr is set, please set this from ltib config screen, or directly in /etc/rc.d/rc.conf.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have made corresponing changes while configure ltib with dhcp off also making changes in rtc.conf.Upon boot the ipaddress changes successfuly.But, whiel&amp;nbsp;bring-up the network the&amp;nbsp;board&amp;nbsp;it is noticed that HWare ADDREss in 00.00.0.00.00&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If any one has any information about how to&amp;nbsp;bring the network up&amp;nbsp;using NAND boot imx25 please provide the info.&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Folwing is the o/p&lt;/P&gt;&lt;P&gt;root@macd ~$ /etc/rc.d/init.d/network start &lt;BR /&gt;Running sysctl&lt;BR /&gt;Setting up networking on loopback device: &lt;BR /&gt;route: SIOCADDRT: File exists&lt;/P&gt;&lt;P&gt;Warning: no IPADDR is set, please set this from the ltib&lt;BR /&gt;config screen, or directly in /etc/rc.d/rc.conf.&lt;BR /&gt;IP address setup bypassed&lt;/P&gt;&lt;P&gt;sbin/ifconfig -a&lt;BR /&gt;can0 Link encap:UNSPEC HWaddr 00-00-00-00-00-00-00-00-00-00-00-00-00-00-00-00 &lt;BR /&gt;NOARP MTU:16 Metric:1&lt;BR /&gt;RX packets:0 errors:0 dropped:0 overruns:0 frame:0&lt;BR /&gt;TX packets:0 errors:0 dropped:0 overruns:0 carrier:0&lt;BR /&gt;collisions:0 txqueuelen:64 &lt;BR /&gt;RX bytes:0 (0.0 B) TX bytes:0 (0.0 B)&lt;/P&gt;&lt;P&gt;eth0 Link encap:Ethernet HWaddr 00:00:00:00:00:00 &lt;BR /&gt;inet addr:192.168.1.20 Bcast:192.168.1.255 Mask:255.255.255.0&lt;BR /&gt;BROADCAST MULTICAST MTU:1500 Metric:1&lt;BR /&gt;RX packets:0 errors:0 dropped:0 overruns:0 frame:0&lt;BR /&gt;TX packets:0 errors:0 dropped:0 overruns:0 carrier:0&lt;BR /&gt;collisions:0 txqueuelen:1000 &lt;BR /&gt;RX bytes:0 (0.0 B) TX bytes:0 (0.0 B)&lt;BR /&gt;Base address:0xe000&lt;/P&gt;&lt;P&gt;lo Link encap:Local Loopback &lt;BR /&gt;inet addr:127.0.0.1 Mask:255.0.0.0&lt;BR /&gt;UP LOOPBACK RUNNING MTU:16436 Metric:1&lt;BR /&gt;RX packets:0 errors:0 dropped:0 overruns:0 frame:0&lt;BR /&gt;TX packets:0 errors:0 dropped:0 overruns:0 carrier:0&lt;BR /&gt;collisions:0 txqueuelen:0 &lt;BR /&gt;RX bytes:0 (0.0 B) TX bytes:0 (0.0 B)&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 09 Apr 2012 10:23:55 GMT</pubDate>
    <dc:creator>jai_appari</dc:creator>
    <dc:date>2012-04-09T10:23:55Z</dc:date>
    <item>
      <title>Communicating over Statically assignend IP.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Communicating-over-Statically-assignend-IP/m-p/151731#M1282</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I would like to know, how one can communicate using statical ip settings between host PC and iMX25 boad.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Following is the requirement:&lt;/P&gt;&lt;P&gt;To pick the ipaddress&amp;nbsp;from a particular&amp;nbsp;file and start comminucating ovet the assigned ipAddress.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;To meat the above feature, when I restarted the network it had poped the following message:&lt;/P&gt;&lt;P&gt;&lt;A href="mailto:root@fressScale~$"&gt;root@fressScale~$&lt;/A&gt; /etc/rc.d/init.d/network restart&lt;/P&gt;&lt;P&gt;follwoing message is given:&lt;/P&gt;&lt;P&gt;Runing sysctl&lt;/P&gt;&lt;P&gt;setting up network on loopback device:&lt;/P&gt;&lt;P&gt;route: SIOCADDRT file exists.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Warning: no IPAddr is set, please set this from ltib config screen, or directly in /etc/rc.d/rc.conf.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have made corresponing changes while configure ltib with dhcp off also making changes in rtc.conf.Upon boot the ipaddress changes successfuly.But, whiel&amp;nbsp;bring-up the network the&amp;nbsp;board&amp;nbsp;it is noticed that HWare ADDREss in 00.00.0.00.00&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If any one has any information about how to&amp;nbsp;bring the network up&amp;nbsp;using NAND boot imx25 please provide the info.&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Folwing is the o/p&lt;/P&gt;&lt;P&gt;root@macd ~$ /etc/rc.d/init.d/network start &lt;BR /&gt;Running sysctl&lt;BR /&gt;Setting up networking on loopback device: &lt;BR /&gt;route: SIOCADDRT: File exists&lt;/P&gt;&lt;P&gt;Warning: no IPADDR is set, please set this from the ltib&lt;BR /&gt;config screen, or directly in /etc/rc.d/rc.conf.&lt;BR /&gt;IP address setup bypassed&lt;/P&gt;&lt;P&gt;sbin/ifconfig -a&lt;BR /&gt;can0 Link encap:UNSPEC HWaddr 00-00-00-00-00-00-00-00-00-00-00-00-00-00-00-00 &lt;BR /&gt;NOARP MTU:16 Metric:1&lt;BR /&gt;RX packets:0 errors:0 dropped:0 overruns:0 frame:0&lt;BR /&gt;TX packets:0 errors:0 dropped:0 overruns:0 carrier:0&lt;BR /&gt;collisions:0 txqueuelen:64 &lt;BR /&gt;RX bytes:0 (0.0 B) TX bytes:0 (0.0 B)&lt;/P&gt;&lt;P&gt;eth0 Link encap:Ethernet HWaddr 00:00:00:00:00:00 &lt;BR /&gt;inet addr:192.168.1.20 Bcast:192.168.1.255 Mask:255.255.255.0&lt;BR /&gt;BROADCAST MULTICAST MTU:1500 Metric:1&lt;BR /&gt;RX packets:0 errors:0 dropped:0 overruns:0 frame:0&lt;BR /&gt;TX packets:0 errors:0 dropped:0 overruns:0 carrier:0&lt;BR /&gt;collisions:0 txqueuelen:1000 &lt;BR /&gt;RX bytes:0 (0.0 B) TX bytes:0 (0.0 B)&lt;BR /&gt;Base address:0xe000&lt;/P&gt;&lt;P&gt;lo Link encap:Local Loopback &lt;BR /&gt;inet addr:127.0.0.1 Mask:255.0.0.0&lt;BR /&gt;UP LOOPBACK RUNNING MTU:16436 Metric:1&lt;BR /&gt;RX packets:0 errors:0 dropped:0 overruns:0 frame:0&lt;BR /&gt;TX packets:0 errors:0 dropped:0 overruns:0 carrier:0&lt;BR /&gt;collisions:0 txqueuelen:0 &lt;BR /&gt;RX bytes:0 (0.0 B) TX bytes:0 (0.0 B)&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 09 Apr 2012 10:23:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Communicating-over-Statically-assignend-IP/m-p/151731#M1282</guid>
      <dc:creator>jai_appari</dc:creator>
      <dc:date>2012-04-09T10:23:55Z</dc:date>
    </item>
  </channel>
</rss>