<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: Write kernel to nand via imx-usb-loader</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Write-kernel-to-nand-via-imx-usb-loader/m-p/834487#M128144</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Igor and thanks for reply. And what with boot with wifi ? because I have single module without ethernet and USB interface on board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Adrian&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 15 Nov 2018 08:34:39 GMT</pubDate>
    <dc:creator>adi1525</dc:creator>
    <dc:date>2018-11-15T08:34:39Z</dc:date>
    <item>
      <title>Write kernel to nand via imx-usb-loader</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Write-kernel-to-nand-via-imx-usb-loader/m-p/834485#M128142</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&lt;/P&gt;&lt;P&gt;I use Yocto and I&amp;nbsp;writed u-boot to I.mx6ul witch use imx_usb_loader by USB debug mode, but I can't find information how write kernel and rootfs, is it posible ? or if I can write it with mfgtools ??&lt;/P&gt;&lt;P&gt;I don't have access to ethernet and USB/SD CARD.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;By the way, is there option in uboot to program kernel or rootfs via WIFI ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Adrian&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 14 Nov 2018 16:13:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Write-kernel-to-nand-via-imx-usb-loader/m-p/834485#M128142</guid>
      <dc:creator>adi1525</dc:creator>
      <dc:date>2018-11-14T16:13:14Z</dc:date>
    </item>
    <item>
      <title>Re: Write kernel to nand via imx-usb-loader</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Write-kernel-to-nand-via-imx-usb-loader/m-p/834486#M128143</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Adrian&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;nxp does not support usb-loader, it was developed by third party, one can check&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-94117"&gt;i.MX USB Loader&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/441563"&gt;Guide to flash iMX6 from Linux&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 14 Nov 2018 22:55:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Write-kernel-to-nand-via-imx-usb-loader/m-p/834486#M128143</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2018-11-14T22:55:02Z</dc:date>
    </item>
    <item>
      <title>Re: Write kernel to nand via imx-usb-loader</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Write-kernel-to-nand-via-imx-usb-loader/m-p/834487#M128144</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Igor and thanks for reply. And what with boot with wifi ? because I have single module without ethernet and USB interface on board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Adrian&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 15 Nov 2018 08:34:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Write-kernel-to-nand-via-imx-usb-loader/m-p/834487#M128144</guid>
      <dc:creator>adi1525</dc:creator>
      <dc:date>2018-11-15T08:34:39Z</dc:date>
    </item>
  </channel>
</rss>