<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: MMC Timeout Crash dump during Data Transfer</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/MMC-Timeout-Crash-dump-during-Data-Transfer/m-p/834358#M128122</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Pandi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;errors may be also caused from external card, one can try with other card.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 24 Jul 2018 08:23:37 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2018-07-24T08:23:37Z</dc:date>
    <item>
      <title>MMC Timeout Crash dump during Data Transfer</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MMC-Timeout-Crash-dump-during-Data-Transfer/m-p/834355#M128119</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am working with the IMX6SLL-EVK board and&amp;nbsp;booting up with the linux-imx-4.9.11_1.0.0_ga kernel.&lt;/P&gt;&lt;P&gt;An external WiFi card is inserted interfaced using the SD3(MMC2) slot and data transfer is tested. The WiFi Card is detected as a UHS-I SDR104 card and the supplied clock frequency is 198MHz.&lt;/P&gt;&lt;P&gt;During Iperf test data transfers the MMC Timeout crash is observed more often. This is caused by the timer callback "sdhci_timeout_data_timer". After this the WIFI card has to be removed and re-inserted to continue further testing.&lt;/P&gt;&lt;P&gt;What is the reason for this dump?&lt;/P&gt;&lt;P&gt;Is it a limitation of the iMX6SLL-EVK platform because of the single core design?&lt;/P&gt;&lt;P&gt;help me debug this further.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;ubuntu@arm:~$ sudo cat /sys/kernel/debug/mmc2/ios&lt;BR /&gt;clock: 208000000 Hz&lt;BR /&gt;actual clock: 198000000 Hz&lt;BR /&gt;vdd: 18 (3.0 ~ 3.1 V)&lt;BR /&gt;bus mode: 2 (push-pull)&lt;BR /&gt;chip select: 0 (don't care)&lt;BR /&gt;power mode: 2 (on)&lt;BR /&gt;bus width: 2 (4 bits)&lt;BR /&gt;timing spec: 6 (sd uhs SDR104)&lt;BR /&gt;signal voltage: 1 (1.80 V)&lt;BR /&gt;driver type: 0 (driver type B)&lt;BR /&gt;&lt;A href="mailto:ubuntu@arm:~$"&gt;ubuntu@arm:~$&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;ubuntu@arm:~$ mmc2: Timeout waiting for hardware interrupt.&lt;BR /&gt;sdhci: =========== REGISTER DUMP (mmc2)===========&lt;BR /&gt;sdhci: Sys addr: 0xe4059d90 | Version: 0x00000002&lt;BR /&gt;sdhci: Blk size: 0x00000004 | Blk cnt: 0x00000001&lt;BR /&gt;sdhci: Argument: 0x9410d004 | Trn mode: 0x00000003&lt;BR /&gt;sdhci: Present: 0x01f8810e | Host ctl: 0x00000013&lt;BR /&gt;sdhci: Power: 0x00000002 | Blk gap: 0x00000080&lt;BR /&gt;sdhci: Wake-up: 0x00000008 | Clock: 0x0000001f&lt;BR /&gt;sdhci: Timeout: 0x0000008f | Int stat: 0x00000000&lt;BR /&gt;sdhci: Int enab: 0x107f110b | Sig enab: 0x107f110b&lt;BR /&gt;sdhci: AC12 err: 0x00000000 | Slot int: 0x00000302&lt;BR /&gt;sdhci: Caps: 0x07eb0000 | Caps_1: 0x8000b407&lt;BR /&gt;sdhci: Cmd: 0x0000353a | Max curr: 0x00ffffff&lt;BR /&gt;sdhci: Host ctl2: 0x00000088&lt;BR /&gt;sdhci: ADMA Err: 0x00000000 | ADMA Ptr: 0xec4d1208&lt;BR /&gt;sdhci: ===========================================&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Pandi Vijayaraj&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 20 Jul 2018 09:37:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MMC-Timeout-Crash-dump-during-Data-Transfer/m-p/834355#M128119</guid>
      <dc:creator>pandivijayaraj</dc:creator>
      <dc:date>2018-07-20T09:37:43Z</dc:date>
    </item>
    <item>
      <title>Re: MMC Timeout Crash dump during Data Transfer</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MMC-Timeout-Crash-dump-during-Data-Transfer/m-p/834356#M128120</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Pandi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can try to adjust pad settings related to signal integrity, like DSE,SRE,SPEED&lt;/P&gt;&lt;P&gt;described in sect.&lt;CODE&gt;25.7.312 Pad Control Register (IOMUXC_SW_PAD_CTL_PAD_SD3_DATA0)&lt;/CODE&gt;&lt;/P&gt;&lt;P&gt;i.MX6SLL Reference Manual (rev.0&amp;nbsp; 6/2017)&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/www.nxp.com/assets/documents/data/en/reference-manuals/IMX6SLLRM.pdf" rel="nofollow noopener noreferrer noopener noreferrer" target="test_blank"&gt;www.nxp.com/assets/documents/data/en/reference-manuals/IMX6SLLRM.pdf&lt;/A&gt;&lt;/P&gt;&lt;PRE&gt;&lt;CODE&gt;
&lt;/CODE&gt;&lt;CODE&gt;&amp;amp;iomuxc { &amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;imx6sll-evk-murata-v2 { &amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;pinctrl_wifi: wifigrp { &amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;fsl,pins = &amp;lt; &lt;/CODE&gt;MX6SLL_PAD_SD3_DATA0__SD3_DATA0 0x170b9 ..
&lt;CODE&gt;&lt;A class="link-titled" href="http://git.freescale.com/git/cgit.cgi/imx/linux-imx.git/tree/arch/arm/boot/dts/imx6sll-evk-btwifi.dts?h=imx_4.9.11_1.0.0_ga" rel="nofollow noopener noreferrer noopener noreferrer" target="_blank" title="http://git.freescale.com/git/cgit.cgi/imx/linux-imx.git/tree/arch/arm/boot/dts/imx6sll-evk-btwifi.dts?h=imx_4.9.11_1.0.0_ga"&gt;linux-imx.git - i.MX Linux Kernel&lt;/A&gt;&amp;nbsp;

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------&lt;/CODE&gt;&lt;/PRE&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 02 Nov 2020 14:14:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MMC-Timeout-Crash-dump-during-Data-Transfer/m-p/834356#M128120</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2020-11-02T14:14:05Z</dc:date>
    </item>
    <item>
      <title>Re: MMC Timeout Crash dump during Data Transfer</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MMC-Timeout-Crash-dump-during-Data-Transfer/m-p/834357#M128121</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Igor,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have already tried to modify the parameters in IOMUX PAD registers.&lt;/P&gt;&lt;P&gt;The MMC clock speed used here is 200Mhz.&lt;/P&gt;&lt;P&gt;SPEED bits should be always set to 11.&lt;/P&gt;&lt;P&gt;SRE is always set to 1, to select the Fast slew rate.&lt;/P&gt;&lt;P&gt;So , the variability is there only in DSE field. I have tested with all the values for the DSE field.&lt;/P&gt;&lt;P&gt;But still the probelm exists.&lt;/P&gt;&lt;P&gt;If we use the value&amp;nbsp; DSE&amp;nbsp; = 111(37 ohm) for the IO pins SD3_DATA0-3, then the scenario improves little bit. But still crash occurs sometimes.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 23 Jul 2018 08:01:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MMC-Timeout-Crash-dump-during-Data-Transfer/m-p/834357#M128121</guid>
      <dc:creator>pandivijayaraj</dc:creator>
      <dc:date>2018-07-23T08:01:27Z</dc:date>
    </item>
    <item>
      <title>Re: MMC Timeout Crash dump during Data Transfer</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MMC-Timeout-Crash-dump-during-Data-Transfer/m-p/834358#M128122</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Pandi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;errors may be also caused from external card, one can try with other card.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 24 Jul 2018 08:23:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MMC-Timeout-Crash-dump-during-Data-Transfer/m-p/834358#M128122</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2018-07-24T08:23:37Z</dc:date>
    </item>
    <item>
      <title>Re: MMC Timeout Crash dump during Data Transfer</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MMC-Timeout-Crash-dump-during-Data-Transfer/m-p/834359#M128123</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Igor,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have tried with multiple cards. Still problem is observed.&lt;/P&gt;&lt;P&gt;whenever this problem occurs driver receives the particular error code -84 EILSEQ from the MMC stack during the read operation from SDIO.&lt;/P&gt;&lt;P&gt;After that the other timeout Error code -110 is returned continuously for all the further writes and at one point, the MMC timeout occurs.&lt;/P&gt;&lt;P&gt;What could be the reason for EILSEQ error during SDIO read?&amp;nbsp;&lt;/P&gt;&lt;P&gt;Whether it could be related to the SDIO clock frequency 200MHz in UHS-I mode?&lt;/P&gt;&lt;P&gt;Could it be because of&amp;nbsp;SDIO port power supply? Anything like fluctuations?&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Pandi Vijayaraj&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 27 Jul 2018 11:30:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MMC-Timeout-Crash-dump-during-Data-Transfer/m-p/834359#M128123</guid>
      <dc:creator>pandivijayaraj</dc:creator>
      <dc:date>2018-07-27T11:30:52Z</dc:date>
    </item>
    <item>
      <title>Re: MMC Timeout Crash dump during Data Transfer</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MMC-Timeout-Crash-dump-during-Data-Transfer/m-p/834360#M128124</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV class=""&gt;&lt;P&gt;Hi Pandi&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;right, power supply may affect it. One can try with external power supply.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 27 Jul 2018 11:59:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MMC-Timeout-Crash-dump-during-Data-Transfer/m-p/834360#M128124</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2018-07-27T11:59:57Z</dc:date>
    </item>
  </channel>
</rss>