<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Untitled in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Untitled/m-p/151720#M1279</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;I'm trying to rebuild updater.sb for mfgtools, using create_updater.sh, which is in rootfs/boot. When i run create_updater.sh i get the message below. When i check the script ans errors what i understand  1) I should give two parameters while running script 2) The script couldn't find the path of elftosb  so how should i run this script?  ---------------------------------------------------------------------------------------  ./create_updater.sh cp: missing destination file operand after `/boot/updater*.bd' Try `cp --help' for more information. sed: can't read updater.bd: No such file or directory sed: can't read updater.bd: No such file or directory sed: can't read updater.bd: No such file or directory sed: can't read updater.bd: No such file or directory sed: can't read updater_ivt.bd: No such file or directory sed: can't read updater_ivt.bd: No such file or directory sed: can't read updater_ivt.bd: No such file or directory sed: can't read updater_ivt.bd: No such file or directory ./create_updater.sh: line 13: elftosb: command not found ./create_updater.sh: line 14: elftosb: command not found&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 08 Apr 2011 07:43:06 GMT</pubDate>
    <dc:creator>AhmetYUCE</dc:creator>
    <dc:date>2011-04-08T07:43:06Z</dc:date>
    <item>
      <title>Untitled</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Untitled/m-p/151720#M1279</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;I'm trying to rebuild updater.sb for mfgtools, using create_updater.sh, which is in rootfs/boot. When i run create_updater.sh i get the message below. When i check the script ans errors what i understand  1) I should give two parameters while running script 2) The script couldn't find the path of elftosb  so how should i run this script?  ---------------------------------------------------------------------------------------  ./create_updater.sh cp: missing destination file operand after `/boot/updater*.bd' Try `cp --help' for more information. sed: can't read updater.bd: No such file or directory sed: can't read updater.bd: No such file or directory sed: can't read updater.bd: No such file or directory sed: can't read updater.bd: No such file or directory sed: can't read updater_ivt.bd: No such file or directory sed: can't read updater_ivt.bd: No such file or directory sed: can't read updater_ivt.bd: No such file or directory sed: can't read updater_ivt.bd: No such file or directory ./create_updater.sh: line 13: elftosb: command not found ./create_updater.sh: line 14: elftosb: command not found&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 08 Apr 2011 07:43:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Untitled/m-p/151720#M1279</guid>
      <dc:creator>AhmetYUCE</dc:creator>
      <dc:date>2011-04-08T07:43:06Z</dc:date>
    </item>
    <item>
      <title>Re: Untitled</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Untitled/m-p/151721#M1280</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi guys,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am trying to create the updater_ivt.sb used by Mfgtools for my board as well but failed to do so.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have followed the steps shown below but still not able to create the updater_ivt.sb file&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2.5 Building the Manufacturing Firmware (To Be Supported)&lt;BR /&gt;Refer to Section 2.2 Installing and Building LTIB, to setup the ltib environment.&lt;BR /&gt;&lt;BR /&gt;Configure the firmware build profile&lt;BR /&gt;&lt;BR /&gt;$ ./ltib --selectype&lt;BR /&gt;&lt;BR /&gt;Choose the following:&lt;BR /&gt;&lt;BR /&gt;--- Choose the platform type&lt;BR /&gt;Selection (imx28) ---&amp;gt;&lt;BR /&gt;&lt;BR /&gt;--- Choose the packages profile&lt;BR /&gt;Selection (mfg firmware profile) ---&amp;gt;&lt;BR /&gt;&lt;BR /&gt;Save and exit.&lt;BR /&gt;&lt;BR /&gt;After ltib completes the build, Updater.sb and updater_ivt.sb will have been created.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you are able to create it, please help by providing any hints or guidance.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Eric&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 25 Apr 2012 03:35:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Untitled/m-p/151721#M1280</guid>
      <dc:creator>EricFung</dc:creator>
      <dc:date>2012-04-25T03:35:30Z</dc:date>
    </item>
    <item>
      <title>Re: Untitled</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Untitled/m-p/151722#M1281</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have already fixed the problem.&lt;/P&gt;&lt;P&gt;I mixed up with the location of the file updater_ivt.sb which was originally I thought placed in ./litb/rootfs/boot. In fact it is stored in the same location as ./ltib.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Eric&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 25 Apr 2012 06:51:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Untitled/m-p/151722#M1281</guid>
      <dc:creator>EricFung</dc:creator>
      <dc:date>2012-04-25T06:51:44Z</dc:date>
    </item>
  </channel>
</rss>