<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic iMX25 WinCE 6 source code. in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/iMX25-WinCE-6-source-code/m-p/211321#M12787</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;I just have a question regarding whether there is updated source code for the iMX25 BSP after the Dec '09 release. I have notice that in the &lt;SPAN class="sortDesc sortModiifed" id="Sortingcol_1" style="cursor: pointer;"&gt;&lt;A href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=WEIMX&amp;amp;fpsp=1&amp;amp;tab=Design_Tools_Tab#"&gt;WCE600_11.04.02_ER_SOURCE&lt;/A&gt;&lt;/SPAN&gt; (dated 02/02/12) there is support for the iMX25 in the source tree but there is no indication that the platform has actually been tested with it. When I browse to the iMX25 tree on the website the only BSP that is listed for the iMX25 is &lt;A href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=WEIMX&amp;amp;fpsp=1&amp;amp;tab=Design_Tools_Tab#"&gt;WCE600_09.12.00_SDK&lt;/A&gt;.&lt;/P&gt;&lt;P&gt;Has anyone else used the later source and can verify that it functions correctly with the iMX25 PDK??&lt;/P&gt;&lt;P&gt;Cheers,&lt;/P&gt;&lt;P&gt;Andre&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Feb 2012 03:09:47 GMT</pubDate>
    <dc:creator>andrew_questps</dc:creator>
    <dc:date>2012-02-15T03:09:47Z</dc:date>
    <item>
      <title>iMX25 WinCE 6 source code.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX25-WinCE-6-source-code/m-p/211321#M12787</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;I just have a question regarding whether there is updated source code for the iMX25 BSP after the Dec '09 release. I have notice that in the &lt;SPAN class="sortDesc sortModiifed" id="Sortingcol_1" style="cursor: pointer;"&gt;&lt;A href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=WEIMX&amp;amp;fpsp=1&amp;amp;tab=Design_Tools_Tab#"&gt;WCE600_11.04.02_ER_SOURCE&lt;/A&gt;&lt;/SPAN&gt; (dated 02/02/12) there is support for the iMX25 in the source tree but there is no indication that the platform has actually been tested with it. When I browse to the iMX25 tree on the website the only BSP that is listed for the iMX25 is &lt;A href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=WEIMX&amp;amp;fpsp=1&amp;amp;tab=Design_Tools_Tab#"&gt;WCE600_09.12.00_SDK&lt;/A&gt;.&lt;/P&gt;&lt;P&gt;Has anyone else used the later source and can verify that it functions correctly with the iMX25 PDK??&lt;/P&gt;&lt;P&gt;Cheers,&lt;/P&gt;&lt;P&gt;Andre&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Feb 2012 03:09:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX25-WinCE-6-source-code/m-p/211321#M12787</guid>
      <dc:creator>andrew_questps</dc:creator>
      <dc:date>2012-02-15T03:09:47Z</dc:date>
    </item>
  </channel>
</rss>