<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic FTM in Output compare mode in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/FTM-in-Output-compare-mode/m-p/832489#M127865</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;[ Environment : Win CE 7 OS on Toradex Colibri iMX7D 512MB board ]&lt;/P&gt;&lt;P&gt;I am using FTM module in output compare mode. I have developed the driver and it is partially working too. But I am not getting the desired result. I have configured FTM in output compare mode with output toggle on channel match. Channel flag sets on channel match however nothing observed on channel output. I am attaching the source code for reference.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Secondly, I want to use an ISR when an event occurs at channel match in(FTM in output compare mode). FTMx_CnSC has a CHIE bit to enable the interrupt so we can enable the interrupt. But how one can trigger a function using this interrupt ? Please guide me, How to write ISR for the channel match interrupt?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Bipin Kumar&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 04 Dec 2018 06:45:20 GMT</pubDate>
    <dc:creator>bipin7301</dc:creator>
    <dc:date>2018-12-04T06:45:20Z</dc:date>
    <item>
      <title>FTM in Output compare mode</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/FTM-in-Output-compare-mode/m-p/832489#M127865</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;[ Environment : Win CE 7 OS on Toradex Colibri iMX7D 512MB board ]&lt;/P&gt;&lt;P&gt;I am using FTM module in output compare mode. I have developed the driver and it is partially working too. But I am not getting the desired result. I have configured FTM in output compare mode with output toggle on channel match. Channel flag sets on channel match however nothing observed on channel output. I am attaching the source code for reference.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Secondly, I want to use an ISR when an event occurs at channel match in(FTM in output compare mode). FTMx_CnSC has a CHIE bit to enable the interrupt so we can enable the interrupt. But how one can trigger a function using this interrupt ? Please guide me, How to write ISR for the channel match interrupt?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Bipin Kumar&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 04 Dec 2018 06:45:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/FTM-in-Output-compare-mode/m-p/832489#M127865</guid>
      <dc:creator>bipin7301</dc:creator>
      <dc:date>2018-12-04T06:45:20Z</dc:date>
    </item>
  </channel>
</rss>