<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Which ECC i.MX6 ROM code uses?</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Re-Which-ECC-i-MX6-ROM-code-uses/m-p/832110#M127808</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The algorithm Yuri attached is one used on i.MX6 processors. &lt;BR /&gt;And the same BCH ECC is used on i.MX7 and i.MX8M processors as well.&lt;BR /&gt;Please make sure that you set right parameters for encoding algorithm.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Victor&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 29 Jun 2018 07:44:10 GMT</pubDate>
    <dc:creator>b36401</dc:creator>
    <dc:date>2018-06-29T07:44:10Z</dc:date>
    <item>
      <title>Re: Which ECC i.MX6 ROM code uses?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Re-Which-ECC-i-MX6-ROM-code-uses/m-p/832109#M127807</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/YuriMuhin_ng"&gt;YuriMuhin_ng&lt;/A&gt;‌ I used your attached BCH_enco.c and found that it generates incorrect code for some data blocks.&lt;BR /&gt;is there any updated version of this file is available?&lt;BR /&gt;This file generated incorrect/different ECC for program_image as compare to ECC generated by kobs-ng utility for NAND.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 28 Jun 2018 12:01:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Re-Which-ECC-i-MX6-ROM-code-uses/m-p/832109#M127807</guid>
      <dc:creator>abdulrasheed</dc:creator>
      <dc:date>2018-06-28T12:01:59Z</dc:date>
    </item>
    <item>
      <title>Re: Which ECC i.MX6 ROM code uses?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Re-Which-ECC-i-MX6-ROM-code-uses/m-p/832110#M127808</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The algorithm Yuri attached is one used on i.MX6 processors. &lt;BR /&gt;And the same BCH ECC is used on i.MX7 and i.MX8M processors as well.&lt;BR /&gt;Please make sure that you set right parameters for encoding algorithm.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Victor&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 29 Jun 2018 07:44:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Re-Which-ECC-i-MX6-ROM-code-uses/m-p/832110#M127808</guid>
      <dc:creator>b36401</dc:creator>
      <dc:date>2018-06-29T07:44:10Z</dc:date>
    </item>
    <item>
      <title>Re: Which ECC i.MX6 ROM code uses?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Re-Which-ECC-i-MX6-ROM-code-uses/m-p/832111#M127809</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Additionally to doublecheck if it is right algorithm please create a technical case:&lt;BR /&gt;&lt;A class="jive-link-thread-small" data-containerid="11688" data-containertype="14" data-objectid="381898" data-objecttype="1" href="https://community.nxp.com/thread/381898"&gt;https://community.nxp.com/thread/381898&lt;/A&gt;&lt;BR /&gt;I will attach the file.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 29 Jun 2018 07:51:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Re-Which-ECC-i-MX6-ROM-code-uses/m-p/832111#M127809</guid>
      <dc:creator>b36401</dc:creator>
      <dc:date>2018-06-29T07:51:04Z</dc:date>
    </item>
  </channel>
</rss>