<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: IMX 6 LCD controller,  SSD1322, 8080mode in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX-6-LCD-controller-SSD1322-8080mode/m-p/831997#M127785</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi igor,&amp;nbsp;&lt;/P&gt;&lt;P&gt;thanks for your support.&lt;/P&gt;&lt;P&gt;However ,&amp;nbsp; the reference manual doesnot describes clearly how to configure LCD controller into 8080mode to communicate with oled mode.&amp;nbsp;&lt;/P&gt;&lt;P&gt;could you give me some sample code ?&amp;nbsp; how to configure the display clock ? should we use the 'run' bit in CTRL register ? rather confused&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 06 Dec 2018 22:57:55 GMT</pubDate>
    <dc:creator>alvenwu</dc:creator>
    <dc:date>2018-12-06T22:57:55Z</dc:date>
    <item>
      <title>IMX 6 LCD controller,  SSD1322, 8080mode</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX-6-LCD-controller-SSD1322-8080mode/m-p/831993#M127781</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;HI&amp;nbsp; I am using arm cortex A7&amp;nbsp; chip , which can be running in 8080 mode to connect to the SSD 1322 oled&amp;nbsp; controller.&amp;nbsp;&lt;/P&gt;&lt;P&gt;1.However , I am confusing about the hardware connection with the SSD1322 controller.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Do we need to use GPIO to control the CS , RS , WR ,RD signals ? &amp;nbsp; or just configure the LCD controller to transfer data in 8080 mode ?&amp;nbsp;&lt;/P&gt;&lt;P&gt;2. and I saw a "run" bit in CTRL register , does it mean every time data transfer , we should set it to '1'&amp;nbsp; to start the transfer ?&lt;/P&gt;&lt;P&gt;3. how to configure the display time cycle?&amp;nbsp; just enable the clock ? &amp;nbsp;&lt;/P&gt;&lt;P&gt;thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 04 Dec 2018 09:00:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX-6-LCD-controller-SSD1322-8080mode/m-p/831993#M127781</guid>
      <dc:creator>alvenwu</dc:creator>
      <dc:date>2018-12-04T09:00:40Z</dc:date>
    </item>
    <item>
      <title>Re: IMX 6 LCD controller,  SSD1322, 8080mode</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX-6-LCD-controller-SSD1322-8080mode/m-p/831994#M127782</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Alven&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;processors with eLCDIF, like i.MX7D or i.MX6UL supports 8080 mode&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-331754"&gt;https://community.nxp.com/docs/DOC-331754&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Detailed description can be found in eLCDIF Chapter of Reference Manual of used processor.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 04 Dec 2018 23:42:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX-6-LCD-controller-SSD1322-8080mode/m-p/831994#M127782</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2018-12-04T23:42:20Z</dc:date>
    </item>
    <item>
      <title>Re: IMX 6 LCD controller,  SSD1322, 8080mode</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX-6-LCD-controller-SSD1322-8080mode/m-p/831995#M127783</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;HI Actually , I try to use it on FreeRTOS platform. However , it seems to be used in Linux . After going through the document , I still can not understand these bits' meaning . Could anyone explain for that ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 05 Dec 2018 01:58:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX-6-LCD-controller-SSD1322-8080mode/m-p/831995#M127783</guid>
      <dc:creator>alvenwu</dc:creator>
      <dc:date>2018-12-05T01:58:36Z</dc:date>
    </item>
    <item>
      <title>Re: IMX 6 LCD controller,  SSD1322, 8080mode</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX-6-LCD-controller-SSD1322-8080mode/m-p/831996#M127784</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;eLCDIF register descriptions can be found in documentation, for example&lt;/P&gt;&lt;P&gt;Chapter 32&amp;nbsp;Enhanced LCD Interface (eLCDIF)&amp;nbsp;i.MX6UL Reference Manual&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.nxp.com/docs/en/reference-manual/IMX6ULRM.pdf"&gt;http://www.nxp.com/docs/en/reference-manual/IMX6ULRM.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 05 Dec 2018 05:24:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX-6-LCD-controller-SSD1322-8080mode/m-p/831996#M127784</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2018-12-05T05:24:38Z</dc:date>
    </item>
    <item>
      <title>Re: IMX 6 LCD controller,  SSD1322, 8080mode</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX-6-LCD-controller-SSD1322-8080mode/m-p/831997#M127785</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi igor,&amp;nbsp;&lt;/P&gt;&lt;P&gt;thanks for your support.&lt;/P&gt;&lt;P&gt;However ,&amp;nbsp; the reference manual doesnot describes clearly how to configure LCD controller into 8080mode to communicate with oled mode.&amp;nbsp;&lt;/P&gt;&lt;P&gt;could you give me some sample code ?&amp;nbsp; how to configure the display clock ? should we use the 'run' bit in CTRL register ? rather confused&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 06 Dec 2018 22:57:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX-6-LCD-controller-SSD1322-8080mode/m-p/831997#M127785</guid>
      <dc:creator>alvenwu</dc:creator>
      <dc:date>2018-12-06T22:57:55Z</dc:date>
    </item>
    <item>
      <title>Re: IMX 6 LCD controller,  SSD1322, 8080mode</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX-6-LCD-controller-SSD1322-8080mode/m-p/831998#M127786</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;HI Currenly , I am using the LCD controller to connect to the OLE SSD1322 to display something.&lt;/P&gt;&lt;P&gt;Seems the simple commands like display on/off work well , but when it comes to the command+ data pairs , it doesn't work at all. nothing could display except the raw display screen.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Could anyone give some advice about that ?thanks.&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 29 Dec 2018 06:51:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX-6-LCD-controller-SSD1322-8080mode/m-p/831998#M127786</guid>
      <dc:creator>alvenwu</dc:creator>
      <dc:date>2018-12-29T06:51:04Z</dc:date>
    </item>
  </channel>
</rss>