<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: iMX287 RTC in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/iMX287-RTC/m-p/831898#M127768</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;1. RTC OK&lt;/P&gt;&lt;P&gt;2. 之前的设计Ethernet是采用Core(TCC7901)+CS8900A，Ethernet 接口采用ISA BUS总线型式，我们现在底板（底板集成有CS8900A）想不改，只想更换核心板，我想问iMX287的Ethernet支不支持ISA BUS总线接口型式，如果支持，硬件怎么连接？&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 16 Nov 2018 02:20:21 GMT</pubDate>
    <dc:creator>7_xi</dc:creator>
    <dc:date>2018-11-16T02:20:21Z</dc:date>
    <item>
      <title>iMX287 RTC</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX287-RTC/m-p/831896#M127766</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;IMX287 RTC能够独立供电及运行吗？手册上写的不清楚？&lt;/P&gt;&lt;P&gt;另外IMX287的网口支持ISA模式吗，怎么接线？有硬件设计说明吗？&lt;/P&gt;&lt;P&gt;资料太少了。&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 14 Nov 2018 00:48:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX287-RTC/m-p/831896#M127766</guid>
      <dc:creator>7_xi</dc:creator>
      <dc:date>2018-11-14T00:48:25Z</dc:date>
    </item>
    <item>
      <title>Re: iMX287 RTC</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX287-RTC/m-p/831897#M127767</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;Hello,&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp;&amp;nbsp; &lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp; Please use Chapter 22 (Real-Time Clock Alarm Watchdog Persistent Bits) of the &lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;i.MX28 Reference Manual. Basically to get the RTC working in power down mode &lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;battery power (BATT) should be applied.&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp; It is possible to configure the battery supply only for RTC domain: &lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;when using a battery and a 5V power connection, the customer should apply the &lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;same circuit connections in the "i.MX28 Reference Schematics", which are posted &lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;on the Web. &lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;This can be accomplished as follows: &lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;1. Clear the DCDC_XFER bit (bit 5) in the HW_POWER_5VCTRL register, which will &lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;disable the automatic transition to the DCDC converter (from the battery) when &lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;5V power is removed. &lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;2. Set the PWDN_5VBRNOUT bit (bit 7) in the HW_POWER_5VCTRL register, which will &lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;automatically power down the device when 5V is removed. &lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;3. Also, customers may want to set the PWDN_BRNOUT bit (bit 18) in the &lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;HW_POWER_VDDIOCTRL, which will automatically power down the device when a VDDIO &lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;brownout occurs. Note this only has effect if 5V is not present. After the VDDIO &lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;brownout is set up, a VDDIO brownout will occur because the SW will not be setup &lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;to run from the battery (via the DCDC converter) when 5V is removed, because the &lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;DCDC_XFER bit will be cleared.&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp; As for i.MX28 network - what do You mean? Please clarify in more details. &lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;Have a great day,&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;Yuri&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;------------------------------------------------------------------------------&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;Note: If this post answers your question, please click the Correct Answer &lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;button. Thank you!&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 15 Nov 2018 07:50:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX287-RTC/m-p/831897#M127767</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2018-11-15T07:50:35Z</dc:date>
    </item>
    <item>
      <title>Re: iMX287 RTC</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX287-RTC/m-p/831898#M127768</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;1. RTC OK&lt;/P&gt;&lt;P&gt;2. 之前的设计Ethernet是采用Core(TCC7901)+CS8900A，Ethernet 接口采用ISA BUS总线型式，我们现在底板（底板集成有CS8900A）想不改，只想更换核心板，我想问iMX287的Ethernet支不支持ISA BUS总线接口型式，如果支持，硬件怎么连接？&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 16 Nov 2018 02:20:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX287-RTC/m-p/831898#M127768</guid>
      <dc:creator>7_xi</dc:creator>
      <dc:date>2018-11-16T02:20:21Z</dc:date>
    </item>
    <item>
      <title>Re: iMX287 RTC</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX287-RTC/m-p/831899#M127769</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;急，为什么没审批没答复？&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 20 Nov 2018 05:41:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX287-RTC/m-p/831899#M127769</guid>
      <dc:creator>7_xi</dc:creator>
      <dc:date>2018-11-20T05:41:21Z</dc:date>
    </item>
  </channel>
</rss>