<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: RiotBoard not executing compiled uBoot image from SD card</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/RiotBoard-not-executing-compiled-uBoot-image-from-SD-card/m-p/831760#M127742</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;You can modify the bootargs in u-boot to boot the kernel from different storage device.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 02 Jan 2019 09:13:54 GMT</pubDate>
    <dc:creator>jimmychan</dc:creator>
    <dc:date>2019-01-02T09:13:54Z</dc:date>
    <item>
      <title>RiotBoard not executing compiled uBoot image from SD card</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/RiotBoard-not-executing-compiled-uBoot-image-from-SD-card/m-p/831759#M127741</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am trying to port riotboard with linux 4.2 from buildroot build on ubuntu 18.XX.&lt;/P&gt;&lt;P&gt;My problem might sound silly but not able to boot board with compiled uboot image from SD card. Its executing some pre-build image.&lt;/P&gt;&lt;P&gt;Bootup logs:&lt;BR /&gt;U-Boot 2009.08-00695-g055df3a (Dec 25 2013 - 09:56:12)&lt;BR /&gt;CPU: Freescale i.MX6 family TO1.1 at 792 MHz&lt;BR /&gt;Thermal sensor with ratio = 181&lt;BR /&gt;Temperature: 30 C, calibration data 0x57b5025f&lt;BR /&gt;mx6q pll1: 792MHz&lt;BR /&gt;mx6q pll2: 528MHz&lt;BR /&gt;mx6q pll3: 480MHz&lt;BR /&gt;mx6q pll8: 50MHz&lt;BR /&gt;ipg clock : 66000000Hz&lt;BR /&gt;ipg per clock : 66000000Hz&lt;BR /&gt;uart clock : 80000000Hz&lt;BR /&gt;cspi clock : 60000000Hz&lt;BR /&gt;ahb clock : 132000000Hz&lt;BR /&gt;axi clock : 198000000Hz&lt;BR /&gt;emi_slow clock: 99000000Hz&lt;BR /&gt;ddr clock : 396000000Hz&lt;BR /&gt;usdhc1 clock : 198000000Hz&lt;BR /&gt;usdhc2 clock : 198000000Hz&lt;BR /&gt;usdhc3 clock : 198000000Hz&lt;BR /&gt;usdhc4 clock : 198000000Hz&lt;BR /&gt;nfc clock : 24000000Hz&lt;BR /&gt;Board: i.MX6DL/Solo-SABRESD: unknown-board Board: 0x61011 [POR ]&lt;BR /&gt;Boot Device: SD&lt;BR /&gt;I2C: ready&lt;BR /&gt;DRAM: 1 GB&lt;BR /&gt;MMC: FSL_USDHC: 0,FSL_USDHC: 1,FSL_USDHC: 2,FSL_USDHC: 3&lt;BR /&gt;In: serial&lt;BR /&gt;Out: serial&lt;BR /&gt;Err: serial&lt;BR /&gt;Net: got MAC address from IIM: 00:00:00:00:00:00&lt;BR /&gt;----enet_board_init: phy reset&lt;BR /&gt;FEC0 [PRIME]&lt;BR /&gt;Hit any key to stop autoboot: 0&lt;BR /&gt;mmc1 is current device&lt;BR /&gt;MMC read: dev # 1, block # 2048, count 8192 ... 8192 blocks read: OK&lt;BR /&gt;Wrong Image Format for bootm command&lt;BR /&gt;ERROR: can't get kernel image!&lt;BR /&gt;MX6Solo RIOT U-Boot &amp;gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;It always bootup probably with default(pre-compiled) uboot (Dec 25 2013 - 09:56:12) . Boot device selected is SD card. But not executing new compiled uboot image from SD card.&lt;BR /&gt;Board will bootup even formatted SD card is connected. But board didn't bootup if SD is not connected.&lt;BR /&gt;Not understanding from where its executing uboot image &amp;amp; why? (May be SPI flash.. not sure). How the board will execute new compiled uboot image from SD card.&lt;BR /&gt;Appreciate your comments &amp;amp; feedback.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Thanks,&lt;BR /&gt;Zahir&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 25 Dec 2018 06:36:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/RiotBoard-not-executing-compiled-uBoot-image-from-SD-card/m-p/831759#M127741</guid>
      <dc:creator>Zaak</dc:creator>
      <dc:date>2018-12-25T06:36:00Z</dc:date>
    </item>
    <item>
      <title>Re: RiotBoard not executing compiled uBoot image from SD card</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/RiotBoard-not-executing-compiled-uBoot-image-from-SD-card/m-p/831760#M127742</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;You can modify the bootargs in u-boot to boot the kernel from different storage device.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 02 Jan 2019 09:13:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/RiotBoard-not-executing-compiled-uBoot-image-from-SD-card/m-p/831760#M127742</guid>
      <dc:creator>jimmychan</dc:creator>
      <dc:date>2019-01-02T09:13:54Z</dc:date>
    </item>
  </channel>
</rss>