<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Multiple build with different rc.local and interface files for same machine in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Multiple-build-with-different-rc-local-and-interface-files-for/m-p/830621#M127629</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Sebastiaan,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The way to configure different images for the same machine would be similar, as in that you would need to write a new image or append an existing one. Instead of changing depending on the machine you would need to have a dedicated image or image version for each configuration. I would strongly suggest that you use different image names and customize them, as this is much easier to manage than having different versions of the same image.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this helps!&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 09 Oct 2018 16:10:17 GMT</pubDate>
    <dc:creator>gusarambula</dc:creator>
    <dc:date>2018-10-09T16:10:17Z</dc:date>
    <item>
      <title>Multiple build with different rc.local and interface files for same machine</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Multiple-build-with-different-rc-local-and-interface-files-for/m-p/830620#M127628</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear People of the NXP community.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is it possible in Yocto to do two different build one the same machine with different rc.local (fsl-rc-local) or interface (netbase). You can easy make different interface and rc.local file for different machine by using the .bbappend. But I do not know how you make different images with different rc.local and interface file for the same machine?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kind regards&lt;/P&gt;&lt;P&gt;Sebastiaan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 05 Oct 2018 10:40:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Multiple-build-with-different-rc-local-and-interface-files-for/m-p/830620#M127628</guid>
      <dc:creator>sebastiaanlaga</dc:creator>
      <dc:date>2018-10-05T10:40:50Z</dc:date>
    </item>
    <item>
      <title>Re: Multiple build with different rc.local and interface files for same machine</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Multiple-build-with-different-rc-local-and-interface-files-for/m-p/830621#M127629</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Sebastiaan,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The way to configure different images for the same machine would be similar, as in that you would need to write a new image or append an existing one. Instead of changing depending on the machine you would need to have a dedicated image or image version for each configuration. I would strongly suggest that you use different image names and customize them, as this is much easier to manage than having different versions of the same image.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this helps!&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 09 Oct 2018 16:10:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Multiple-build-with-different-rc-local-and-interface-files-for/m-p/830621#M127629</guid>
      <dc:creator>gusarambula</dc:creator>
      <dc:date>2018-10-09T16:10:17Z</dc:date>
    </item>
  </channel>
</rss>