<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Openocd on the imx6ULL EVK</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Openocd-on-the-imx6ULL-EVK/m-p/830586#M127621</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Ian&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;seems similar issue was reported on openocd mail list&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://sourceforge.net/p/openocd/mailman/message/35884014/" title="https://sourceforge.net/p/openocd/mailman/message/35884014/"&gt;OpenOCD - Open On-Chip Debugger / Mailing Lists&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;One can try kernel boot parameter enable_wait_mode=off to disable&lt;/P&gt;&lt;P&gt;entering low power mode.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 21 Jul 2018 05:46:40 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2018-07-21T05:46:40Z</dc:date>
    <item>
      <title>Openocd on the imx6ULL EVK</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Openocd-on-the-imx6ULL-EVK/m-p/830585#M127620</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi All,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We designed a custom board using an imx6ULL processor, and I have been trying to get openocd (using a Olimex ARM-USB-TINY-H) to work with it, but I get so far, and then it stops.&lt;/P&gt;&lt;P&gt;We then purchased a imx6ULL EVK assuming there might be something wrong with our custom board, but it has the same / similar issues.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have got it to a state where it looks like it is starting up OK, but I can not halt or reset the EVK.&amp;nbsp; Note there is no firmware programming into the EVK (the microSD card is out).&amp;nbsp; I am happy to provide my exisitng imx6ull.cfg and openocd.cfg files if anyone is interested.&amp;nbsp; This is the output I am getting:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P style="padding-left: 30px;"&gt;Open On-Chip Debugger 0.10.0&lt;BR /&gt;Licensed under GNU GPL v2&lt;BR /&gt;For bug reports, read&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;&lt;/SPAN&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fopenocd.org%2Fdoc%2Fdoxygen%2Fbugs.html" rel="nofollow" target="_blank"&gt;http://openocd.org/doc/doxygen/bugs.html&lt;/A&gt;&lt;BR /&gt;Info : auto-selecting first available session transport "jtag". To override use 'transport select &amp;lt;transport&amp;gt;'.&lt;BR /&gt;Warn : imx6.sdma: nonstandard IR value&lt;BR /&gt;adapter speed: 1000 kHz&lt;BR /&gt;trst_and_srst separate srst_gates_jtag trst_open_drain srst_open_drain connect_deassert_srst&lt;BR /&gt;adapter speed: 1000 kHz&lt;BR /&gt;jtag_ntrst_delay: 1000&lt;BR /&gt;Info : clock speed 1000 kHz&lt;BR /&gt;Info : JTAG tap: imx6.dap tap/device found: 0x5ba00477 (mfg: 0x23b (ARM Ltd.), part: 0xba00, ver: 0x5)&lt;BR /&gt;Info : TAP imx6.sdma does not have IDCODE&lt;BR /&gt;Info : JTAG tap: imx6.sjc tap/device found: 0x088c101d (mfg: 0x00e (Freescale (Motorola)), part: 0x88c1, ver: 0x0)&lt;BR /&gt;Error: target-&amp;gt;coreid 0 OSLock sticky, core not powered?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When turning on debug I get the following:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P style="padding-left: 30px;"&gt;Info : 351 1185 core.c:959 jtag_examine_chain_display(): JTAG tap: imx6.sjc tap/device found: 0x088c101d (mfg: 0x00e (Freescale (Motorola)), part: 0x88c1, ver: 0x0)&lt;BR /&gt;Debug: 352 1185 core.c:1190 jtag_validate_ircapture(): IR capture validation scan&lt;BR /&gt;Debug: 353 1191 core.c:1248 jtag_validate_ircapture(): imx6.dap: IR capture 0x01&lt;BR /&gt;Debug: 354 1191 core.c:1248 jtag_validate_ircapture(): imx6.sdma: IR capture 0x00&lt;BR /&gt;Debug: 355 1191 core.c:1248 jtag_validate_ircapture(): imx6.sjc: IR capture 0x01&lt;BR /&gt;Debug: 356 1191 openocd.c:153 handle_init_command(): Examining targets...&lt;BR /&gt;Debug: 357 1191 target.c:1517 target_call_event_callbacks(): target event 21 (examine-start)&lt;BR /&gt;Debug: 358 1191 arm_adi_v5.c:603 dap_dp_init(): &amp;nbsp;&lt;BR /&gt;Debug: 359 1203 arm_adi_v5.c:637 dap_dp_init(): DAP: wait CDBGPWRUPACK&lt;BR /&gt;Debug: 360 1203 arm_adi_v5.h:428 dap_dp_poll_register(): DAP: poll 4, mask 0x20000000, value 0x20000000&lt;BR /&gt;Debug: 361 1222 arm_adi_v5.c:644 dap_dp_init(): DAP: wait CSYSPWRUPACK&lt;BR /&gt;Debug: 362 1222 arm_adi_v5.h:428 dap_dp_poll_register(): DAP: poll 4, mask 0x80000000, value 0x80000000&lt;BR /&gt;Debug: 363 1274 arm_adi_v5.c:785 dap_find_ap(): Found APB-AP at AP index: 1 (IDR=0x44770002)&lt;BR /&gt;Debug: 364 1283 arm_adi_v5.c:712 mem_ap_init(): MEM_AP Packed Transfers: disabled&lt;BR /&gt;Debug: 365 1283 arm_adi_v5.c:723 mem_ap_init(): MEM_AP CFG: large data 0, long address 0, big-endian 0&lt;BR /&gt;Debug: 366 1294 arm_adi_v5.c:785 dap_find_ap(): Found AHB-AP at AP index: 0 (IDR=0x74770001)&lt;BR /&gt;Debug: 367 1303 arm_adi_v5.c:712 mem_ap_init(): MEM_AP Packed Transfers: enabled&lt;BR /&gt;Debug: 368 1303 arm_adi_v5.c:723 mem_ap_init(): MEM_AP CFG: large data 0, long address 0, big-endian 0&lt;BR /&gt;Debug: 369 1331 cortex_a.c:3007 cortex_a_examine_first(): didr = 0x3515f005&lt;BR /&gt;Debug: 370 1331 cortex_a.c:3008 cortex_a_examine_first(): cpuid = 0x410fc075&lt;BR /&gt;Debug: 371 1346 cortex_a.c:3017 cortex_a_examine_first(): target-&amp;gt;coreid 0 DBGPRSR&amp;nbsp; 0x2b&lt;BR /&gt;Debug: 372 1346 cortex_a.c:3026 cortex_a_examine_first(): target-&amp;gt;coreid 0 was reset!&lt;BR /&gt;Debug: 373 1357 cortex_a.c:3033 cortex_a_examine_first(): target-&amp;gt;coreid 0 DBGOSLSR 0xa&lt;BR /&gt;Debug: 374 1357 cortex_a.c:3039 cortex_a_examine_first(): target-&amp;gt;coreid 0 OSLock set! Trying to unlock&lt;BR /&gt;Debug: 375 1388 cortex_a.c:3050 cortex_a_examine_first():&amp;nbsp;&amp;nbsp;&amp;nbsp; ret = 0, OSLSR = a&lt;BR /&gt;Error: 376 1388 cortex_a.c:3052 cortex_a_examine_first(): target-&amp;gt;coreid 0 OSLock sticky, core not powered?&lt;BR /&gt;Debug: 377 1388 openocd.c:155 handle_init_command(): target examination failed&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Note I have added some extra debug to the 0.10.0 log which is the return from trying to clear the OS Lock. and the DBGOSLSR regsiter is still the same.&lt;/P&gt;&lt;P&gt;Looking at the DBGPRSR it is showing 0x2B, which indicates (the bottom bit) that the core is powered, but I am still unable to unlock the OS Lock.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Does anyone have a working configuration file for this processor, or any hints about how I can get past this place?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;regards,&lt;/P&gt;&lt;P&gt;Ian Caddy&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 19 Jul 2018 07:39:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Openocd-on-the-imx6ULL-EVK/m-p/830585#M127620</guid>
      <dc:creator>iancaddy</dc:creator>
      <dc:date>2018-07-19T07:39:00Z</dc:date>
    </item>
    <item>
      <title>Re: Openocd on the imx6ULL EVK</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Openocd-on-the-imx6ULL-EVK/m-p/830586#M127621</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Ian&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;seems similar issue was reported on openocd mail list&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://sourceforge.net/p/openocd/mailman/message/35884014/" title="https://sourceforge.net/p/openocd/mailman/message/35884014/"&gt;OpenOCD - Open On-Chip Debugger / Mailing Lists&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;One can try kernel boot parameter enable_wait_mode=off to disable&lt;/P&gt;&lt;P&gt;entering low power mode.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 21 Jul 2018 05:46:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Openocd-on-the-imx6ULL-EVK/m-p/830586#M127621</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2018-07-21T05:46:40Z</dc:date>
    </item>
    <item>
      <title>Re: Openocd on the imx6ULL EVK</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Openocd-on-the-imx6ULL-EVK/m-p/830587#M127622</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Igor,&lt;/P&gt;&lt;P&gt;Thanks for the reply, but unfortunately there is no firmware running on either board (except the ROM bootloader).&amp;nbsp; The EVK did not have the uSD card inserted.&amp;nbsp; Later in another test we put the uSD card in to see if the EVK was working correctly and it booted up OK.&lt;/P&gt;&lt;P&gt;When using OpenOCD with the Linux kernel in place, it stops (reboots) the kernel, but then allows the kernel to continue starting up after OpenOCD has finished initialiising.&lt;/P&gt;&lt;P&gt;We are also running a imx6ULL which seems to be different to the imx6UL.&amp;nbsp; I have also put this same question over on the OpenOCD mailing list, but so far have had zero interest in this issue.&lt;/P&gt;&lt;P&gt;regards,&lt;/P&gt;&lt;P&gt;Ian Caddy&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 23 Jul 2018 00:52:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Openocd-on-the-imx6ULL-EVK/m-p/830587#M127622</guid>
      <dc:creator>iancaddy</dc:creator>
      <dc:date>2018-07-23T00:52:41Z</dc:date>
    </item>
    <item>
      <title>Re: Openocd on the imx6ULL EVK</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Openocd-on-the-imx6ULL-EVK/m-p/830588#M127623</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi All,&lt;/P&gt;&lt;P&gt;I appear to have this working now, and wanted to post the solution, although I am still a bit confused about it.&lt;/P&gt;&lt;P&gt;In my imx6ull.cfg file I based it on the original imx6.cfg file in the openocd tree but had to change the DAP address as it was incorrect for the imx6ULL part:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P style="padding-left: 30px;"&gt;# core 0&amp;nbsp; -&amp;nbsp; 0x82150000&lt;BR /&gt;# core 0&amp;nbsp; -&amp;nbsp; 0x02130000&lt;BR /&gt;set _TARGETNAME $_CHIPNAME.cpu.0&lt;BR /&gt;target create $_TARGETNAME cortex_a -chain-position $_CHIPNAME.dap \&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; -coreid 0 -dbgbase 0x02130000&lt;/P&gt;&lt;P style="padding-left: 30px;"&gt;&lt;/P&gt;&lt;P&gt;Originally the DAP was setup to be 0x82150000 but looking through the im6ULL Reference Manual it shows the DAP to be at 0x02130000, and I could get DAP information at this address, but seems my write to clear the OSLock bit was failing (although the write said it worked OK, but did not change the value).&lt;/P&gt;&lt;P&gt;Looking through other imx configurations in the examples, I noticed that on the imx53.cfg file there was no DAP address loaded, so I thought maybe on a single core it was not needed, so I removed it:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P style="padding-left: 30px;"&gt;set _TARGETNAME $_CHIPNAME.cpu.0&lt;BR /&gt;target create $_TARGETNAME cortex_a -chain-position $_CHIPNAME.dap&lt;/P&gt;&lt;P style="padding-left: 30px;"&gt;&lt;/P&gt;&lt;P&gt;And the JTAG then tried to discover the DAP address from the ROM table:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P style="padding-left: 30px;"&gt;Detected core 0 dbgbase: 80030000&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Not anwhere near what the memory map in the reference manual indicates (in fact this address is somewhere int he DDR space).&amp;nbsp; Anyway, it is now working and I can halt the chip so I can start developing and debugging.&amp;nbsp; I have enclosed the imx6ull.cfg and openocd.cfg files I am currently using for reference, on the imx6ULL EVK.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;imx6ull.cfg:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P style="padding-left: 30px;"&gt;# Freescale i.MX6ULL processor&lt;BR /&gt;if { [info exists CHIPNAME] } {&lt;BR /&gt;&amp;nbsp;&amp;nbsp; set&amp;nbsp; _CHIPNAME $CHIPNAME&lt;BR /&gt;} else {&lt;BR /&gt;&amp;nbsp;&amp;nbsp; set&amp;nbsp; _CHIPNAME imx6&lt;BR /&gt;}&lt;BR /&gt;# CoreSight Debug Access Port&lt;BR /&gt;if { [info exists DAP_TAPID] } {&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; set _DAP_TAPID $DAP_TAPID&lt;BR /&gt;} else {&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; set _DAP_TAPID 0x5ba00477&lt;BR /&gt;}&lt;BR /&gt;jtag newtap $_CHIPNAME dap -irlen 4 -ircapture 0x01 -irmask 0x0f \&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; -expected-id $_DAP_TAPID&lt;BR /&gt;# SDMA / no IDCODE&lt;BR /&gt;jtag newtap $_CHIPNAME sdma -irlen 4 -ircapture 0x00 -irmask 0x0f&lt;/P&gt;&lt;P style="padding-left: 30px;"&gt;&lt;/P&gt;&lt;P style="padding-left: 30px;"&gt;# System JTAG Controller&lt;BR /&gt;if { [info exists SJC_TAPID] } {&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; set _SJC_TAPID $SJC_TAPID&lt;BR /&gt;} else {&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; set _SJC_TAPID 0x088c101d&lt;BR /&gt;}&lt;/P&gt;&lt;P style="padding-left: 30px;"&gt;&lt;/P&gt;&lt;P style="padding-left: 30px;"&gt;jtag newtap $_CHIPNAME sjc -irlen 5 -ircapture 0x01 -irmask 0x1f \&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; -expected-id $_SJC_TAPID&lt;/P&gt;&lt;P style="padding-left: 30px;"&gt;&lt;/P&gt;&lt;P style="padding-left: 30px;"&gt;# GDB target: Cortex-A7, using DAP, configuring only one core&lt;BR /&gt;set _TARGETNAME $_CHIPNAME.cpu.0&lt;BR /&gt;target create $_TARGETNAME cortex_a -chain-position $_CHIPNAME.dap&lt;/P&gt;&lt;P style="padding-left: 30px;"&gt;&lt;/P&gt;&lt;P style="padding-left: 30px;"&gt;# some TCK cycles are required to activate the DEBUG power domain&lt;BR /&gt;jtag configure $_CHIPNAME.sjc -event post-reset "runtest 100"&lt;/P&gt;&lt;P style="padding-left: 30px;"&gt;&lt;/P&gt;&lt;P style="padding-left: 30px;"&gt;proc imx6_dbginit {target} {&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; # General Cortex-A8/A9 debug initialisation&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; cortex_a dbginit&lt;BR /&gt;}&lt;/P&gt;&lt;P style="padding-left: 30px;"&gt;&lt;/P&gt;&lt;P style="padding-left: 30px;"&gt;# Slow speed to be sure it will work&lt;BR /&gt;adapter_khz 1000&lt;BR /&gt;$_TARGETNAME configure -event reset-start { adapter_khz 1000 }&lt;BR /&gt;$_TARGETNAME configure -event reset-assert-post "imx6_dbginit $_TARGETNAME"&lt;BR /&gt;$_TARGETNAME configure -event gdb-attach { halt }&lt;/P&gt;&lt;P style="padding-left: 30px;"&gt;&lt;/P&gt;&lt;P&gt;openocd.cfg file:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P style="padding-left: 30px;"&gt;&lt;BR /&gt;source ../openocd-0.10.0/tcl/interface/ftdi/olimex-arm-usb-tiny-h.cfg&lt;/P&gt;&lt;P style="padding-left: 30px;"&gt;&lt;/P&gt;&lt;P style="padding-left: 30px;"&gt;# Setup information for our busblaster and imx6 solo&lt;BR /&gt;set DAP_TAPID 0x5ba00477&lt;BR /&gt;set SJC_TAPID 0x088c101d&lt;/P&gt;&lt;P style="padding-left: 30px;"&gt;&lt;/P&gt;&lt;P style="padding-left: 30px;"&gt;# imx config&lt;BR /&gt;source imx6ull.cfg&lt;/P&gt;&lt;P style="padding-left: 30px;"&gt;&lt;/P&gt;&lt;P style="padding-left: 30px;"&gt;# SRST connects to POR_B&lt;BR /&gt;#reset_config srst_only&lt;BR /&gt;#reset_config trst_and_srst srst_pulls_trst&lt;BR /&gt;#reset_config trst_and_srst separate trst_open_drain srst_open_drain&lt;BR /&gt;reset_config trst_and_srst trst_open_drain srst_open_drain&lt;/P&gt;&lt;P style="padding-left: 30px;"&gt;&lt;/P&gt;&lt;P style="padding-left: 30px;"&gt;# No RTCK&lt;BR /&gt;adapter_khz 1000&lt;BR /&gt;#$_TARGETNAME configure -event reset-start { adapter_khz 1000 }&lt;/P&gt;&lt;P style="padding-left: 30px;"&gt;&lt;/P&gt;&lt;P style="padding-left: 30px;"&gt;# Can't get watchdog to reset correctly yet.. for now, just don't reset here.&lt;BR /&gt;# We already did a reset back in init_reset anyway.&lt;BR /&gt;#$_TARGETNAME configure -event reset-assert {}&lt;/P&gt;&lt;P style="padding-left: 30px;"&gt;&lt;/P&gt;&lt;P style="padding-left: 30px;"&gt;# This delay affects how soon after SRST we try to halt, so make it as&lt;BR /&gt;# small as possible. However, if it is too small we will fail the JTAG scan.&lt;BR /&gt;# Delay determined by experimentation&lt;BR /&gt;jtag_ntrst_delay 1000&lt;/P&gt;&lt;P style="padding-left: 30px;"&gt;&lt;/P&gt;&lt;P style="padding-left: 30px;"&gt;gdb_port 3333&lt;BR /&gt;telnet_port 3000&lt;/P&gt;&lt;P style="padding-left: 30px;"&gt;&lt;/P&gt;&lt;P style="padding-left: 30px;"&gt;&lt;/P&gt;&lt;P&gt;Now to add in the DDR init and see if we can start debugging real code.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Ian Caddy&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 24 Jul 2018 02:37:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Openocd-on-the-imx6ULL-EVK/m-p/830588#M127623</guid>
      <dc:creator>iancaddy</dc:creator>
      <dc:date>2018-07-24T02:37:50Z</dc:date>
    </item>
  </channel>
</rss>