<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: otg connect new hub in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/otg-connect-new-hub/m-p/830271#M127563</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The problem OK, it`s hardware .&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 12 Jul 2018 02:40:15 GMT</pubDate>
    <dc:creator>yuhundehao</dc:creator>
    <dc:date>2018-07-12T02:40:15Z</dc:date>
    <item>
      <title>otg connect new hub</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/otg-connect-new-hub/m-p/830268#M127560</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The imx6qsd development board I used originally had and hub now I want to use OTG to connect to a hub (gl850g). how to do it?&lt;/P&gt;&lt;P&gt;kernel :3.0.35&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 29 Jun 2018 07:13:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/otg-connect-new-hub/m-p/830268#M127560</guid>
      <dc:creator>yuhundehao</dc:creator>
      <dc:date>2018-06-29T07:13:00Z</dc:date>
    </item>
    <item>
      <title>Re: otg connect new hub</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/otg-connect-new-hub/m-p/830269#M127561</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;STRONG&gt;(1) 2 USB OTG ports&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;there are 2 USB OTG ports, only one of them can be used to be USB OTG(dual role: Host or device), the other one should be work at HOST MODE.&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;(2)USB OTG working at Dual Role mode&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;USB OTG ID should be pulled down to LOW if you want it to work at HOST mode, and the pin should be pulled up to HIGH. By default, the ID pin is HIGH level, it means if you don't set the pin, USB OTG will work at device mode.&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;(3) for you application&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;--USB OTG1 should be set to be HOST mode&lt;/P&gt;&lt;P&gt;--USB OTG1 ID should be pulled down to LOW via a resistor ( 2.2K , or 3.3K or others)&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 04 Jul 2018 08:02:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/otg-connect-new-hub/m-p/830269#M127561</guid>
      <dc:creator>Rita_Wang</dc:creator>
      <dc:date>2018-07-04T08:02:11Z</dc:date>
    </item>
    <item>
      <title>Re: otg connect new hub</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/otg-connect-new-hub/m-p/830270#M127562</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks&amp;nbsp;&lt;A _jive_internal="true" data-content-finding="Community" data-userid="213877" data-username="b45499" href="https://community.nxp.com/people/b45499" style="color: #3d9ce7; background-color: #ffffff; border: 0px; font-weight: 200; text-decoration: underline; font-size: 1.286rem;"&gt;Rita Wang&lt;/A&gt;.&lt;/P&gt;&lt;P&gt;I ID pin is low level,My OTG communication hub（gl850） has no response. Does the Kerenl&amp;nbsp;have to be configured accordingly?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 04 Jul 2018 08:29:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/otg-connect-new-hub/m-p/830270#M127562</guid>
      <dc:creator>yuhundehao</dc:creator>
      <dc:date>2018-07-04T08:29:06Z</dc:date>
    </item>
    <item>
      <title>Re: otg connect new hub</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/otg-connect-new-hub/m-p/830271#M127563</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The problem OK, it`s hardware .&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 12 Jul 2018 02:40:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/otg-connect-new-hub/m-p/830271#M127563</guid>
      <dc:creator>yuhundehao</dc:creator>
      <dc:date>2018-07-12T02:40:15Z</dc:date>
    </item>
    <item>
      <title>Re: otg connect new hub</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/otg-connect-new-hub/m-p/830272#M127564</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;OK&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 12 Jul 2018 02:50:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/otg-connect-new-hub/m-p/830272#M127564</guid>
      <dc:creator>Rita_Wang</dc:creator>
      <dc:date>2018-07-12T02:50:54Z</dc:date>
    </item>
  </channel>
</rss>